SIMATIC IOT2020
SubscribeThe IOT2020 gateway is compatible with most Arduino sketches that can be uploaded directly from the Arduino IDE. Many other programs can be compiled and or run under Yocto Linux on the used controller X1000 SOC (X86). Third-party hardware such as PLCs and sensors from various different brands can be integrated via Ethernet or Serial (via USB adapter) using many available and open protocols including Modbus, Profinet, REST or MQTT
The IOT2020 is also compatible with Arduino shields and various programming languages, including high-level languages such as Java, C++ and Python via a range of IDEs that includes Eclipse and compilers for Yocto Linux. It is also expandable via an on-board mPCIe port. Node-Red, MQTT and SQLITE3 can also be used to connect and control local and remote peripherals, such as sensors on a device.
Questions & Answers
Find solutions
Looking for a solution to a design conundrum? Browse our Simatic IOT2020 questions and find the best answers, as voted for by our community.
Answer questions
You don’t have to be an expert to answer a question, in the DesignSpark community you can offer assistance and answer community questions whatever your skill level.
Ask a question
Looking for answers to those questions you just can’t find an answer too?
Why not ask our community for help?
Latest Activity Stream
-
@peteroakes Hi, I have the same problem. Do you know how to fixed ?
-
@peteroakes Did you get any solution for that?
I got the same problem, same situation.
Thank you -
Hi Heiko. Frederick Vandenbosch has made a good 3d-printed cover design for that 3rd display you show in your post.
http://frederickvandenbosch.be/?p=2521 -
@peteroakes That's really helpful thank you so much. PS Thanks also for all the great videos on the IOT2020. They too have helped me hugely.
-
@Mldavies The COIL voltage of the relay would be the rating compatable with the IOT2020 outputs, so typically up to ~30V (24V normally for industrial) but the IOT2020 IO module can also handle 12V so you...
IoT2020 on board SPI
Hi been busy with my project where I am using IoT2020(Intel Galileo Gen2) and I am faced with the
3 Answers 5 Upvotes
I have a MEGA Arduino, can I use with this IOT2020, else what other model?
1 Answers
Trainer for IOT2020
Especially for educational purposes it is required to have an easy-to-get-started solution. I just found a training board especially made for the educational sector on Kaftan Media. Looks really exciting...

LCD displays for SIMATIC IOT2020
Are you looking for a LCD display for your IOT2020 project? Here is some useful information to get one done. Select your preferred variant.

Program the IOT2000 with Arduino IDE!
In this article I will show you how to program an IOT2000 with Arduino IDE!

Adding a C++ LCD Display Driver to the IOT2020
The Hitachi type LCD displays are used in many designs. They work with an Arduino sketch on the IOT2020. If you're building a C++ project, this driver class can help.

Talk UART to any Microcontroller with C++ and IOT2020
Serial communication between the SimaticIOT2020 and a (not so) random micro-controller.

Drive an I2C DAC with C++ on IOT2020
Control an I2C Digital to Analog converter with C++ on IOT202. Generate a sinus signal from stored samples. IC: DAC8571

Debug IOT2020 C++ Program with Eclipse Neon and Windows10 64-bit
How to remote debug an IOT2020 C++ program with Eclipse Neon. Work-around for the standard CDT and GDB combination that has reported issues with this combination.

1 year ago