Skip to main content

First steps to Direct Modelling Part 5: Look at the Combine Tool

by DesignSpark

This tutorial requires:

DesignSpark Mechanical V6.0

This tutorial is in progressive sections and will guide you with the main model creation commands in DesignSpark Mechanical. The first two sections will help you build two models (using the Sketch, Select and Pull tools) and the third section will show you how to assemble the models together (using a range of Move functions). Following sections will illustrate further skills, including Fill (removing features) and Combine (cutting into one model using another model or merging two models together). You will then be able to design your own parts and assemble them using the same tools and functions.

SECTION 5 - COMBINE TOOL

The combine tool is designed to allow two main actions to be carried out:

1. Using the shape of one solid to cut into another one, and

2. Merging adjacent or overlapping models into one object

The following exercise will go through some examples so that the skills can be applied to future work.

1. Open DesignSpark Mechanical (and close the welcome help screen)

2. Open the COMBINE MODELS file attached.

3. Triple left click on the connector to select it and press z to zoom in to the extents of the selected item

4. Select the Move tool on the Ribbon bar

5. Click on the anchor button to the left of the design screen

6. Select the inner face of the connector body by left clicking to place the move anchor on that face

7. Left click on the blue arrow of the move anchor and then click on the “Up to” command icon

8. Select the outer face of the rectangular casing by clicking on it to move the face of the connector onto it

9. Click in white space to end the Move action

10. Select Combine on the Ribbon bar

11. As prompted, select the casing as the target object

12. Select the connector as the cutter object (note that there are now lots of new solids listed in the structure tree – these are all the parts of the casing sidewall which have been cut by the profile of the connector)

13. Next to the 7156 connector solid in the structure tree un-tick the box to hide the object

14. Whilst still in Combine mode, drag a select box around the lines in the wall of the casing created by the connector to remove those parts of the wall of the casing

15. Click in white space to end the Combine action (note that the structure tree shows only the 3 solids again after all the cut parts of the casing have been removed)

16. Re-tick the 7156 box in the structure tree to see the connector in position

17. Now position the RS logo using the Move and Move – up to tools so that it is placed onto the outer face of the casing as shown and note that there are now 4 solids shown on the structure tree (7156 connector plus the casing and the 2 parts of the logo)

18. Click in white space to end the Move

19. Re-select the Combine tool on the Ribbon bar

20. As prompted, select the casing as the target object

21. Now, instead of selecting a cutter object, select the Merge icon as shown

22. Drag a select box around the RS Logo to select both solids and click on the logo

Note that the structure tree is now only showing 2 solids (the connector and the casing which now incorporates the logo)

The combine exercise is now complete. You may want to save these examples or continue to develop them.

RS DesignSpark is the go-to platform for students, makers, hobbyists and professional design engineers, providing design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software. Join the community today at https://www.rs-online.com/designspark/register
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments