Skip to main content

First steps to Direct Modelling Part 1: Look at the Sketch, Select and Pull tools

This tutorial requires:

DesignSpark Mechanical V6.0

This tutorial is in progressive sections and will guide you with the main model creation commands in DesignSpark Mechanical. The first two sections will help you build two models (using the Sketch, Select and Pull tools) and the third section will show you how to assemble the models together (using a range of Move functions). Following sections will illustrate further skills, including Fill (removing features) and Combine (cutting into one model using another model or merging two models together). You will then be able to design your own parts and assemble them using the same tools and functions.

The models created in sections 1 & 2 are used in later tutorials and they are also attached to the tutorials.

Section 1. Pin cube

  1. Open DesignSpark Mechanical

  2. Select File > New > Design if moving on from a previous design and close the welcome screen

    72e7d0220aba7aa05975604f8732f37c1082751d.png

  3. Ensure the Design tab on the Ribbon bar is selected

    0bf4f292b0147969941d03b47addc58020f9c223.png

  4. Select Plan view in the Design options on the Ribbon bar

    3e61a14d6f2bcbf04c5793b872cd776b9ce7dfef.png

  5. From the Sketch tools select Rectangle

    a052e4f3a7f9a015044e72c73c43c8013d6fb8a6.png

  6. On the sketch grid, left click & hold, drag, and click again to create a rectangle

  7. Type 25 to set the dimension in one axis

    327129355b1f06c67f9d7533797b2d646ff981f7.png

  8. Press Tab key on the keyboard to switch axes

  9. Type 25 to set the dimension in the other axis

  10. Press Enter – you should now have a 25mm square sketch on the grid in plan view

  11. Select Home view (top left on Ribbon bar)

    06a2c069c7ae4bca2b4f03fa33781ad80527e043.png

  12. Select the Pull tool on the Ribbon bar621cef214ed0a6f1002ac3ca7fc8975aa4000a49.png
  13. Left click on the square sketch surface and pull the shape up a few millimetres in the direction of the yellow arrow using left click and drag (alternatively hover the cursor over the square and left click & drag it up) and keep the left mouse button held down then

  14. Type 25 to set the new height of the cube

  15. Press Enter (and release mouse button)

  16. Press Home to reset the view

  17. Left click in white space to end the extrude action

  18. To round off the edges of the cube, multiple select them using Ctrl + left click (to select them all you will need to tumble the cube using the middle mouse button & manipulate mouse). To select all edges more easily you can edit the Selection filter (white cursor arrow at bottom of screen) by deselecting Smart and Faces.

  19. Whilst still in Pull mode drag a box around the model. All edges should then be selected and highlighted orange, but none of the faces.

  20. Using the Pull tool, left click and drag the yellow arrow towards the centre of the cube a small distance

  21. Type 2 to set the radius of the round

  22. Press Enter – the cube should now have all edges rounded

  23. From the sketch tools on the ribbon bar select Circle and the sketch grid should appear active

  24. Hover the cursor over a face of the cube to position the grid there, left click to start sketching (you should see that the grid is centred on the mid-point of the face of the cube)

  25. Left click the sketch cursor on the centre point of the sketch grid, hold & drag to 10mm (along an axis to keep clean dimensions) (or type dimension) and release

  26. In the same way as when you dragged the sketch to create the cube, use the Pull function to drag the circle up a short distance and release the drag

  27. Type 7 to set the length of the pin

  28. Repeat the last 4 steps on all faces of the cube. You will need to tumble the cube to view all sides by holding down middle mouse button and manoeuvring the mouse (the cube should now have 6 x 10mm diameter pins, 7mm long, on it)

  29. To add a round to the end of the pins, ensure the Pull tool from the ribbon bar is active

  30. Left click on the edge of the end of the pin to highlight

  31. Left click and drag the arrow down a short distance

  32. Type 1.5 to set the radius of the round

  33. Repeat the last 3 steps for each pin

  34. Save your file as PIN CUBE

THE PIN CUBE IS NOW COMPLETE.

RS DesignSpark is the go-to platform for students, makers, hobbyists and professional design engineers, providing design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software. Join the community today at https://www.rs-online.com/designspark/register