Skip to main content

Thingatron

by DrLucyRogers

The General Purpose Input/Output (GPIO) ports on development and microprocessor boards generally only work with logic level signals. This means they can only supply 3.3v and a few mA of current from each pin. This is enough to power an LED but to control a more powerful load (like motors) some additional circuitry to boost the current and/or voltage to a higher level is required.

One way to do this is to use an open collector driver. This is an electronic circuit that uses a transistor – that is turned on by a logic level signal from a GPIO port to its base terminal. The transistor can then switch a much bigger current via its collector terminal. This big current flows back to a separate power supply. An open collector driver can switch any voltage and current for the load so long as it is within the rating of the transistor.

The Open Collector driver, with an indicator LED, can be made on a breadboard, as in the picture diagram.

ThingatronOnly_bb1_ea3a0a84c79e58ffc9c8ddd42b4f876544005e5b.jpg

Thingatron4_403a060a9faeb5c7cf297d467cd91316fa6515d0.jpg

The Thingatron

As I need them a lot, I designed a PCB and have called it a Thingatron. It has screw terminals for the power and the load.

Related articles

This Thingatron mini project is provided as an addition to my WineTime project. See the related 'Battery Switch' mini-project too:

I am an inventor, engineer, writer and presenter. Other stuff: Royal Academy of Engineering Visiting Professor of Engineering: Creativity and Communication at Brunel University London; Fellow of the Institution of Mechanical Engineers and have a PhD in bubbles; Judge on BBC Robot Wars.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments