DesignSpark フォーラム
このフォーラムでは、世界中のDesignSparkに登録しているメンバーと様々な技術的相談や、議論を行うことができます。また、自身のアイデアに賛同してくれるエンジニアを、世界中から探すこともできるでしょう。
英語の投稿が目立ちますが日本語の質問でも問題ありません。よく海外から片言の日本語で回答を頂いたりします。自動翻訳レベルでも結構ですのでグローバルなユーザとのコミュニケーションをお楽しみください。
YoutubeでDSMの使い方を勉強しています。
【DS Mechanical】MISUMI-VONAのCADデータを活用する(DesignSparkJP Official)https://www.youtube.com/watch?v=3t02UJK5Tmk
で、3:00から台車のハンドル部分を延ばすデモを行っていますが、同じ操作が出来ません。
まず、ドラッグしても同じ様ななオブジェクトが選択されません。移動しても台車全体が移動して、ハンドル部分が伸びません。
どういう操作をすれば、同じような操作が出来るでしょうか? 初歩的な質問ですが、モデリングした部品の寸法を編集するのに、その部品の設計履歴の表示方法が知りたいです。スケッチの寸法を修正したり、押し出しの長さを変更したりしたいのですが、見つけることができません。もしかしたら、プランによって機能が制限されていたりしますか?私はEXPLORERを使用しています。よろしくお願いします。
Designspark Mechanical 6.0.3 can not Run with Win11,input User Name and Password show this massage,who know this problem?
In recent years, the rapid advancement of technology has given rise to a new era called "Industry 4.0." This industrial revolution focuses on automating processes through advanced robotics, artificial intelligence (AI), machine learning, and IoT devices. One essential component in this transformation is the Industrial AIoT Computer - an all-in-one device that serves as the brain of smart factories and production lines. In this article, we will explore the purpose and application of industrial AIoT computers from a professional perspective to understand their significance in today's fast-paced world.
1. What is an Industrial AIoT Computer?
An Industrial AIoT computer is a compact, ruggedized device that combines various functionalities such as computing power, connectivity options, and data processing capabilities. It serves as the central hub for IoT devices in industrial settings, allowing seamless communication between machines, sensors, and other equipment. The primary purpose of an Industrial AIoT computer is to facilitate real-time monitoring, analysis, and control over various processes within a smart factory or production line.
Key Features of Industrial AIoT Computers:
a) Ruggedized Design: These computers are built with durability in mind, designed to withstand harsh industrial environments such as high temperatures, vibrations, dust, and moisture. They often come equipped with IP65 or higher ratings for protection against water and dust ingress.
b) High Performance Processing: Industrial AIoT computers utilize powerful processors that can handle complex tasks like real-time data processing, machine learning algorithms, and advanced analytics. This enables them to make intelligent decisions on the fly and optimize production processes.
c) Multiple Connectivity Options: These devices support various communication protocols such as Wi-Fi, Ethernet, Bluetooth, Zigbee, and more, allowing seamless integration with existing industrial systems and IoT devices.
d) Expandability & Customization: Industrial AIoT computers often come with multiple expansion slots or I/O ports for adding peripherals like GPS modules, barcode scanners, RFID readers, etc., to cater to specific industry requirements.
e) Energy Efficiency: To reduce energy consumption and operating costs, these devices are designed with low power consumption in mind while maintaining high performance levels.
Applications of Industrial AIoT Computers:
a) Smart Factory Automation: Industrial AIoT computers serve as the control center for smart factories by monitoring production lines, analyzing data from sensors and machines, and making real-time decisions to optimize processes and increase efficiency.
b) Predictive Maintenance: By collecting data on machine performance and condition, these devices can predict potential issues before they become critical, allowing for timely maintenance and reducing downtime.
c) Quality Control & Assurance: Industrial AIoT computers enable continuous monitoring of product quality by analyzing data from sensors, detecting anomalies or defects in real-time to ensure that only high-quality products reach the end consumer.
d) Logistics Management: In supply chain management and logistics operations, these devices can track assets, monitor inventory levels, optimize routing, and manage deliveries for improved efficiency and cost savings.
e) Environmental Monitoring & Control: Industrial AIoT computers are used in industries such as agriculture, construction, and mining to monitor environmental conditions like temperature, humidity, and air quality, ensuring optimal working environments and safety standards.
Conclusion:
Industrial AIoT Computers have become an indispensable part of the Industry 4.0 revolution by bridging the gap between physical systems and digital technologies. By facilitating real-time monitoring, analysis, and control over industrial processes, these devices are helping industries transition to smarter, more efficient operations that benefit both businesses and consumers alike. As technology continues to advance at an unprecedented pace, it is essential for organizations across various sectors to embrace the potential of Industrial AIoT computers in their journey towards a digital future.
Jahone Chong
for more info
DRC does not report spacing violation. In this case, I set all spacing is 8 mil on the design technology but text-board, text-text, text-pad, text-via, component-component errors are not reported.
It looks like copper layer related issue is reported correctly. Is it normal behaviour?
Especially, if the resist mask and text overlap, it will be erased at the manufacture, so I would like to have it report an error. Do you have an idea?
I have signed up for Solidworks Electrical and now I'm trying to get my files from Designspark Electrical. Where are all the project files located? I can't seem to find them through file explorer.
Thanks, DS起動時に下記ポップアップが出て起動しません。PWを変更しましたが同じ現象です。どのように対処すればよろしいでしょうか?
There is a way to flip normals to have an stl file oriented as I want? Thanks Hi, I have made some shapes in plan view and normaly when I click on pull then on mouse over the shapes turn yellow with an arrow of direction and I can then pull the shape, I have done something and now only the vertices change colour to green and have an arrow, how do I get it to pull faces again ?
Thanks
Stuart Is anyone else having a problem ? Any <clicks> in Library manager, including <reindex> and editing any other item causes lots of network activity and then a stalling delay then a BOMB. Or, "Is it only me, Sadly, is it only me "??
I know that DS PCB needs the Internet to rego check to start. This was made clear when an Austrlain telco had a melt down. However, so far, once RS PCB is running, if I disable the Internet, then all the library functions operate correctly and enabling my PC Internet again eventually breaks the Library functions.
My question to the forum is "IS IT ONLY ME, DOES MY PC HAVE THE PROBLEM?".
Meanwhile, I love RSPCB and use it a lot.
我在使用DSM6.0.3时,草图画在中间的图转为实体图编辑时,图中间的图形总是空的,是什么选项选错了。
When I use DSM6.0.3, when the sketch in the middle of the picture is converted to a solid diagram for editing, the graphics in the middle of the picture are always empty. What option is wrong? Hi,
Is there away to run DSM (paid registered user) offline? I can only start it when online. Once in I can then use offline.....but that's no benefit initially. I'm travelling and some times don't have internet connectivity available.....it would be good to able to open DSM and make some changes or corrections.
Thanks.... I am trying to add a multilayer ceramic capacitor to my project. It is an RS stocked item 852-3782 but ModelSource does not have it listed nor does the search function find it, either searching on the RS stock number or manufacturers part number.
I tried to use the ECAD Part Wizard but it won't install without MS Office.
Thanks in advance. There is a little white + with a circle that sometimes appears at the origin, but sometimes not. How do I make it visible? PC入替に伴い、ライセンスキーをエクスポートするなどの対応は必要ですか?最近のフォーラム投稿
MisumiのCADデータの操作の仕方について
モデリングの履歴表示およびその修正
Designspark Mechanical 6.0.3 can not Run with Win11
Application for industrial all in one computer--------Jahone
DRC does not report spacing violation
Where are Designspark Electrical project files located?
登録の間にエラーが発生
stl flip normals
What Have I Done ?
Is anyone else having a problem with library editing ??
求教:草图转为实体后中间的图形总是空的
Offline use
Adding Components
Turning on the origin symbol in PCB?
PC入替に伴うライセンスのエクスポートについて