Microcontroller Interfaces: LEDs and Lamps
Updated: 14th October 2026
Key Takeaways
- MCU vs MPU: A microcontroller (MCU) combines the processor, memory and input/output (I/O) on a single chip; a microprocessor (MPU) relies on external memory and peripherals.
- Choosing a device: Match the number and types of GPIO pins and serial interfaces to the peripherals your design needs to connect.
- Driving an LED: A single LED can run directly from a GPIO pin, either sourcing or sinking current, as long as a current-limiting resistor is fitted.
- Resistor value: R = (supply voltage minus LED forward voltage) ÷ current. For a red LED on a 3.3V Pico GPIO at 4 mA, that's around 400 Ω, so a standard 470 Ω resistor works.
- Filament lamps: Lamps need more voltage and current than a GPIO pin can supply, so they are switched through a transistor, such as a power Darlington.
Sensor interfacing. From left to right: (a) Transmit and Receive ultrasonic transducers requiring a lot of interfacing hardware to make a rangefinder. (b) OTS PING))) rangefinder with on-board transmit/receive hardware and a 3-pin MCU connection. Host MCU handles time measurement and distance calculation. (c) OTS SRF-04 rangefinder with 4-pin connector. Still requires host MCU to handle all calculations. (d) OTS SRF-08 rangefinder with 5-pin connector. Communicates with host via I2C bus. Responds to range request with distance in cm or inches as required. Multiple addressable units can share the same two-wire bus.
This is the first part of a short series of articles on the basics of interfacing peripheral components to a microcontroller (MCU) based system. I’ll go through some criteria that need to be considered when deciding which chip or board is best for your application – that choice will influence the design of peripheral interfaces. But first, let’s get some definitions out of the way to avoid confusion later. By the end of this article, you'll know how to drive a single LED directly from a GPIO pin, calculate its current-limiting resistor, and switch a filament lamp using a transistor.
What Is Microcontroller Interfacing?
Microcontroller interfacing refers to the hardware and software that connect a microcontroller to the outside world. Every peripheral, whether it's an LED, a switch, a motor or a sensor, needs an interface that matches its voltage, current and signal type to what the microcontroller's pins can safely supply or read.
Simple devices connect directly to a general-purpose input/output (GPIO) pin, often with just a resistor. Others need extra components, such as a transistor to handle higher currents, or communicate over a serial bus such as UART, SPI or I2C.
| Interface Type | What It Does | Example Peripherals | Covered In |
|---|---|---|---|
| Digital output (GPIO) | Switches a device on or off | LEDs, filament lamps (via a transistor) | This article |
| Digital input (GPIO) | Reads an on/off state | Pushbuttons, switches | Part 2: Switches and Buttons |
| Power output | Drives loads that need more current than a GPIO pin can supply | Solenoids, motors, servos | Parts 3 to 5 |
| Analogue input/output | Converts between analogue signals and digital values using an ADC or DAC | Potentiometers, analogue sensors | Introduced below |
| Serial bus | Exchanges data over a few wires using a protocol such as UART, SPI or I2C | Sensor modules, displays, wireless modules | Introduced below |
CPU, MPU, MCU or DSC? Understanding the Terminology
The Central Processing Unit (CPU)
For the early computers, this was a whole boxful of valves, transistors or simple logic chips spread out on more than one board that performed the basic fetch and execution of maths and logical instructions. It did not contain any form of memory storage (apart from a few working registers and counters) and certainly no peripheral interfaces or I/O ports. Eventually, integrated circuit technology improved to the point where all the CPU functionality could be incorporated on a single ‘chip’:
The Microprocessor (MPU)
MPU devices even today, generally don’t possess any on-chip storage, with most of the pins providing access to the main internal address and data busses for the purpose of linking to high-capacity external memory, usually DDR SDRAM. The first 8-bit MPUs had 16-bit address busses yielding a maximum of 64KB of memory space, some of which was sacrificed to permit the inclusion of ‘memory-mapped I/O’. Until the introduction of the RP2040 MCU chip on the Pico board (212-2162) , all Raspberry Pi computer boards were based on microprocessor-type chips.
The Microcontroller (MCU)
Soon after the first 8-bit MPUs appeared, such as the Intel 8080, MOS Technology 6502 and Motorola 6800, it became obvious that they were never going to power serious ‘desktop’ computers (PC). Embedded control was a much better bet. That led to the development of the MCU, with on-chip program/data memory, and most important of all, latched 8-bit Input/Output Ports replacing the external data/address busses. A firm called Arizona Microchip introduced the first true MCU called PIC, short for Peripheral Interface Controller in 1976. Originally, engineers at General Instruments had designed it as a companion to a microprocessor, giving the latter I/O ports. Those engineers, realising its potential, left GI and formed the company we now call Microchip to make the game-changing PIC microcontrollers. PIC now stands for ‘Programmable Intelligent Computer’ apparently.
The Digital Signal Processor (DSP) and the Digital Signal Controller (DSC)
For the sake of completeness, I’ll just mention these two variations of the MPU and MCU respectively. Each contains special hardware and an extended instruction set to enable complex digital signal processing algorithms to be run in real-time. The Texas Instruments TMS320 family contains classic DSPs, while Microchip, who invented the term DSC, have their dsPIC ranges.
CPU, MPU, MCU or DSC? Understanding the Terminology
MCU vs MPU at a Glance
| Microprocessor (MPU) | Microcontroller (MCU) | |
|---|---|---|
| Memory | External memory chips, connected over address and data buses | Program and data memory built into the chip |
| Input/output | Added with separate peripheral chips | GPIO ports and serial interfaces built in |
| Typical use | General-purpose computers and single-board computers such as the Raspberry Pi | Embedded control, such as the Raspberry Pi Pico |
| Interfacing peripherals | Needs more supporting hardware | Many peripherals connect directly to its pins. |
Choosing the Right Processor for Your Peripherals
When choosing a processor chip for an embedded application, you have a number of things to consider such as clock speed, measured in Millions-of-Operations-Per-Second (MIPS), program and memory capacity, and what sort of peripheral devices need to be attached. It’s that last item I’ll be looking at in this series of articles on peripheral interfacing.
So, how do peripheral devices influence the choice of processor chip? Crudely, it comes down to the number of pins it has dedicated to I/O. Designing at chip-level pretty much eliminates MPUs and DSPs for the reasons outlined above. That leaves MCUs and DSCs. Nearly all the pins on these chips are dedicated to General Purpose digital I/O (GPIO), usually, but not always grouped together as 8-bit Ports. These Ports form what used to be called ‘Parallel I/O’ as opposed to ‘Serial I/O’ such as UART, SPI and I2C. Most MCUs make all these serial port formats available too, plus in many cases, USB. The third type of I/O commonly available is Analogue, taking advantage of the on-chip ADCs and DACs. When it comes to your design, it’s just a question of matching the I/O requirements to a particular device from the family chosen to meet the speed/memory specification. Two recent projects of mine involved PIC24-based interfaces with very different I/O requirements: Creed 75 teleprinter and Elliott paper tape reader. Both are custom-board designs working at chip and discrete component level, and programmed in Assembler, ‘Bare-Metal’ code.
You don’t have to work at chip level though: there are literally thousands of board-level products on the market ranging from thumbnail-sized ‘tiny’ modules, through ‘mini’ modules such as the Raspberry Pi Pico, to ‘development’ boards such as MikroElektronika’s Clicker 2 (170-8233) , the legendary Arduino series, Microchip’s Curiosity range, and of course, the Raspberry Pi single board computers.
Developing with Modular Peripheral Boards
Basic peripherals such as single-LEDs and pushbuttons are easily attached to any single GPIO pin with a minimum of extra components; perhaps just a single resistor. Analogue signals can obviously be connected to on-chip ADCs and DACs via pins designated as analogue I/O. Increasingly though, complex peripheral circuit functions such as accelerometers, gyroscopes and wireless comms, are being made available in chip form, communicating with a host processor via a serial bus. This has led to an explosion in the variety of peripheral modules available that just plug-in to development boards fitted with matching sockets. The ‘Click’ range from MikroElektronika is extensive and growing rapidly. Their MikroBUS standard sockets are not confined to their own processor boards; Microchip Curiosity (187-6209) boards feature them and adapters for the Arduino Shield format (823-1883) and Raspberry Pi Hat standard (162-3385) connectors are available. These modular systems may make development easy, but production board design will still need the engineer to understand how to interface these peripheral devices at component level. Admittedly, the effort involved in embedded application development is shifting from hardware design to software coding.
Basic Digital Output: Interfacing a Single LED
Let’s start with the simplest of display devices: the single LED (Fig.1). The host MCU is an RP2040 – the key component of a Raspberry Pi Pico module. The function is just digital, LED on or LED off, so a single GPIO pin set to be an output does the job and the only other component is a current-limiting resistor. There two ways to wire this up: (Fig.1a) with the LED anode to the GPIO pin and the cathode to 0V via the resistor, or (Fig.1b) with the anode to +3.3v and the cathode to GPIO via the resistor. Either will work, but the logic is reversed, so for circuit (a) GPIO = 1 will turn the LED on, but for (b) GPIO = 0 is required. Both designs work because the GPIO port driver is symmetrical and can either supply (SOURCE) current (a), or SINK it (b). Some older MCUs can only sink current.
Fig. 1: Two ways to connect an LED to a GPIO pin. (a) The GPIO pin sources current to the LED. (b) The GPIO pin sinks current from the LED.
Sourcing vs Sinking Current
| Fig. 1a: GPIO Sources Current | Fig. 1b: GPIO Sinks Current | |
|---|---|---|
| Wiring | LED anode to GPIO pin, cathode to ground | LED anode to +3.3V, cathode to GPIO pin |
| LED on when | GPIO output = 1 (high) | GPIO output = 0 (low) |
| Logic | Active high | Active low |
Both options work on the Pico because its GPIO pins can source and sink current equally. On older MCUs that can only sink current, use the Fig. 1b arrangement.
Resistor Calculation
This is not very critical. A small LED like this only needs a few milliamps of current to light up and the Pico GPIO current defaults to 4mA. To calculate the resistor value using Ohm’s Law R = V/I, we know I = 4mA and V = the voltage across it. V = 3.3 minus the LED forward voltage VF taken from a datasheet. LEDs have different values for VF depending on their colour. Red VF = 1.7v. For reference, Yellow = 2.1v, Green = 2.2v, Blue and White = 3.5v. For the Red LED this gives a resistor voltage of 1.6v and thus a resistor value of 400Ω. A standard value of 470Ω will do just fine. Note that the Pico current setting does not represent a current-limiter operation which would have removed the need for a resistor: leave it out and the GPIO output driver will be overloaded and probably burn out. Check out the C code that flashes the LED once per second (Code 1). Notice that it uses a useful power-saving feature as a timer: sleep_ms(500) powers down the processor core for 500ms.
Code 1: C code for the Raspberry Pi Pico that flashes an LED once per second.
Calculating the LED Resistor Value
| LED Colour | Typical Forward Voltage (VF) | Calculated Resistor (3.3V, 4mA) | Nearest Standard Value | Resulting Current |
|---|---|---|---|---|
| Red | 1.7V | 400Ω | 470Ω | About 3.4mA |
| Yellow | 2.1V | 300Ω | 330Ω | About 3.6mA |
| Green | 2.2V | 275Ω | 330Ω | About 3.3mA |
| Blue/White | 3.5V | Not possible | N/A | VF is higher than the 3.3V supply, so use a higher supply voltage switched by a transistor. |
Always check the LED's datasheet, as forward voltage varies between parts.
Basic Digital Output: Interfacing a Filament Lamp
A filament lamp interface is more complicated (Fig.2) because the lamp requires a lot more current than the GPIO pin can supply; 10 times as much in fact. Although it doesn’t need a current-limiting resistor, it does require 6v across it to light up. Hence the ‘Power-Darlington’ BJT transistor.
Fig. 2: Switching a 6V filament lamp from a GPIO pin using a BD677A power Darlington transistor.
Darlington transistors have a huge gain, so a tiny Base current will turn it full-on like a switch. They are fast too, so are frequently used as buffers between GPIO lines and high-voltage or high-current peripheral devices. The BD677A can handle a 4A current and will have no problem with this weedy torch bulb. A 12V 21W car direction indicator bulb should be within its capabilities, but the switch-on surge of any filament lamp of this size might just be too much for it.
LED vs Filament Lamp Interfaces Compared
| Single LED | Filament Lamp | |
|---|---|---|
| Supply voltage | Runs from the 3.3V GPIO output | Needs its own supply (6V in this example) |
| Current | Within the GPIO pin's drive current (4mA by default on the Pico) | Around 10 times more than a GPIO pin can supply |
| Current-limiting resistor | Required | Not required |
| Switching device | None: connects directly to the GPIO pin | Transistor, such as the BD677A power Darlington |
| Watch out for | Running without a resistor can overload the GPIO driver | Switch-on surge current in larger lamps. |
Building Your First Microcontroller Interfaces
LEDs and lamps are the simplest peripherals to interface, but they cover the basics you'll use again and again: matching a device's voltage and current to what a GPIO pin can handle, and adding a transistor when it can't. Try the LED and lamp circuits on a Raspberry Pi Pico, then share your results or questions on the DesignSpark forums.
Next time in part 2, I’ll be looking at simple mechanisms for GPIO input: pushbuttons and switches. The mechanical nature of these devices means that the interfaces require special attention to ensure reliable operation.
Explore the Microcontroller Interfaces Series
This article is Part 1 of DesignSpark's Microcontroller Interfaces series. Continue with the rest of the series:
| Part | Article | What It Covers |
|---|---|---|
| Part 2 | Microcontroller Interfaces: Switches and Buttons | Reliable GPIO input from mechanical switches |
| Part 3 | Microcontroller Interfaces: Electromagnets and Solenoids | Interface for an electromagnetic actuator. |
| Part 4 | Microcontroller Interfaces: PMDC Motors | Controlling permanent magnet DC motors |
| Part 5 | Microcontroller Interfaces: RC Servos | Positioning radio control servos |
For more on LEDs, explore DesignSpark's LED technology guides:
| Topic | Article |
|---|---|
| LED Basics | LED (Light-Emitting Diodes) Basics |
| LED Drivers | LED Drivers: All You Need to Know |
| LED Dimming | LED Dimming with Pulse Width Modulation (PWM) |
| LED Lumens | What Are Lumens? |
Frequently Asked Questions
What is interfacing in a microcontroller?
Interfacing is how a microcontroller connects to external devices such as LEDs, switches, motors and sensors. The interface matches the device's voltage, current and signal type to what the microcontroller's pins can safely supply or read.
What is the difference between a microcontroller and a microprocessor?
A microcontroller has its processor, memory and input/output ports on a single chip, so that many peripherals can connect directly to it. A microprocessor needs external memory and peripheral chips to work.
Can you connect an LED directly to a microcontroller pin?
Yes, as long as you fit a current-limiting resistor and keep the current within the pin's rating. Without a resistor, the LED can draw too much current and overload the GPIO driver.
How do you calculate the resistor value for an LED?
Subtract the LED's forward voltage from the supply voltage, then divide by the desired current. For a red LED (1.7V) on a 3.3V pin at 4m A, that's 1.6V ÷ 0.004A = 400 Ω, so a standard 470Ω resistor works.
What is the difference between sourcing and sinking current?
When a GPIO pin sources current, current flows out of the pin, through the LED and to ground, so the LED lights when the output is high. When it sinks current, current flows from the supply, through the LED and into the pin, so the LED lights when the output is low.
Why does a filament lamp need a transistor?
A filament lamp needs more voltage and current than a GPIO pin can supply. A transistor, such as a power Darlington, lets the small GPIO current switch the much larger lamp current from a separate supply.
If you're stuck for something to do, follow my posts on Twitter. I link to interesting articles on new electronics and related technologies, retweeting posts I spot about robots, space, and other issues. To see my back catalogue of recent DesignSpark blog posts type “billsblog” into the Search box above.
Comments