DesignSpark Circuit Simulator Maintenance on 23rd May at 15:00 UTC for 2 hours

Skip to main content

DSPCB - Creating "solder jumpers"

Jumper Pads

Pads can be used to provide a 'jumper' function by applying a solder bridge. These can be more compact than using a pin header with configurable jumper links. Although still user-configurable they should be used only for jumpers that the user is unlikely to need to change.

Some examples are chip address pins, 50Hz/60Hz configuration and also debugging aids for field servicing and development where you may require to isolate grounds at a common point (star point) and separate analogue, digital and power ground connections.

Many modern PCBs that provide solder jumper options often simply use standard surface mount pads. There is nothing inherently wrong with this approach, but it has been known to cause confusion and be considered a missing component!

Also, solder tends to naturally form a ball when melted so the traditional split circular pad is still considered desirable.

For solder jumpers consisting of two semi-circular copper pads closely spaced, we now illustrate how to create these.

1. From the Library Manager select the PCB Symbol Tab, select the destination library and click <New Item>.

Note you can also select the required Technology File to use for the footprint from the <Tech Files…> button or the ‘last used’ will be used.

Library Manager - PCB Symbol Tab - Select New Item

2. In the PCB Symbol Editor, add a Pad, right click and select Style.

PCB Symbol Editor - add a pad

3. Provide a name for the new style.

Select “Bullet” and enter the Width and Length you require, the Length must be a minimum of half the width (which will produce a semicircle).

Set the Hole Size to Zero and uncheck “Plated”.

Click OK to save.

Pad Style Window

4. You now have the pad as you defined.

Pad defined

5. Add a second pad and rotate and position for the required gap.

Add a second pad and rotate

6. If you require that there is no solder mask between the pads, add a shape on the Top Solder Mask layer.

Change Layer setting

7. Select the added shape and in the Properties check the “Filled” check box.

Shape Properties Settings

8. The footprint is essentially now complete, we just have to change the layers to restrict it to the top layers.

Footprint complete - simply need to restrict top layers

9. Select a pad and use the shortcut “L” to change the layer. Repeat for the second pad.

Change layer

10. Now use the “Save” icon and save to your required library with the desired symbol name.

Save to library

11. In the Library Manager – PCB Symbols tab, you can preview your footprint.

Preview symbol in library manager

12. Now create a component.

Create a schematic symbol or use an existing symbol.

From the Library ManagerComponents Tab, select <New>.

Select the Schematic Symbol and the PCB symbol and complete the text fields. Click <OK>.

Create a component

13. In the Editor, complete the Pin Mapping and then click the "Save" Icon to finalise the component which is now ready for use in all your designs.

In Editor complete pin mapping

Use the component as normal.

Using "Add Component" shows the component preview.

Add component

Here we show our example solder jumper in a schematic and translated to a PCB design.

Example showing schematic and PCB design

The component was designed for the top copper layer, simply use the Flip command to place it on the bottom copper layer.

With an Engineer subscription, DSPCB users can also control the paste mask opening using pad-style exceptions using the techniques described here:

Technical Support for DesignSpark PCB
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments