How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
Power over Ethernet (PoE) is basically a way of powering a device over a twisted pair Ethernet cable, so providing both data and power in a single cable and not needing a separate power supply next to the installed device, which makes installation much simpler and cost-effective. Devices being powered by PoE are widely found around the IT industry and include:
- IP Cameras (with pan & tilt functionality)
- Network Routers
- VoIP phones
- Wireless access points
- IPTV decoders
- Point of sales kiosks
- Industrial control systems
However, what happens if there is an issue during the installation? A fault on the cable, such as a short/open circuit or wrong connection. There may be insufficient power being provided over the network to power the device. Then identifying and troubleshooting the issue can be complex and time-consuming as often the installed device is in a remote location, but help is on hand from the new Fluke Networks Microscanner PoE as illustrated in the video below.As the video shows the Microscanner PoE has all the key features to take the guesswork out of troubleshooting:
- Shows the class of power provided over the network to determine if sufficient for the connected device
- Cable Tester, which will show the location of common faults
- Built-in tone generator for tracing wires
- Shows the speed of the Ethernet connection up to 10G
The Microscanner PoE range includes:
- Fluke Networks MicroScanner PoE (185-3021)
- Fluke Networks MicroScanner PoE Kit (185-3022)
- Fluke Networks MicroScanner PoE Wiremap Adaptor (185-3023)
- Fluke Networks MicroScanner Remote Identifier for PoE (185-3024)