Skip to main content

Building a Pi Powered Wireless Label Printer

by Andrew Back

Main17_fa40403def72fde10b8b92d42b6d8e413dbee0c5.jpg

Combining a Raspberry Pi and a Brother QL-700 to create a self-contained wireless label printer complete with an integrated web based label designer.

Every organised workshop needs labels and with the addition of a Raspberry Pi the low cost Brother QL-700 (840-6302) can be turned into a handy wireless label printer with an integrated designer.

QL Label Printers

Printer_dd7a1c359ec5014e8f7bdb2b6d5322a132b94ba3.jpg

The Brother QL label printers come in various configurations. The QL700 model is reasonably compact and can take various different sizes and types of label stock. Thanks to some neat software from Philipp Klaus, it’s now possible to drive them without needing to have official driver support from Brother — meaning that non-x86 platforms can also be used, such as the ARM-based Raspberry Pi. Which of course is perfect for a bolt-on wireless print server — and more!

Let’s take a look at how we’d configure a Pi to drive the QL-700 via a simple web interface.

Installing Raspbian and dependencies

So first we need to write out Raspbian to a Micro SD card. The Lite variant is perfectly sufficient and highly advisable (no need for desktop software etc). Assuming you used a Linux machine to write out the SD card, once this has completed if you remove and reinsert the card so that its partitions get mounted, we can edit a few files.

$ sudo vi /media/<your username>/rootfs/etc/hostname

Change the hostname to something easily remembered, like “labels”.

$ sudo vi /media/<your username>/rootfs/etc/hosts

Then update the hosts file with the same name.

$ sudo touch /media/<your username>/boot/ssh

And create the file that tells Raspbian to enable the SSH server.

Of course, feel free to replace vi with your text editor of choice.

If we now insert the card into our Raspberry Pi and apply power, after a short while we should be able to log in via SSH using mDNS. E.g.

$ ssh pi@labels.local

Alternatively, you could just attach a keyboard and monitor.

Next if we update the system.

$ sudo apt-get update

$ sudo apt-get dist-upgrade

And then install the packaged dependencies with:

$ sudo apt-get install python3-setuptools python3-pip libopenjp2-7-dev libtiff5 git fontconfig

Wireless setup

If you do want to be able to print over a wireless connection instead of wired, you’ll need to also configure the WPA supplicant. If wired Ethernet suits your needs you can skip this step.

To configure the Raspberry Pi to join a wireless network we need to edit a file:

$ sudo vi /etc/wpa_supplicant/wpa_supplicant.conf

And add configuration for the network SSID and passphrase to the bottom of the file. E.g.:

network={
    ssid="MyNetwork"
    psk="NetworkPassword"
}

Following which if we save the file and reboot it should join the network. For further details see the documentation on the Raspberry Pi website.

Brother QL printers Python package

RPLP_brother_ql_print_5f9506248688cfc24b430ed437b25911491bb896.jpg

The brother_ql Python package provides the foundations for this project and enables driving QL series label printers without the usually required printer drivers. Once this has been installed raster language files can either be generated via your own programs or from image files using the supplied command line utilities. To install this via PIP we simply enter:

$ sudo pip3 install brother_ql

Following which we can take a look at the options for the tool which creates language files which are understood by the printer, from image files, by entering:

$ brother_ql_create --help

One of the nice things about these printers is that they take different sizes of labels, with stock also available as individual labels and on a continuous roll. To list the supported sizes we enter:

$ brother_ql_info list-label-sizes

For details of the options for both of these commands see the GitHub repo.

We had the 62mm wide continuous roll supplied with the printer loaded and so created a PNG file of this width, with the DesignSpark logo centred and a small white border around it

DS_Logo_62mm-wide_Red_BG_6577a659f09af2e94ea1dd212fabe9bcbc9f0960.jpg

Note that the red background wasn’t present in the image printed and this has just been added to show the image used to scale.

The printer language file was then created with:

$ brother_ql_create --model QL-700 DS_Logo_62mm-wide.png --label-size 62 > DS_Logo.bin

In order to access the printer ports we need to be in the “lp” group and we can add the pi user account to this with:

$ sudo usermod -G lp -a pi

Following which it is necessary to log out and then back in again.

Finally, we can print the generated .bin file with:

$ brother_ql_print DS_Logo.bin /dev/usb/lp0

DS_Logo_bd9cd2e69f07c6aaf9b214ba6d4559327a886a4d.jpg

With the label printed and length cut according to the size of the image file.

Web service label designer

RPLB_Hello_DesignSpark_05c6ffd739cac313973180f525df87f4423e14db.jpg

The author of brother_ql has created a very cool piece of software that builds on this to create a standalone web-based label designer, meaning that you can simply point your browser at the Pi, enter some text, set the font and label parameters, and print! To install this we:

$ mkdir src

$ cd src

$ git clone https://github.com/pklaus/brother_ql_web.git

$ cd brother_ql_web

$ sudo pip3 install -r requirements.txt

$ cp config.example.json config.json

It’s then necessary to edit config.json to set the printer model, along with default label size and fonts etc. It’s also worth changing the server port setting to 80 so that you don’t have to remember some non-standard port number to enter as a URL suffice.

Following minimal configuration we can start this with:

$ sudo python3 brother_ql_web.py

Pointing a browser at the pi — e.g. http://labels.local — we should get the user interface and be able to enter text and print.

DS_Text_66061550b0191b5a0881fa9ed347c297f69a3287.jpg

Final touches

If we’d like this to start automatically at boot we just need to edit /etc/rc.local and before the exit 0 line add:

cd /home/pi/src/brother_ql_web; /usr/bin/python3 brother_ql_web.py&

Finally, more often than not with something such as this we should configure the Pi such that upon boot it mounts the root filesystem read-only, otherwise we risk filesystem corruption if power is removed without the Pi getting shut down properly. There are various guides that detail how to do this, but one particularly easy solution is to use the rpi-readonly script.

$ git clone https://github.com/ways/rpi-readonly.git

$ cd rpi-readonly

$ sudo ./setup.sh

This does actually make some serious changes and so, as noted in the GitHub repository, it pays to make a copy of the SD card first.

— Andrew Back

Open source (hardware and software!) advocate, Treasurer and Director of the Free and Open Source Silicon Foundation, organiser of Wuthering Bytes technology festival and founder of the Open Source Hardware User Group.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments