How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
The NEX10 what it is, what it does, and how it can help you?
The NEX10 is the new connector interface for PIM stability designed in collaboration with leading manufacturers.
Okay, sounds good (I think), so what is PIM? For those like me who had heard of PIM but didn’t really understand the implications, simply click the image below for more information.
Image source: https://www.anritsu.com
The NEX10 has been specifically designed to help the whole PIM issue and with manufacturers like Radiall, Huber & Suhner and Rosenberger you can be sure a lot of research, design, testing and re-testing went into this product to ensure the parts do indeed do what they are designed for.
Premeditated to Meet the Demands of Approaching 5G Networks
Main features of the NEX10 as stated is the PIM stability but it also has additional features that can also help with your applications.
Below is the technical stuff!
- Tough and reliable performance for outdoor use
- Dependable performance eradicating installation errors
- Enhanced for ¼inch cable
- Outstanding return loss and electrical performance
- Interface safe from installation damage
- Flexibility in installation
- Low PIM independent of coupling mechanism
- Operating frequency up to 20 GHz
- Small size, flange height of 12.7 mm
- Protection of contact area
What applications do I hear you ask?
- In small cell applications
- NEX10 is particularly suited for challenging space restrictions and electrical performances requirements
- In low power base stations, NEX10 can be used for interconnections in the remote radio head as well as an interface on the antenna and on the jumpers
- In multi-operator/multiband DAS, the NEX10 can be used where RF signals have to be combined, terminated, or distributed to the antenna
- Blind mating for panel-to-panel and test and measurement
- For dense applications, the multi-coax will offer the best solution with four signal lines in one connector
- For more information see the links and video below.
NEX10 - the new low PIM, small size and robust interface
https://www.radiall.com/products/rf-coaxial-connectors/quick-lock-and-secure-connectors/nex10.html
See the latest offer from RS Components below
NEX10 Straight Plug Screw-on |
||
NEX10 Push-pull Plug |
||
NEX10 Straight Jack with Flange Solder |
||
NEX10 F Bulkhead Jack Solder |
||
NEX10 Rectangle Flange Receptacle |
||
NEX10 Straight Plug Screw-on |
||
NEX10 Push-pull Plug |
||
NEX10 Straight Jack with Flange Solder |
||
NEX10 F Bulkhead Jack Solder |
||
NEX10 Rectangle Flange Receptacle |