Skip to main content

CAD in the automotive industry

by DesignSpark

CAD in the Automotive Industry: How Car CAD Software Works

Updated: 21.08.2026

Key Takeaways


  • What it is: CAD (computer-aided design) software in the automotive industry allows car designers to create precise 3D models, simulations, and visualisations of vehicles throughout the full design process.

  • History: Automotive CAD dates to Pierre Bézier's UNISURF program in the 1960s. By 1968, Peugeot had used it to design the complete bodywork for its 204 model.

  • Key uses: Body concept design, component modelling, 3D printing integration, real-world visualisations, and multi-team collaboration.

  • Get started: DesignSpark Mechanical Explorer is free to download. Upgrade to Creator or Engineer for advanced design features.

It's fair to say that the last few years have been a bumpy road for the automotive industry. The COVID-19 pandemic and ensuing semiconductor chip shortage around the world had a massive impact on both manufacturing and sales. Even at ground level, people were using their cars less, with no reason to drive anywhere.

Recently, however, the car industry is seeing a real return to form. Demand is growing every month, prices in the used car market are flying and people are back using their vehicles regularly again. With the pandemic-driven panic over, the industry is looking forward to the next paradigm shift in its timeline: the mass introduction of electric cars as petrol, diesel and even hybrid models are gradually phased out.

Alongside the ever-more impressive technology of electric vehicles (EVs) is the increasing sophistication of computer-aided car design. At the heart of this side of the industry is specialised computer-aided design (CAD) software – but what’s the story of CAD in the automotive industry?

What is CAD in car design?

CAD plays an essential role in automotive development. 3D CAD enables car designers to produce precise geometric information and accurate data on the configuration of the model's modules and systems. CAD can be used for every step of the car designing process, from body concepts through to product assemblies, as well as real-world visualisations and simulations to enhance creator and client understandings of the design.

CAD as we (roughly) know it now has been around in the industry since the 1980s and has naturally become the central design basis via which all car concepts are produced. Today, it's more advanced than ever, allowing car designers to explore more digital design possibilities than ever before.

What's the history of automotive CAD design?

While 'modern' CAD modelling surfaced in the industry in the 80s, the history of CAD in the automotive market dates back to the 1960s and a pioneering French designer called Pierre Bézier.

Bézier began working for French auto giant Renault in 1933. In the late 50s, he started to push Renault to invest in researching numerical controls for car body tooling and modelling – a suggestion which was initially rejected before interest in tech-assisted design started to grow through the 1960s.

During that period, Bézier was designing the first CAD software for cars: UNISURF. UNISURF used a tape-based computer to create ink drawing and tooling concepts for car bodies using infinitely scalable parametric curves coined Bézier curves. The introduction of the Bézier curve allowed engineers to replicate the complex curvature of car bodywork via computer design and, by 1968, Peugeot (which had a R&D agreement with Renault) had utilised UNISURF to design the complete bodywork for its new 204 model.

By the 1980s and the rise of early desktop computers, automotive CAD software had advanced to beginnings of what we know it to be today, offering the ability to create, model, analyse and edit designs.

How do car designers use CAD?

CAD is key to today's automotive sector, in which modelling and designing are two fast-moving and constantly changing disciplines. One of the biggest ways in which CAD is impacting the design element of the process is via 3D printing, which is allowing car designers to create layer-by-layer builds that are more complex and detailed than ever before.

Using 3D printing off the back of automotive CAD software's 3D modelling capabilities has enabled various improvements, such as the rapid production of multi-iteration prototypes to reduce the car's weight and create bespoke designs for custom models.

There are also the increasing real-world capabilities of CAD – i.e. the ability to offer accurate visualisations and simulations within 3D modelling – to consider. Design elements like these are enabling automotive manufacturers to collaborate better throughout the design, allowing for process improvements like quicker revisions and virtual-reality demonstrations for internal collaborators and clients.

 

Automotive CAD Software: Which Type Do You Need?

The automotive industry uses a range of specialist CAD software depending on the stage of the design process and the scale of the project. Unlike general-purpose CAD tools, automotive CAD programs typically include industry-specific databases of materials, tolerances, and component specifications to support the demands of car design.

Software Type

Best For

Cost

Free 3D CAD (DesignSpark Mechanical Explorer)

Designers getting started with 3D modelling and concept visualisation

Free

Mid-tier CAD (DesignSpark Creator)

Intermediate automotive design with advanced 3D modelling and engineering drawings

Paid subscription

Professional CAD (DesignSpark Engineer)

Full professional automotive design with complete drawing and annotation tools

Paid subscription

What are the benefits of using CAD to design a car?

CAD in the automotive industry has undoubtedly had a massive impact for businesses that have adopted it over the last few decades. As the technology advances, it's continuing to boost key performance metrics for the organisations using it, from speed of production to bottom-line costs.

Benefit

What It Means in Practice

Faster, more efficient designs

High-quality designs are easier than ever to build; concepts reach market quicker, and production windows shrink

Improved accuracy

CAD eliminates human error earlier in the process, addressing safety and quality concerns before physical modelling begins

Better collaboration

Teams across the world can work together, log updates, and address revisions in real time

Customisation and design scope

Greater flexibility to push design boundaries and create bespoke models with unique USPs

Cost-effective

Faster, more accurate, more collaborative processes reduce costs; removing physical 3D models also provides environmental benefits

Faster, more efficient designs made simple

One of the most obvious benefits of automotive CAD is the streamlining of the design process. High-quality designs are easier than ever to build and, likewise, the process required to make them is only getting quicker. That means that concepts can be brought to market quicker and windows of production can be minimised.

Improved accuracy

Car designers are naturally accurate professionals with excellent attention to detail. Despite this, however, human error can never be removed entirely from the manual design process. Automotive CAD software allows users to create highly accurate models of parts before anything is even thrust into a 3D model, meaning that any safety or quality-control concerns can be addressed earlier in the process, design faults are eliminated and standards of production are higher across the board.

Better collaboration

Car design is a hugely complex, multi-stage process that requires numerous designers with different skillsets to work together to deliver the final product. With CAD, designers can work together more easily, logging updates, quickly addressing revisions (which are minimised in the first place via the software's improved accuracy) and communicating with fellow team members – and all from anywhere in the world.

Customisation and design scope

CAD allows for great flexibility and optionality in design, giving car designers more scope to customise designs, further push the envelope and seek out new USPs for their car models.

Cost-effective

The bottom line for every business, the faster, easier, more collaborative and error-free process that CAD offers naturally leads to cost benefits for any business. Removing the need for physical 3D models without any loss of detail, automotive CAD software also offers environmental benefits that tie into the cost-saving.

CAD Across Industries: More from DesignSpark

CAD software is used across a wide range of industries beyond automotive. Explore our full series of CAD use case guides below. You can also read our guide to the top 3D CAD software solutions on the market.

 

Industry / Use Case

Guide

Architecture

CAD in Architecture: How It Works and Benefits 

Construction

CAD in Construction 

Civil Engineering

The Use of CAD in Civil Engineering

Mechanical Engineering

CAD for Mechanical Engineering

Electrical Engineering

CAD for Electrical Engineers

Building Design

CAD Software for Building Design 

Manufacturing

The Use of CAD in Manufacturing 

Interior Design

How is CAD Used for Interior Design?

Jewellery Design

CAD for Jewellery Design

Fashion Design

How is CAD Used in Fashion Design?

Rapid Prototyping

How is CAD Used for Rapid Prototyping?

Download DesignSpark Mechanical Explorer for free today

You can get started with our CAD software right now for free! Download DesignSpark Mechanical Explorer to see what our basic CAD package looks like, then upgrade to Creator or Engineer to get a host of advanced features.

If you want to know more about what our CAD software has to offer, you can learn the basics of DesignSpark Mechanical here or take a look at our support FAQs and Mechanical forum to get all the answers that you need.

Download DesignSpark Mechanical Explorer for free

Sign up to DesignSpark Mechanical Creator today

Sign up to DesignSpark Mechanical Engineer today

 

Frequently Asked Questions

What is automotive CAD software?

Automotive CAD software is a specialist computer-aided design software used by car designers and engineers to create 2D drawings and 3D models of vehicle components and assemblies. It enables designers to model everything from body panels and interior components through to mechanical systems and electrical architectures, all before any physical prototype is produced.

 

Modern automotive CAD programs include industry-specific material databases, tolerance specifications, and simulation tools tailored to vehicle development.

Which CAD programs are used in the automotive industry?

The automotive industry uses a range of CAD programs, depending on the organisation’s size and the project’s complexity. Large OEMs and Tier 1 suppliers typically use enterprise-grade specialist automotive CAD platforms. 

 

For designers and engineers looking for a free or low-cost starting point, DesignSpark Mechanical provides 3D CAD capability suitable for automotive design work, from concept modelling through to detailed component engineering. DesignSpark Mechanical Explorer is free to download, with Creator and Engineer subscription plans available for more advanced features.

How is CAD used in car design?

CAD is used throughout the entire car design process:

 

  • In the early stages, designers use CAD to explore body concepts and proportions, quickly creating multiple iterations. 

  • As the design develops, CAD is used to model individual components and assemblies with precision, identify potential conflicts or weaknesses, and run virtual simulations. 

  • 3D printing — driven directly from CAD files — is widely used to produce rapid physical prototypes. 

  • In the final stages, CAD supports production planning and the handover of manufacturing data.

What are the benefits of CAD in the automotive industry?

The main benefits are faster design cycles, improved accuracy, better multi-team collaboration, greater design flexibility, and lower costs. 

 

CAD removes the need for expensive physical 3D models at early stages, allows revisions to be made in minutes rather than days, and enables real-world visualisations and simulations that were previously impossible. 

 

For the automotive industry specifically, CAD also plays a critical role in meeting safety standards and regulatory requirements by enabling precise tolerancing and virtual testing.

Is there free automotive design software?

Yes. DesignSpark Mechanical Explorer is a free 3D CAD download suitable for automotive design work, including component modelling, assembly design, and STL file creation for 3D printing. It requires a free registration to access. 

 

For more advanced automotive design capabilities, including engineering drawings, annotations, and extended modelling features, Creator and Engineer subscription plans are available. 

 

RS DesignSpark is the go-to platform for professional design engineers, providing application and product content and design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments