I have a Sony TC377 Tapedeck (1973 Apx) and i want to replace the motor run capacitor, the one that is on there is an aluminium can type about 30cm x 60cm. The rating says 1.5uF and 0.5uF it has three terminals one is bridged, it is a 250v A/C. Does it matter if the repacment is higher than 250v and is this a permanant split capacitor or can i just replace it with a 2uF? I have looked on your wedsite and have pick out 3 possibles. R.S.Pro 196-4646. Kemet 377-8740. Epcos 200-9283. Can you recomend one. Thanks Mike
Share this post