How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
The new innovative electrical measuring instruments from Testo offer a high level of user-friendliness, setting new standards with intelligent and completely new technology. Digital multimeters with automatic measurement parameter recognition, clamp meters with a unique grab mechanism and Bluetooth or voltage testers which also measure current.
The digital multimeter testo 760.
Recognize measurement parameters automatically.
testo 760 eliminates incorrect settings, because the measurement parameters are detected automatically via the assignment of the measuring sockets and also shown by the illumination of the appropriate function keys. Function keys replace the traditional dial, which means easier operation and greater reliability.
Order information:
905-5885 testo 760-1 Digital Multimeter
905-5888 testo 760-2 Digital Multimeter
905-5882 testo 760-3 Digital Multimeter
The clamp meter testo 770.
Grab cables without touching.
The testo 770 clamp meter family is ideally suited for current measurement in switching cabinets. One of the two pincer arms can be fully retracted into the instrument. This unique grab mechanism means that cables in tight switching cabinets can be easily grabbed. The automatic measurement parameter detection also ensures reliable work: in the current and voltage area, all three instruments detect direct and alternating current and select other parameters such as resistance, continuity, diode and capacitance automatically, while the testo 770-3 also offers Bluetooth with a free Testo App for Smart Phones.
Order information:
905-5891 testo 770-1 Clampmeter
905-5894 testo 770-2 Clampmeter
905-5898 testo 770-3 Clampmeter
The voltage tester testo 750.
Comfortably legible from any position.
The testo 750 voltage tester family includes the first instruments with an all-round LED display. The display can be seen from any position and guarantees an ideal voltage indication thanks to its unique fiber optics. All three models meet the latest voltage tester standard EN 61243-3:2010 and have a safety specification according to CAT IV. They have the most important functions for voltage testing, continuity testing and rotating magnetic field measurement.
Order information:
905-5866 testo 750-1 Voltage indicator
905-5860 testo 750-2 Voltage indicator
905-5879 testo 750-3 Voltage Indicator
The current/voltage tester testo 755.
The first voltage tester measuring current.
They are the first of their kind: voltage testers which meet the latest standard and which can also measure current. This means the two instruments are suitable for virtually all daily electrical measuring tasks. Each time they are used they automatically select the right settings and therefore prevent dangerous incorrect settings. Both models have all the important functions for determining voltage/deenergization, for measuring current and resistance, as well as for continuity tests. Their measuring tips can be changed easily, so that the whole instrument does not need to be replaced in the event of damage.
Order information:
905-5872 testo 755-1 Voltage indicator
905-5876 testo 755-2 Voltage indicator
The non-contact voltage tester testo 745.
Filters high-frequency interference.
The testo 745 non-contact voltage tester with a measuring range of up to 1,000 V is particularly well-suited to fast initial checking of any suspected fault sources. When the presence of alternating voltage is determined, the testo 745 gives a warning via a clear visual and acoustic signal. In order to increase the reliability, the voltage tester has a filter for highfrequency interference.
Order information:
905-5863 testo 745 Non Contact Voltage Indicator