After you launch the software, you should see a 'Quick Guide' tab to the left. Within here there are step-by-step instructions to create your first design and get familiarised with the basic functionality. Also visit our support centre to see our library of video tutorials. Click Here for Video Tutorials.
Can I run DesignSpark Mechanical on a virtual machine?
Users report successfully operating DS Mechanical on VMware Workstation 7.x and Player 3.x, Oracle Virtual Box 4.3 and higher.
Our DesignSpark software is available for use by registered DesignSpark members. The software will periodically check that the user is still registered on DesignSpark, if the software can not verify the user i.e. there is no internet connection, then it will continue trying for 30days and then give notice that the software will stop working after a further 30days. It is therefore recommended that the system is connected to the internet at least once every 30 days to ensure seemless usage.
How do I import an ECAD file like IDF or EMN from DesignSpark PCB or another software?
An IDF exported from DSPCB comprises of two files - IDB (board file) and IDL (library file) Make sure to always keep the IDB and IDL in the same folder. To open in DSM, select only the IDB file.
Edits will always be saved in DS Mechanical's native format of RSDOC.
Does the license for the add-on modules expire?
There is NO expiration date for any of the licenses (Exchange, Drawing or the bundle) you have purchased. However, it is essential to remember that the add-on modules come with 12 months maintenance package included in price, which gives you access to any enhancements to the premium functionality, bug fixes, etc.