Skip to main content

How can I add power & ground symbols to a schematic?

This tutorial requires:

DesignSpark PCB V11.0.0

Power and ground symbols are used in the Schematic to indicate a connection to a power source. These symbols are required for aesthetic purposes and are not translated to the PCB (because they do not have PCB footprints associated with them). The signals they represent are connected together at the translate stage by ‘implied’ connectivity. The power & ground symbols themselves can contain inherent net name properties that are automatically used when the symbol is attached to the net.

066e0ddd20cef23fdd200aac20ccb5585d463ddc.png

1. Adding power symbols

You can add power symbols by using the Add Component browser on the Interaction bar <F9>.

963366eb31c1e07b84286ae1d2723634bb8da43a.png

Select the Schema library from the drop-down list. For reference, this is a schematic only component library and will not have any PCB symbols associated with them.

In the Component list select 0V. You will see the symbol selected in the preview box. Remember, all these symbols have no PCB Symbol associated with them, they are Schematic-only symbols.

Drag the 0V symbol into the design from the browser.

e7abfb9f5d252f69ee288d084fc93bfbb75985bc.png

Connect it by dragging off the symbol to the existing connection. A confirmation dialog will be displayed to indicate a non-named net is being connected to a named net. This ensures you aren’t joining nets which you don’t know about.

d5aa7e52ecc512430518557f06aa0cab38da1272.png

2. Adding ground symbols

You can also add a ground symbol by using the Add Component browser on the Interaction bar <F9>. Select the Schema library from the drop-down list. For reference, this is a schematic only component library and will not have any PCB symbols associated with them.

In the Component list select GND. You will see the symbol selected in the preview box. Remember, all these symbols have no PCB Symbol associated with them, they are Schematic-only symbols.

f4db60997da69cd2b10351d282d68feca4ad39d9.png

The rest of the steps of connecting the symbol to an existing circuit are the same as the power symbol.

RS DesignSpark is the go-to platform for students, makers, hobbyists and professional design engineers, providing design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software. Join the community today at https://www.rs-online.com/designspark/register
DesignSpark Electrical Logolinkedin