DESIGNSPARK FORUMS
Communicate freely with other DesignSpark members via the forums area. Create new conversations or join existing discussions about products, technology, software, and future innovation.
Help to provide solutions or seek answers to your own technical problems by calling upon a global network of like-minded engineers.
I very often have a geometry error when loading rsdoc in DSM v6 (Right click on a solid -> Check Geometry).In version 5 there were still no geometry errors.
基準の線から、角度を決めて線を引きたいが、基準としたい線からの角度が表示されない。
添付ファイルのように、外角を指定したいが、内角からしか指定できない。
Hi all, is it possible to re-order the drawing sheets? I'm trying to drag sheet 13 up between sheets 4 and 5.
I want to know how to dispaly the net name on PAD?
Kind regards
C.C. We bought an Upgrade to Premium DSM 5 from RS-Components.
(export STEP-files)
After updating to DSM 6, this upgrade does not work anymore.
Any trial to contact any service leaded to no answer!
Would be pleased for any hint how to go on now. - THANKs Mike Ich hab' schon vielfach versucht, die Konturlinien etwas "dicker" auszudrucken, so dass sie deutlicher im Druckbild erkennbar sind. Alles was ich bisher versuchte, war ergebnislos. Weder über die Layer-Eigenschaften noch über globale Eigenschaften mit den Liniendicken konnte ich eine Änderung erzielen. Was mache ich falsch? First I could not log on and then when i could i cannot load drawing sheets that have be made. Need help. ソリッドをトリプルクリックすると、全体が朱色になっていたが、
突然、エッジだけが表示されるようになった。
何処の設定を戻せばよいでしょうか?
Been using both Desgin Spark PCB and Mechanical since version 1.0. Now I go to use both of them today and I can't even log in to send a complaint that my license can't connect to the backend server. I'm attempting to use the latest versions PCB 11.0 and Mechanical 6.0, both Explorer for now... I don't see how I be justinfied to put any money into a product that's completely broken with no way to contact support for resolution. To top it off I can't even get version PCB 10.0 to work so I can attempt a port of several old projects that are still alive to 11.0. If anyone can help it would be greatly appreciated. Hi, trying to open DS mechanical, and I get a licensing backend connection error.
When might this issue be resolved? I work with 3d scans of small to medium sized objects and need to edit them as solids to reverse engineer mounting points, clearances, etc. Using a high end scanner and software the mesh outputs are great quality and watertight. In v5 i could convert .obj to solids and while it was a little slow even on a very high spec PC it worked. Now V6 is out and i paid for the advanced versions to keep .obj import and covert to solid capabilities but it freezes the software everytime I try. Processor usage goes to 90% for 30 seconds and then drops to 10% with no recovery even if left for 1hr or more on a fairly simple object. Salve, qualcuno mi puo aiutare a capire perchè non riesco più ad accedere a designspark eletrical, inserendo e-mail e password mi da errore sconosciuto.
Era un po di tempo che non lo utilizzavo ed è un bel programma mi trovavo benissimo.
Grazie spero di ricevere qualche risposta. Is creator the same to create/make threads internal/external as on explorer, or does the subscription creator enhance that? I can't seem to find that before I make decision to subscribe. I would like to place a 3D view on my drawing sheet. The default isometric or trimetric views show the assembly from the wrong side, hiding all the detail.
Is there a way to specify which direction the model is being viewed from in the view?
What I want:
What I get:
Really simple, i create text on a 3D object (annotation plane on a solid) and as soon as i click the "project" button Designspark freezes. After a few second the application crashes. I tried .OTF and .TTF fonts, both crash.
I watched tutorials on youtube to ensure i did exactly the same as others, who succeeded in making 3D Text this way. I would import my text as vector or any other filetype but you guys decided to remove that option in November last year...
[System: Win10, i9 9900k, 9/32GB Ram used, 150GB Free on C: Drive where DSM Explorer resides]New Posts
Geometry error on solid after loading rsdoc in DSM V6
基準の線からの角度を指定して線を引く
Re-order Drawing Sheets
How to dispaly the net name on PAD?
RS Upgrade to Premium DSM does not work for actual new version DSM6 anymore
Konturlinien beim Ausdruck verstärken
Drawing sheets
Solidの表示がエッジだけ
Can't connect to licensing backend?
Server down?
Convert to solid unusable in v6.0
Non riesco più ad accedere a DSE
making a thread on creator
3D Sheet View Direction
V6 crashing when projecting text