Skip to main content

Debug IOT2020 C++ Program with Eclipse Neon and Windows10 64-bit

by jancumps (No longer a member)

The standard Remote Debug doesn't work for me in Eclipse Neon. It's a known situation.
I have a process to get it working though. It's not as streamlined, but you have the full debug powers.

What works:

  • stepping through code
  • viewing variables & expressions
  • the typical things you do in a debugger.

What doesn't work (yet?):

  • uploading the binary to the IOT2000 when you start the debug session
  • automatic start of the GDB server on the linux side
  • redirecting output to the Eclipse console
  • automatically find the correct path of every source file when stepping trough code

None of the "doesn't work" topics is a showstopper. There's a replacement technique that covers each of them.

 

 

 

 

 

 

 

Additional software

You'll need to have the Cygwin version of the GDB executable installed on your Windows PC. The poky version in the Siemens SDK (and the mingw and linaro versions that I tried) don't work well together either with Windows10 64-bits or the GDB server on the IOT2000. This GNU Debugger isn't installed by default when you install Cygwin. Select it during the installation. It's available under the Devel tree:

 Change Skip to Install to get it as part of Cygwin.

You also need WinSCP or another means to transfer files to the IOT2020.
That's all there is to install. Let's go over the debug cycle now.
I'm assuming that you have the SDK example from Siemens loaded and built. Let's go trough the steps.

 

Move the binary to IOT2020

The default GDB debugger configuration does that for you. It also sets the executable flag. This fails when using Eclipse Neon on the IOT2020. We'll use WinSCP to do both tasks.

 

 

Start WinSCP, enter ip and credentials of your IOT2020 and connect.
Navigate to the project folder of your development PC and find your compiled binary (in the Release folder of your project). Even though the project says it's a Release version, the Siemens SDK sets the -g3 option of the compiler. That means that all symbolic info needed for a debug session is available in the binary. On the right side, navigate to your Linux ProjectFolder directory. Copy the file over (if asked select binary mode).
When copying is finished, right click on the destination file and select properties. Set the executable flag.

 Start the Remote Debugger

Open an IOT2020 Linux shell (via PuTTY or your personal favourite serial comms program). Navigate to the ProjectFolder directory and execute the following command:

> gdbserver localhost:2000 ./HelloWorld

The debug server will patiently wait until you start your debug session in Eclipse on your PC.

 Create a Debug Configuration in Eclipse Neon

The last step. We'll set up the client side and launch the debugger.

 

 

 

 

 

 

 

 

 

 

You create this via the Run -> Debug Configurations... menu
Create a new Remote Application debug configuration (either by right-clicking on the parent node or using the New button at the top of the dialog.
Give the config a meaningful name, end select the project (use the Browse... button for that).
You can let Eclipse fill in the Application by pressing the Search Project... button. At the bottom of the dialog, change the GDB Launcher from Automatic to Manual Remote Debugging.

 

 

 

 

 

 

 

 

 

Switch to the Debugger tab, and in the GDB debugger field, browse to the Cygwin GDB executable that you've installed earlier on. Double-check if the "Stop on startup at main" checkbox is ticked.

All other GDB binaries that I tried, from MingW, Linaro or the Siemens SDK either failed to load, didn't get a stable connection with the server side GDB, or didn't stop at main. I love to be corrected on this particular issue. It may be me.

 

 

 

 

 

 

 

 

 

 

Then in he Connection subtab, select TCP. Enter the IOT2020 ip address and the same port number you used to kick off the GDB server in Linux (2000 if you followed my steps).

Apply, then click the Debug button. Enjoy!

Other things

If you write text to stdout in your program, it will appear in the PuTTY session you used to cick off the debugger. The standard CDT remote launcher manages to redirect it to an Eclipse console.
When stepping trough the code, the debugger sometimes can't find your source code. Use the Locate Source File button that appears in that case to select your source. This seems to be related to using the Cygwin debug client while not in a Cygwin shell. It thinks that your code is in /home/drive/d..... , a construct that only works when you're inside a Cygwin shell.

But: the debugger works!

 

jancumps (No longer a member)
This person is no longer a member and their bio is unavailable
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments