こちらの記事について、内容・翻訳・視点・長さなど、皆様のご意見をお送りください。今後の記事製作の参考にしたいと思います。
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
こちらの記事の感想をお聞かせください。
Dremel, founded in 1932 by Albert J. Dremel, is known worldwide for being the creator and manufacturer of high speed rotary tools. Dremel Markets the first handheld, high-speed rotary tool called the Multi-tool. Today, the Dremel brand has earned a reputation for quality and performance among do-it-yourselfers and hobbyists.
The Dremel 3D Idea Builder is a ground-breaking addition to the Dremel product portfolio, compared to its usual product line. This makes it one of Dremel’s most innovative and inspiring products in the company’s recent time.
An easy and convenient way to turn your ideas into objects.
- Ready to use straight out of the box
- Easy-to-operate system, intuitive software for adapting and designing models
- Eco-Friendly build material and a large printing surface for custom designs
Features:
- Over 100 print templates from which you can choose your favourite model – available on the Dremel UK website.
- Printer uses PLA, eco-friendly plant based plastic – comes in form of spools.
- Filament comes in 10 colours – in black, white, translucent white, blue, red, green, orange, violet and metallic gold or silver.
- Printer melts and prints the filament and creates an object layer by layer – applying ultra-fine layers up to 100 micrometres in thickness (0.1mm).
- Build chamber is protected by a transparent door that keeps out contamination such as dust and hairs while printing is in progress.
- The chamber also acts as a sound insulator for the blower which controls the temperature inside the unit.
- Removable build platform – Dimensions are 23 x 15 x 14 cm.
- A build tape affixed in the platform holds the models in position during printing and stops them from moving.
- 3D printer has an in-built full colour touchscreen, allowing you to preview your builds in optimal detail.
- In built SD card reader with a maximum storage of 32GB – allowing you to transfer print files conveniently from your PC/Laptop.
Specifications |
Dremel 3D Idea Builder |
Maximum build resolution |
100 µm (0.10 mm) |
Maximum print size (length x width x height) |
23 x 15 x 14 cm |
Data transfer |
SD card, USB cable |
Size (length x height x width) |
48.5 x 40 x 33.5 centimetres |
Weight (excluding filament) |
8.85 kg |
Recreating the Favourite Landmarks of London
Dremel recreated some of London’s most loved landmarks with precision. The architectural icons included Big Ben, Tower Bridge and St Paul’s Cathedral, which were all recreated in a 3D model format with high detail.
“We wanted to show what 3D printing, and this printer in particular, is capable of.” And to “inspire people to see the possibilities for themselves”
“Crafting replicas of some of Britain’s best-loved buildings and photographing them like this is just one way we can really show the capabilities this technology has to offer, even on a small scale.”
“The only limit is your imagination and we’re encouraging everyone, whether they are a keen crafter, DIY-er, specialist designer or simply a family who want an appliance that can make them anything that they can think of, to get printing… and build on their ideas.”
Each finished model, when printed using the Idea Builder, is easily removable from the platform. The model will be strong but lightweight, allowing you to sand it down for a smoother finish, paint it for a more “realistic” feel, or add something creative of your own for a more personalised touch.
Available in the following regions
BUY A Dremel 3D Printer- France
BUY A Dremel 3D Printer- Germany