DesignSpark フォーラム
このフォーラムでは、世界中のDesignSparkに登録しているメンバーと様々な技術的相談や、議論を行うことができます。また、自身のアイデアに賛同してくれるエンジニアを、世界中から探すこともできるでしょう。
英語の投稿が目立ちますが日本語の質問でも問題ありません。よく海外から片言の日本語で回答を頂いたりします。自動翻訳レベルでも結構ですのでグローバルなユーザとのコミュニケーションをお楽しみください。
Hi,
I just installed DS PCB 11, I'm a long time user but now there's something I don't get: in the schematic editor I cannot do Copy/Paste (ctrl c and ctrl v). Also, when I right-click there is no menu item copy or paste.
When I do ctrl c on a component I can see it in the clipboard, so copy seems to work.
Copy and paste are working in all other Windows programs. I checked my keyboard, it is not in caps lock.
I restarted/rebooted, to no avail.....
I use Windows 10 Pro
Geert 面の調整びついて、[デザイン] タブの [編集] グループで [面の調整] をクリックします。となっていますが、 [面の調整] のアイコンがありません。このアイコンはどこにありますか、お教えください。 DesignSpark Mechanical Version 6 ist jetzt erhältlichhttps://www.rs-online.com/designspark/mechanical-download-and-installation
Infos zu den neuen Funktionalitäten findet ihr hier auf deutsch:https://www.rs-online.com/designspark/subscriptions-pricing-page-de
PS:
Ich bin eine Kollegin von Dave, der das auf Englisch gepostet hat Can you please add an annual subscription model with more payment options. My company is unwilling to pay for multiple users on current payment methods. It's a perfect subscription model for individuals but buisiness dont tend to like it. Ihr könnt Version 11 jetzt hier herunterladenhttps://www.rs-online.com/designspark/pcb-download-and-installation-de
Die neuen Funktionalitäten werden hier erklärt:https://www.rs-online.com/designspark/subscriptions-pricing-page-de I learned about SpaceClaim while evaluating Icepack. While we chose a different solution, I stumbled on DSM5 and have been using it for a year or so since it met my needs, was free and was based upon SpaceClaim. My use case for any 3D modeling SW is simply deign of 3D printable items for use around the house. Since my use is infrequent and doesn't generate income, my focus is on no charge SW packages.
With the elimination of opening step and STL files this no longer serves any purpose for me. I had looked forward to the mirror feature in DSM6 and hoped it would crash less often. Time to move on to Fusion or try to leverage a solidworks license at the office occasionally. Hopefully DSM5 continues to function for awhile longer
Windows 10 专业工作站版 22H1 安装后无法启动,以为是soildworks2019的问题,卸载soildwork2019,也是这样,删除软件重新安装也是这样,请教如何解决。 V6.0公開により、STEPファイルのエクスポートだけでなくインポートもできなくなったようですが、従来のExchangeモジュールはV6.0にも適用できるのでしょうか? After upgrading v6.0, STEP format data can not import.
Is this my installation problem? or intended change? Nach der Installation der Version 6.0 kann ich meinen Registrierunsschlüssel, den ich vor zwei Jahren mit der Version 5 erworben hatte, nicht mehr eingeben um das Programm in vollem Unfang nutzen zu können. Hat jemand eine Idee? Hello,
during start the DSP 11.0 I got the following Message: Error code: 12507
Does someone have any idea to solve that problem?
best reagrds Franz
Having just installed DS6 Creator version I have tried to export a simple cylinder shape as a STEP file. This results in a 'Failed to export' message in the staus history. Has anyone else experienced this?
Shape can be saved as a RSDOCX file without a problem
This is installed on a Win 7 machine. Bonjour ,
j'aimerais savoir si les 2 modules sous la V5.0 achetés sont devenus totalement obsoletes dans la version 6.0 ou sont-ils encore valables
env. 1000€ déboursé, il n' a pas si longtemps que ça, je souhaiterais passer à la version 6, mais si mes modules ne sont plus actifs je n'aurais plus acces à mes mise en plan et je ne pourrais plus exporter en STEP.
Un geste commercial pour les detenteurs des modules en V5.0 est-il prévu
cordialement i would like to ask anyone who already makes a project of Laundry Automation?
a customizable program/circuit from filling of water, washing up to drying (spinning) cycles
thanks! V6 cant import .stl files ???
is this a bug 最近のフォーラム投稿
No Copy Paste
操作方法
DSM Version 6 ist jetzt erhältlich
Subscription Models
Version 11 ist jetzt erhältlich
Disappointed by decontenting DSM5 in the DSM6 explorer edition
DesignSpark Mechanical在注册过程中 发生错误。
V6.0でのExchangeモジュール使用について
V6.0 can not imports STEP format
Nach Designspark mechanical 6.0 Installation kann ich keinen Registrierungsschlüssel eingeben.
Error Code 12057
DS6 Creator Version STEP file Export problem
anciens modules V5.0 (mise en plan et export STEP)
automation, laundry
V6 cant import .stl files ???