DesignSpark PCB: New Version 13 - NOW AVAILABLE

Skip to main content

3D View - Libraries that contain the 3D models

by DesignSpark

This tutorial requires:

DesignSpark PCB V11.0.0

The following shows the library structure and which libraries must be enabled for the 3D View to correctly render the PCB. These images were captured from, but Explorer and Creator are very similar.

Library Manager.

From the "Library Manager", select the Folders tab. If the "Default" library is not enabled (greyed out), select to highlight and check the "Folder Enabled" check box.

In the lower window area you will see four supplied folders of type .pkg, these contain the 3D models and must be enabled.

3D models

Now select the "3D View" tab.

To be able to see the available 3D component models select "All Libraries" and the list will be fully populated.

With the "Preview" checked, select any component and you will be able to see the component model and footprint symbol. The PgUp and PgDn keyboard keys can be used to move up and down the list or individual components can be examined by selecting with a left-click of the mouse.

Reports.

A further useful feature is the "Report" button which can be configured to generate component model reports and their use within the libraries.

An example using the above is shown below.

For further information, the built-in Help files include many details in the Index under “3D....” and “Edit 3D Package”.

RS DesignSpark is the go-to platform for professional design engineers, providing application and product content and design resources such as the award winning DesignSpark PCB and DesignSpark Mechanical CAD software.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments