DesignSpark フォーラム
このフォーラムでは、世界中のDesignSparkに登録しているメンバーと様々な技術的相談や、議論を行うことができます。また、自身のアイデアに賛同してくれるエンジニアを、世界中から探すこともできるでしょう。
英語の投稿が目立ちますが日本語の質問でも問題ありません。よく海外から片言の日本語で回答を頂いたりします。自動翻訳レベルでも結構ですのでグローバルなユーザとのコミュニケーションをお楽しみください。
Looking for some guidance on how to set up Home Assistant on a Rock.
Any guidance and input would be welcome.
https://www.home-assistant.io/
Can I continue to use my AddOn license (Export & Drawing) after updating from 5.0 to 6.0? Or do I have to update to Creator/Engineer?
Are there new features in Creator or Engineer that are not included in the AddOn package? Hello,
DS multilayer PCB vias have pads also in the layer with no connection. This implies that internal GND planes for example under a BGA have a lot of holes larger with respect to what needed for vias without unused pads.
Is there a way to avoid unused pads on vias?
Thanks
Antonio I've detected problem when trying load project file generated with DSM v5 to new DSM v6.
It's unable to load even simplest project file generated with DSM v5 to DSM v6.
Is this problem known?
When I try to load project file, I've got info message You can see as atachement.
You can see even 3D detail, but if I clik OK then loading stops.
Can You give me any helpfull info ? Just installed DSM 6.0
"Check for software update" button advises a new version: 6.0.4 is available from the subscription dashboard but it only shows the original DSM 6.0 download.
Where is it pls? bonjour,
je voudrai installer ce logiciel sur un deuxieme PC mais je n'arrive pas à me connecter suite à l'installation?
comment faire?
merci pour vos réponse
Thierry Hi,
Is there a way to report a bug other than the forum?
In DSPCB11 I found that when you make a change to an already used component, update component does not work. Even if you instantiate the new component, the old version that seems to be embedded in the sheet pops up. You have to delete all instances of the component on the sheet to be able to instantiate the new version.
Geert
Nach der Installation der V6 wollte ich mich mit dem Namen und dem Passwort Registrieren. Da kam dann die Fehlermeldung wie im Anhang ersichtlich. Bei der ersten Installation auf einem Rechner keine Probleme. Nun hätte ich das gerne auf einem 2. Rechner, wie seither auch. Das war mit der V5 kein Problem. Hi there,
seems that the GLB export from v6 has some problems:
-> look at the screenshot of the meshes exported from v5 and v6, v5 exports a much cleaner mesh, file size is also much smaller
currently DSMv6-Creator GLB export is not useable for us, hope this will get a fix..
サブスクリプションを使ってます。
DXFまたはDWGに保存ができません。
前のバージョンではすぐ保存できたのですが、
今回の6.0では保存を押してから1時間経っても保存ができないままで
反応ありませんになります。
windows11では不安定なのでしょうか?
STEP形式では保存はできました。
after installing designspark mechanical 6.0 cannot register and open it
this was the error prompted i also have admin rights in the computer im using and its windows 10
any help is very much appriciated
thanks after using the last version 6 fro five days, I cannot launch it anymore, i click on the icon and nothing happens, any help?
I have already tried the solution provided by the website, but the files it was suggesting to erase, wer not even into the spaceclaim folder..
Since signing up to DSM V6 I have been having problems with the licence.
I design most of my components on my computer in the house and then take over in my workshop.
I have been doing this since September 2020 with V5 without any problems. I cannot get DSM V6 to work in my workshop. Any ideas?
Ver6にアップしてみたのですが、STEPが読み込めないのでVer5に戻したいのですが、方法はありますか? Is there a change log available (as there usually has been in the past) listing the changes in DS PCB software between version 10 and version 11?最近のフォーラム投稿
Anyone with experience running Home Assistant on Rock?
Updating from 5.0 to 6.0
unused pads of multilayer PCB vias
Failed to load body geometry when trying load project file generated with DSM v5 to new DSM v6.
Can't find 6.0.4 update
activer DesignSpark Mechanicals sur un deuxieme PC
Bug report
Fehler während der Registrierung
DSM v6 bad GLB Export
エクスポートについて
cannot use or register designspark mechanical 6.0
cannot launch the version 6
Licence problem
Ver5に戻したいのですが
Is there a change log DS PCB 10 to DS PCB 11?