Skip to main content

Dragon Breath

by DrLucyRogers
A dragon that smokes (using an e-cig and a remote control).

Want to build along?

You can buy the full kit including all the parts from RS Online. Remember to log in to your account to access exclusive discounts.

Parts list

Qty Product Part number
1 CE4 Atomizer Clearomizer - 10 off for £5.79
2 18650 Battery Holder 3.7V
1 18650 Battery Charger
2 Ampking 18650 2500mAh 30A Rechargeable E-cig Battery
1 Y - Piece connector, 8mm od
1 Silicone Tube ID 8mm Hose Tube 2m Long
1 Vegetable Glycerin
1 DV 1.5-6V mini Air Pump

Please be aware this is not a beginners project.

Please take the necessary precautions and care.

The e-cig needs a high current and works at a high temperature.

The smoke is also hot.

My friends Polly and Chris enjoy Steampunk things - they are fantastic at making the costumes etc. but wanted a dragon that breathed smoke - they could make the dragon, but the smoking part they were not sure about.

The casting of the head and the making of the dragon is shown in another project.

This project shows how I hacked an e-cig and added some LEDs and controlled them using a remote control. (See the article How to remote control a Thing.) 

IMG_5767_8d48818ce8a0eec4d66e0ed39c100624c3452d9c.jpg

This is the "atomiser" end of an e-cig. The black part is the mouthpiece. A battery screws into the other end. The clear "bottle" holds the liquid that will be vaporised. Instead of using anything that smells or contains nicotine, I used food grade vegetable glycerine.

IMG_57701_d468384371e94ee8941d40e022f738c2e293ccd9.jpg

There's a pin inside the e-cig:

IMG_5775_71e5f65cff9ff711123928cd3192f67f009c791e.jpg

Using needle nose pliers, remove the central pin. I made sure the pin was clear of any glycerin by cleaning it with IPA (Isopropyl alcohol). A better way would be to take it apart *before* testing it works!

IMG_5771_7c8a89e2be47bcaa4811e5793f83fa1b8a296aef.jpg

Note - it is not necessary to take the atomiser completely apart!

How the e-cig works: Electricity runs up the inner pin, and conducts to the small metal wire wrapped around the bundle of "string" and then out to the outer part of the e-cig (third part in from right). The wires heat up like an incandescent lightbulb. The string wicks the glycerine up to the heated part, where it vaporises. Air passing from the bottom of the atomiser (the right-hand side) causes the vaporised glycerine to pour out of the mouthpiece (black part).

Solder a red wire to the pin. Use a relatively thin wire.

IMG_5783_9fa6ecf90f60d249430fb2da30a249bf038abe44.jpg

This is the hardest part as the solder does not stick to the pin easily. Tin the red wire and the end of the pin - be careful not to block the hole - this is where the air goes in.

IMG_5777_8f9a404ca902e50c9898b2d4f96b8daeb9189a0d.jpg

Heat the pin with the soldering iron (make sure there is solder on the tip), then place the red wire on it until the solder joins the two.

Again, make sure the hole is not blocked. 

IMG_5790_ca04534545d80e0164b5f1efa5e5a38df1927879.jpg

Solder a black wire to the outer e-cig body.

IMG_5795_9239766d44c75b867273665eda27310fd029a1f6.jpg

Make sure the inner pin, any solder touching it or the metal wires from the red wire do not touch the outer e-cig body when re-assembled.

IMG_5764_077191a0e70c577566e50e4de1aa9847d2d11fbb.jpg

Air Pump.

IMG_5799_323e033d0ed090fa0991668967629a760b2bfd7e.jpg

The other ends of the wires are soldered to the air pump.

IMG_5798_76f0cdf7eea7f5cd8140b24bad40393ebc7ff070.jpg

Re-assemble the e-cig.

With care to line up the output of the pump with the air hole by the central pin of the e-cig, hot melt glue the pump and the e-cig together. I found this to be very messy and difficult to get right.

IMG_5797_f1c6be0e6a71bcc2313ce6d0fb5b285ece97560d.jpg

Add the glycerine. It goes in through the mouthpiece. Do not overfill - half full is more than enough.

The wires from the air pump will go to the Thingatron, which is controlled via the Remote Control a Thing system. The e-cig battery is connected to the Thingatron, and power to the e-cig and pump is only applied when the Thingatron is switched on.

IMG_6219_cb4361ce47bef128c0bd211d6a0251c40d77e5d0.jpg

A silicon tube, and a "Y" adaptor channel the smoke from the mouthpiece to the nostrils of the dragon.

IMG_5751_b23bd456ca823d7d98bbd53f7df2f8a0aebe4c3d.jpg

This is a Thingatron. Another output pin from the Trinket on the "Remote Control a Thing" goes to another Thingatron (built on to the veroboard) which controls two sets of LEDs - one set for the eyes and the other for the nostrils.

IMG_5728_322b6b25f9e61c61d299ccf14123d2a64e200e2b.jpg

Random notes:

  • I programmed two buttons on the remote -  "A" does LEDs and smoke, button "B" just LEDs
  • To stop overheating, I programmed in a delay so you can’t re-press the buttons for 30 seconds
  • You need to run the smoke about three times before it comes out - once there’s smoke in the tube, it’s fine.

Remote Smoke video


Articles in this series

  1. How to Remote Control a Thing - make the remote element
  2. Dragon Breath - electronics for the eyes and smoke
  3. Experiments in Casting a Dragon - creating the mould
I am an inventor, engineer, writer and presenter. Other stuff: Royal Academy of Engineering Visiting Professor of Engineering: Creativity and Communication at Brunel University London; Fellow of the Institution of Mechanical Engineers and have a PhD in bubbles; Judge on BBC Robot Wars.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments