- Startseite
- Community
- Foren
DesignSpark Foren
Kommunizieren Sie über den Forenbereich frei mit anderen Mitgliedern von DesignSpark. Eröffnen Sie neue Unterhaltungen oder beteiligen Sie sich an bestehenden Diskussionen über Produkte, Technologie, Software und zukünftige Neuheiten. Helfen Sie mit, Lösungen zu finden oder suchen Sie nach Antworten auf Ihre eigenen technischen Probleme, indem Sie auf ein globales Netzwerk von gleichgesinnten Ingenieuren zurückgreifen.
Good morning
I need help for a newbie
I would like to know how to fill a wireframe object.
I cut an object in half.
I would like to add it to a solid object, I need some explains, please
THANKS
DesignSparkPCBv11.0.0をダウンロードして起動しようとしましたが、
Login情報を入力した際に添付のエラーメッセージが出て起動できません。
DesignSpark Mechanicalv6.0は問題なく起動するため、Login情報は間違っていないと思いますし、
ネットワーク上の問題でもないと思います。
以前使用していたDesignSparkPCBv10.0.1ではこのような症状は発生しませんでした。
対処法を教えて頂けますでしょうか。
Bonsoir,
Il y a t'il possibilité de zoomer avec la molette centré sur le curseur. Hi everyone.
How could I make a track plated or exposed? I would like to have tin to be over the track. I also thought of using a custom pad but I can only make the pads straight vertical/horizontal
Any ideas?
Thanks Does anyone know what to do about this issue I am having with the installation ?
Has anyone else run into the same problem?
Thanks,
TT I bought a new PC but Spark Mechanical theme crashes my PC.
I have a PC with the following data:CPU: AMD Ryzen 7 5800XMotherboard: MAG B550M MORTAR WIFI (MS-7C94)Graphics card: NVIDIA GeForce RTX 3060Ram: 32.0GB
When I work with Design Spark Mechaical, my PC immediately shuts down and restarts. This can be right at the beginning or after 10 minutes. I have already installed a new graphics card, renewed the CPU, RAM and the power supply. The problem is still there.
I also ran benchmarks and stresses for hours. Everything went without a problem.
Does anyone have an idea what is causing this? Hi, I would to say if it's possible to export files project from design spark pcb to Orcad.
thanks
Hi,
I am using V6 version of DSM with "Explorer" option.
Can I open a STEP file just to watch it?
If not with what option can I do it?
thank you for your feedback.
The next image contains a cylinder with text. There's 2 copies of the same cylinder, only seen from different directions. The cylinder is an imported STEP-file and it contains some friendly guidance pointed to me. I have DSM version 6.0 Creator, the cylinder is made in a 1000% higher cost CAD program.
The properly typeset text is no problem today; one can put it together in a 2D vector drawing program and export it as DXF. DSM Creator imports it.
But placing the text on a cylinder (=pulled circle) goes offroad in the beginning:
The projection is usable only in a narrow zone in the middle. In the left and right ends the letters are stretched intolerably.
In an older discussion of the same problem one suggests recomposing the surface to narrow slices which are arranged temporarily to a line in parallel with the text. Another suggests placing one letter at a time.
The third suggestion was "turn on option wrap around ". There was a link to a SpaceClaim tutorial of it. The tutorial said it works with planar and cylindrically curved surfaces, so it sounds very reasonable when compared to those 2 ultra tiresome other suggestions. Except: How to turn that wrap around ON? There's no such option shown for DSM project tool. It's hidden or it's nonexistent.
I saw the STEP file was easy to make in a high cost professional CAD program. Is there any known easy method to do the same in DSM 6? I am designing a PCB prototype and am getting an error when I submit it to the manufacturer.
When I check it with a gerber viewer all I get is a black screen and board outline on the paste mask layer.
I can't see why this is happening as when I view it before i run the program to produce the gerber output it is shown.
Also,on the NC drill data output the board is not showing the correct size on the screen, even though in the position tab, the positions are the same as the other layers.
I have just moved over to DSM version 6 and now i cannot seen to project text onto my project, all i get is a swerling circle and no responce senario, I had no problem with DSM v5 Hey everyone,
I've been trying out the DesignSpark 11 "Engineer" version and I can't seem to get a preview when creating a 3D model of a component package. When I launch the 3D view of the board, it does show up. This makes it very difficult to create and edit 3D models. Does anyone have a solution to this problem?
Does anyone know the procedure to create plated slotted holes in DesignSpark v11? DSMのビギナーです。ver.6.0にて作図しました。3Dpdfにエクスポートを試みましたが、うまくいきません。エラー表示もありません。ファイルに問題でもありますかね? Hello,
I recently upgraded from DS Mechanical 5.0 to 6.0 and I stumbled upon a problem, which I can't seem to find a fix for.
Whenever I try to create a pattern of any kind as soon as I input distance and/or angle the option to change said value dissappears and I can only edit the number of copies. It is quite annoying as it worked fine in 5.0.
Is there some kind of option I have not turned on, or is it a bug?
Sincerelly,MichałNeue Forumsbeiträge
Fill an objet
起動ログイン時のエラー
Zoom a la souris
Exposed plated track or custom pad
Issues with installing DSM 6.0
Theme Spark Mechanical crashes my PC
export files project on Orcad
Open step file
How to wrap text properly around a curved surface
No Paste layer?
Projection
No 3D Preview when creating 3D model
Plated slotted holes
DSM ver.6.0 3D PDFにエクスポートできません
Problem with editing pattern
Unser Forum
Software
Activist Engineering
Community
Ambitionen als Ingenieur
- Beiträge
- 2
Mein erstes Design-Projekt war
- Beiträge
- 16