Skip to main content

EMI Debugging with an Oscilloscope

by Rohde & Schwarz (No longer a member)

Benefits of using an oscilloscope

Oscilloscopes are the workhorses for power electronics engineers. With powerful and easy-to-use FFT analysis capabilities, their application fields extend to EMI debugging – and that saves a lot of time and money. A typical task is verifying the effectiveness of an EMI filter – early in the development phase.

Rohde & Schwarz oscilloscopes offer a powerful, easy-to-use FFT analysis functionality to measure the magnitude of the frequency component. Users are able to see the time domain related signals at the same time and can therefore correlate unwanted spectral emissions with time domain events. This makes these oscilloscopes powerful stand­alone instruments for performing early conducted emis­sion tests on power electronics designs. They can easily detect electromagnetic interference from electronic circuits with high speed and accuracy. The basic working principle of an oscilloscope is to capture sig­nals when the input signal exceeds a specific trigger value, which helps to capture the peaks of the noise signal.   

Overall, the major benefits of using an oscilloscope can be summarized as follows: 

  • Visible correlation between frequency and time domain
  • Wide and instantaneous frequency coverage
  • Deep memory for capturing long signal sequences
  • Gated FFT analysis for correlated time-frequency analysis
  • Frequency masks for triggering on intermittent events with lab-class instruments
  • Overlapping FFT computation with color grading with lab-class instruments

 

Evectiveness of the EMI filter

The FFT functionality of Rohde & Schwarz oscilloscopes is a powerful feature that enables designers to debug con­ducted emissions of power supplies. When using an oscilloscope to test conducted emissions, the R&S®RTM3000 plus a line impedance stabilization net­work (LISN) are an ideal combination for debugging. To measure conducted emissions of a power supply, you need an LISN, for example the R&S®HM6050-2, to decou­ple the device under test (DUT) from the external power supply.

Once the FFT is applied to the signal, and by selecting the center frequency and span, an oscilloscope can show the time domain and the frequency domain traces – compa­rable to what you can find on a spectrum analyzer. When comparing emission limits, you need to take into account that the signal might be attenuated due to the LISN. The EMI filter of the switched mode power supply is re­sponsible for the reduced EMI spectrum; the noise gener­ated at the input of the DC/DC converter is clearly visible in the left screenshot. With the low-pass-filter, you see that the conducted emissions on the input are effectively at­tenuated. For some frequencies, up to 30 dB attenuation is visible.

spectrum_comparison_10ed87e2b0e2ca9436fc787590f0cb0cd80c6658.png

 

Comparison: lab-class vs. medium-class oscilloscopes

For debugging and locating emission sources using an oscilloscope, a combination of the R&S®RTM3000 or the R&S®RTA4000 oscilloscope and the R&S®HZ-17 near-field probe set can do an excellent job. In addition to that, lab-class oscilloscopes have extended trigger and analysis capabilities that provide valuable tools for analyz­ing difficult EMI problems. Lab-class oscilloscopes’ ability to define multiple and different types of triggers for time, frequency and digital signals can be useful in examining the cause and effect of the captured signals.

To summarize, compared to medium-class oscilloscopes, lab-class oscilloscopes offer a few very useful features:

Comparison_083383be0943dab5f02fc304c17c71de3587d313.png

 

Rohde & Schwarz (No longer a member)
This person is no longer a member and their bio is unavailable
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments