United Kingdom
Technical Manager | ebm-papst UK Ltd
My background is in Mechanical & Production Engineering however working for ebm-papst that has expanded into electro-mechanical, some electronic and acoustic engineering. When it comes to acquiring and passing on knowledge, I try to keep it as simple and as least painful as possible. I am happy to receive feedback and if there are any questions that arise from anything that gets published. If I don't know the answer to your question immediately, I am sure that I know someone that can help.
Published Content

10 months ago
Rack Cooling Solutions from ebm-papst
Ever increasing data transmission rates in equipment installed in a 19-inch rack applications, require close management of temperature. Fans and controllers can deliver cooling when required to optimise equipment performance and reliability

10 months ago
Fans in Refrigeration - Condensing Units
For the low-pressure high-volume operating point of a refrigeration condenser, the selection of an axial fan with its wide area of coil coverage ensures that maximum heat exchange efficiency can be achieved. This article explores the reasons why.

1 year ago
Fans in Refrigeration - Axial fans for Unit Coolers
Whether cooling is required for bulk food storage, maintaining a low temperature for food preparation, controlling the ambient temperature in a processing plant or drinks cellar cooling, unit coolers using axial fan technology provide the solution

1 year ago
Making a RadiCal Change – Delivering Quieter Enhanced Efficiency
When the application needs airflow and there is resistance, using a backward curved fan can maximise efficiency, minimising noise and energy use. The RadiCal backward curved fan range enhances efficiency delivering air using less energy, more quietly

1 year ago
Fans in Healthcare
Behind the scenes of one of the essential services in the UK, fans are used to provide the delivery of air for several reasons. This article explores some of the many areas where fans support the healthcare industry...

1 year ago
Manufacturing Made Simple - RS Components Custom Assembly Service
When there is uncertainty, flexibility is key to maximising the return on investment. Flexibility can be achieved using lean manufacturing, which is where ebm-papst & RS Components higher level assembly service adds value to your production processes

1 year ago
More than Saving Energy – Potential Opportunities to be realised by upgrading your equipment
Legacy equipment performing day to day tasks are the backbone of the infrastructure and services we rely on. Many of these systems and equipment have been around for years and could benefit from an upgrade...

2 years ago
Turning Virtual Reality into a Fully Immersive Experience
Colleagues at RS Components, Austella and ebm-papst UK got together to discuss how to add an extra dimension to the Radial-G virtual reality racer to make the game more immersive. This project grew to be a very interesting and exciting challenge!

2 years ago
S-Force Axial fan Produces Superior Performance
As the largest S-Force compact axial fan, the 2200F combines state of the art aerodynamic design and intelligent motor technology to deliver high flow with high-pressure development. Perfect for demanding applications where space is at a premium.

2 years ago
Birdly - Making the Dream of Flying a Virtual Reality
Max Rheiner is making the dream of flight a virtual reality. In this interview, the head of the master’s degree program for design interaction at the Zurich University of the Arts explains how it’s done and why moving air plays an essential role...

2 years ago
Using the Natural Environment to Manage Heat Loads - The Case for Free Cooling
For sensible heat loads, using the local ambient air with some provisions for moisture and particulate protection, can provide adequate all year round free cooling without the extra power requirements a mechanical cooling system

2 years ago
Powerful Performance under Pressure – Fans for Inverter Drive Cooling
To meet the need to reduce energy consumption variable speed drives are used to match supply with demand. Frequency Inverters can achieve this however size restraints, high power density and efficiency losses mean that forced cooling is required.