Skip to main content

Solid State Relays: An effective solution for Motor Control

by ManonD.

ccelduc logo

Solid State Relays: An effective solution for Motor Control

Motor control is usually hard to deal with, as a motor is an inductive load with lots of high starting currents (increasing the cost of protection devices) and overvoltages generated during turn-off.

Indeed, there are drawbacks when direct starting a motor:

  • High inrush current: Heat, flicker risks, energy and installation costs
  • Noise, arcs: Short control lifetime and high maintenance costs
  • High transient torque: Excessive wear of the coupling parts leading to maintenance costs

All of these disadvantages can lead to quality problems during production.

Thanks to their size and high adaptability, solid state relays are more and more popular to control motor loads.

One of the main advantages of using power electronics is that the numerous control modes can easily perform thanks to very fast response time, and computing power of microprocessors.

Types of electrical motors

ac Alternative current motors

AC motors are the most used. They are powered by an alternating current that converts the electricity in order to get a rotative mechanical movement.

There are different types of AC motors:

  • Squirrel cage motors
  • Wound motors
  • Synchronous motors
  • Traction motors

ac motor

AC motors represent a lot of advantages:

  • Low power required for start-up
  • Controlled acceleration
  • Speed control
  • Controlled starting current
  • The customizability of torque requirements
  • Decrease the power line disturbance

dc Direct current motors

DC motors have a more specific use, for instance for boats or machines needing high-speed rotation.

There are different types of DC motors :

  • Shunt motors
  • Separate excitation motors
  • Series DC motors

dc motor

The main advantage of DC motors is that it is easy to set up and control their speed. Nevertheless, DC motors tend to wear quickly and can generate a lot of noise.

Types of Solid State Relays for motor control

Three-phase ON/OFF solid state relays

ON/OFF solid state relays are often available in zero cross and random versions. They can only work in a binary way (on or off). Reliable and efficient, ON/OFF SSR ranges are the perfect choice for industrial motor control. Indeed, ON/OFF SSRs have been elaborated to handle very frequent start and stops of three-phase motors.

three-phase on/off 1three-phase on/off 2

Soft Starter

A soft starter limits the inrush current and increases the life expectancy of the mechanical pieces. It then allows to softly start the motor, and reduce the starting current, limiting the peak energy demand.

Soft starters are available in single-phase and three-phase versions.

soft starter 1 soft starter 2

Motor inverters

Rotation inversion is often used to effectively change the load rotation movement, or for counter-current braking. It is then needed to use a device to limit the torque and current overload. Inverters are then to the optimal solution for this type of use.

inverter 1inverter 2inverter 3

Solid State relays advantages

life expectancy A very high life expectancy

Solid state relays do not have any moving mechanical parts so they are not subject to any contact failure, mechanical strain or corrosion. A solid-state relay has an average lifespan of millions of cycles with no deterioration in performance.

Nevertheless, in order to benefit from a solid state relay’s infinite lifespan, it is highly recommended to use heatsinks in order to help the solid state relay to evacuate the heat generated by its use, and then avoid any overheating that could lead to serious damage.

energy A low energy consumption

Solid state relays required very low currents to switch high power loads. Since SSRs do not have to energize a coil and physically open and close contacts, they actually consume 75% less power than electromechanical relays.

silent Silent operation

SSR technology uses electronic circuits to provide switching, meaning SSRs make no acoustical noise. This is a highly needed feature in medical applications for instance.

resistant Resistant to shocks and vibrations

As SSRs have no moving parts and are entirely enclosed in a housing, they are well-suited for harsh environment applications. This makes them highly efficient in industries with harsh environments, such as the railway industry.

switchingA very high switching frequency

Solid State Relays switch on and off faster than electromechanical relays. Power to a load then can be applied and removed very quickly and precisely.

diagnostic Various control types and diagnostics functions

Solid State Relays offer different types of controls (specific choice of switching time) and possible diagnostic features.

mounting Various mounting configurations

Solid State Relays are available in different housings (Hockey-Puck, 25 mm, PCB), meaning they adapt to various types of mounting (DIN rail, PCB, panel mount).

celduc® relais has developed specific solid state relays for motor control. celduc® SSR manufacturing is 100% based in France, which guarantees quality and reliability for each product.

With nearly 200 full-time employees in 4 countries on 3 continents, celduc® relais is a leading player in the global market for industrial automation and magnetic proximity sensors. Founded and located in Sorbiers, France, celduc® relais, is known as the expert in solid state relays and magnetic sensors. Every year, we are proud to manufacture more than 1 million relays sold worldwide, helping to promote French industrial expertise and “100% made in France” quality.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments