DesignSpark Circuit Simulator Maintenance on 23rd May at 15:00 UTC for 2 hours

Skip to main content

Banksy Shredder Frame - Version LR1

by DrLucyRogers
Recently, Banksy shred one of his artworks - just as it sold at auction for over a £1million. People wanted to know why and what it meant. I wanted to know how. So I made my own versions. This is version 1 - using a commercially available shredder.

Parts list

Qty Product Part number
1 Picture Frame A4
1 Picture Frame A5
1 Wooden Box
1 Inverter,quasi,UK,12Vdc/230Vac,300W 735-0715
1 Battery,rechargeable,sealed,lead acid,UPS,12V,5Ah 320-4508
1 Yuasa Lead Acid Battery Charger, with UK Plug 533-6821
1 A4 strip cut shredder
1 Wireless remote control socket / "Bye Bye Standby"
1 Ikea Knagglig Pine Box 23 x 31 x 15 cm

In October 2018, Banksy shredded one of his artworks - just as it had been sold for over £1million (including fees) at auction. While people were wondering whether the purchaser would have to still buy the piece, whether Sotherby's the auctioneers were "in on it" and who was ultimately responsible, I was wondering how it was done.

A few technical questions sprung to mind:

  • How was it powered? It wasn't plugged in so had to be battery or some form of mechanical/clockwork/spring mechanism.
  • How was it triggered?
  • Was the original actually shredded, or was it a variation on the Money Making Magic Trick?

Money_Maker_Magic_Trick11_90aacf692df77ee97e3fe872d04a481160f08e75.jpg

My first step was to get something similar working, so I bought a Wilko strip-cut shredder

Wilko_Shredder1_58653a8cff0af91219bbbbd6ccf3c75e25e19bbf.jpg

And a Remote-control standby energy saving kit - Bye Bye Standby

ByeByeStandby1_176f17e39cc9582ca080a17380881600de0e92ff.jpg

Plugged one into the other, and, with the shredder on "auto" mode, was able to shred a piece of paper using the remote control.

I then wanted it to resemble the Banksy installation. As Banksy had said of a previous artwork:

"Never underestimate the power of a big gold frame."

Sotheby's catalogue says the frame was 101x78x18cm. It also, unusually for this type of thing, listed the artwork as "in artist's frame". Also, 18cm is very deep.

Girl_with_Balloon_Banksy1_438832b365fd59d3e1cfa54cb20201da451a536f.png

The shredder I bought had a maximum width of paper it would take of 22cm. So I scaled everything down a bit.

I bought a couple of frames from a charity shop:

IMG_5640_d818b9dfad2742c257de6093f1d9c7a0e3275e1e.jpg

IMG_5641_5398350c63184a04bac53f042d71bc71c9e8fe8a.jpg

I nailed one to the other to give it bulk and also to hide the shredder.

I then hacked an Ikea Knagglig Box

knagglig-box-pine_c21250d811dfd64dd9b34cf468bc59be38113e75.jpg

The shredder was too deep to fit inside, so I needed to take the back off.

IMG_5645_db0260c041d04643fbe1d6a1c054eb18c781654f.jpg

The result can be seen in the video below:

I was pleased with this, but the frame at Sotherby's was not plugged in.

So I got an inverter and a battery and tested it all to make sure it still worked.

IMG_5992_87b64735e8afde9f9508b8f11313e67147987d6b.jpg

Then fitted those inside the box too - although the box needed more hacking, and now has a back, but no bottom!.

IMG_5998_5aa2dbbd01b44545e8020e8a638fc61418011b37.jpg

 

The final result is better - it's wireless! But it's still not perfect.

Some things that suggest this is not the way Bansky did it:

  • The inverter remains "on" and using power, even when the shredder is not on. The battery life would, therefore, be limited.
  • Inverter hums when it is on.
  • The picture is on A4 paper - the image is just at the top. The bottom of the page gets shredded first, which is blank.
  • The remote control is bulky and obvious.
  • This type of shredder has serrated blades - leaving the "shreds" serrated.

Banksy has put out a few videos about "how he did it" but there are red herrings or errors in these, such as using scalpel blades flat side rather than point side up, holding a soldering iron by the hot bit, and using scalpel blades AND a shredder mechanism. 

Although Banksy said it was meant to shred the whole thing, and not just part way, I am not convinced.

If I were making this and needed it to work perfectly first time, I wouldn't do it this way.

However, this is one way it could have been done. And one that needed little in the way of electronics skills.

I am an inventor, engineer, writer and presenter. Other stuff: Royal Academy of Engineering Visiting Professor of Engineering: Creativity and Communication at Brunel University London; Fellow of the Institution of Mechanical Engineers and have a PhD in bubbles; Judge on BBC Robot Wars.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments