- Startseite
- Community
- Foren
DESIGNSPARK FOREN
Kommunizieren Sie über den Forenbereich frei mit anderen Mitgliedern von DesignSpark. Eröffnen Sie neue Unterhaltungen oder beteiligen Sie sich an bestehenden Diskussionen über Produkte, Technologie, Software und zukünftige Neuheiten. Helfen Sie mit, Lösungen zu finden oder suchen Sie nach Antworten auf Ihre eigenen technischen Probleme, indem Sie auf ein globales Netzwerk von gleichgesinnten Ingenieuren zurückgreifen.
Are there any plans for DS to implement .3MF exports? I use designspark for creating 3D printing models with multicolor printing. .3MF exports are very necessary. Please tell me this in the works and will be released soon.... Ich kann die oben genanten Formate nicht importieren. Die Version ist 6.03 und ich bin bei rs-online angemeldet. Was läuft hier falsch?
Vielen Dank! You can find Schematic and PCB reference designs for DesignSpark PCB software and live circuit simulation reference designs for DesignSpark Circuit Simulator in this reference design centre.
For example, check out Siemens' article about
Tighter Fuel Metering with a “Quick-Off” Injector Driver
This and more at https://www.rs-online.com/designspark/reference-designs
See more of the information you need, with DesignSpark Creator and DesignSpark Engineer
Product data, environmental and lifecycle information as well as 3D models, footprints and schematics for a billion products - more info here:
https://www.rs-online.com/designspark/product-design-centre
Good morning I'm looking for an instruction manual for the Windmoller Triumph V made in 1972. I would like if anyone has the pdf
this is the first page, and I have just this. Ok, on my switch project I was getting along fine and thought I could make the whole thing without asking for help. But, although I can easily make this spacer without the splines in the form of cones or straight cylinder shapes using the revolve tool and it will likely work fine, I was wondering how I could make it look like the original. I have added a pic of the spacer and would like to know the best approach or steps to make this odd piece that will be 3D printed likely with supports. I just need a little guidance. :)
I am thinking make and extrude the circle in the center then add a sketch shaped like a plus sign and extrude it for the left side. Then add another sketch for the right side but it has a step there, so make the short section and add yet another sketch to finish the right side?
Thanks in advance!
Hi, why is there a green boarderd around my part? I drew the part from scratch, according to the geometry check no issues. How do I fix this I need to to be consistent with the other 10 similar parts I drew that did not have a green boarder.
Thanks
Bonjour,
Comment calculer la distance minimale entre deux pistes et la largeur du piste dans un Pcb qui contient uniquement quatre connecteurs et des pistes pour faire le test de diélectrique pour une tension de 1000V.
Moderator Translation:
How to calculate the minimum distance between two tracks and the width of the track in a PCB which contains only four connectors and tracks to do the dielectric test for a voltage of 1000V.
Bonjour,
C'est la quelle est la différence entre plan de masse et le coulée de cuivre dans un Pcb ?
Merci d'avance .
Moderator Translation:
what is the difference between ground plane and copper pour in a PCB? Bonjour,
C'est quoi la signification de ce trait bleu ?
Merci d'avance
Moderator - Translation:
What does this blue line mean?
Pozdrav
Na koji nacin mogu obnoviti pretplatu te izvrsiti uplat After creating the sketch, DSM automatically cuts out the surface for me. How to turn it off. It used to be enough to turn off the Enable Constraint based sketching option. now it doesn't work. Hello, I am a complete newbie to the program. Nevertheless, I created a CAD drawing of my project as part of my final thesis. Now I would like to insert this into my PowerPoint as a rotating object. Does the program offer me this option? I would then record it with OBS and then embed the video in the PowerPoint.TLDR:I need an automatic rotation of the CAD drawing When can the program be adapted for macOS? This is the best design program for Windows. But I switched to macOS. Hi, I can't find out how I can start to draw a line (or anyting) a spesific distance from another line (or object).
I'm drawing a house, and when I want to draw a window in the wall, I want to start 1000 mm from left and 500 mm from top of the wall. How can I start at this point.
So far I'm drawing lines (1000 from left and 500 from top) and then erase them after the window is finished.
I hope there is another way to do this?Neue Forumsbeiträge
.3MF export
Creator Version, kein Import von dxf, dwg, stl oder step möglich
What are reference designs for Circuit Simulator?
What is the DesignSpark Product Design Center?
WindMoller & Holscher Manual
Best way to model this part?
Green boarder around part?
Distance entre les pistes - Distance between tracks
Pan de masse / coulée de cuivre - Copper Ground / Pour
Trait bleu - Blue Line
Kako mogu obnoviti pretplatu - Renew Subscriptions
automatic cutting of sketch surfaces
Rotate a 3D model for a presentation
When will it be available for macOS?
Start line a spesific distance from another line.
Unser Forum
Software
Activist Engineering
Community
Ambitionen als Ingenieur
- Beiträge
- 2
Mein erstes Design-Projekt war
- Beiträge
- 16