你觉得这篇文章怎么样? 帮助我们为您提供更好的内容。
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
你觉得这篇文章怎么样?
Hardware test for DC DC interleaved boost converter
Hardware test for Monolithic interleaved boost converter with MPPT:
-Hardware model: ST microelectronics, ISV008V1, (complementary 3 X SPV 1020)
-Use DC power supply and photovoltaic cell 2V to 28V input voltage
-Value and waveform of V, I, P, I ripple will be recorded by CRO.
PSIM simulation will be repeated if true hardware parameters are obtained by manufacturer’s manual or measurement.
Previous PSIM simulation data:
The ISV008V1 has 3 sets of SPV1020 on same board and could be operated separately. DC power supply is used for hardware test and use only one channel for safe.
Rheostat is adopted as a resistive load for adjustment.
It is found that ISV008V1 requires an initial voltage for its operation. The gain is around 4~5 times and similar to the PSIM simulation.
The data are measured from one of the channel of ISV008V1. The converter will be operated when input voltage ranges around 6V~10V in two resistive loads.
The input voltage is about 8V and the converter will not further boost the output voltage though that rises to 18V.