- 浏览 DesignSpark Mechanical 界面并创建新项目
学习 DesignSpark Mechanical
完成这些教程后,您将能够:
- 使用推拉和直接建模工具创建及编辑 3D CAD 模型
- 导入、放置并处理 3D 零件与装配体
- 解决常见建模问题,包括几何错误与操作失败
- 准备并导出用于 3D 打印和制造的 3D 模型
教程
使用我们为初级、中级和高级工程师提供的分步教程,在从设计到制造的过程中先发制人

入门
了解如何下载、安装和登录软件

Mechanical 用户界面
学习如何浏览和使用软件内的功能

开始新的 Mechanical 项目
"我们的如何操作指南可以帮助您构建您的第一个可打印设计 "

3D 部件相关的操作
了解 3D 模型以及如何使用它们

创建您的 Mechanical 3D 设计
使用软件内的功能来完成您的项目

为打印准备 3D 模型
准备您的 3D 项目设计,以便打印它
DesignSpark Mechanical 社区
寻找灵感,获得支持,并与其他 DesignSpark Mechanical 创作者分享您的作品。
I'm making a part for a motor mount and need it to be 3Dprinted but it says (Part mesh is not watertight) I dont know how to fix this, I've tried making it solid but i'm new to this and dont know what im doing. 下記エラーが出てファイル保存できません。何かご存知の方いればよろしくお願いします。
(パス+ファイル名).rsdocxの保存中にエラーが発生しました。このコマンドを実行するための十分なクォータがありません。 In the online help it says to select the note tool on the Annotation ribbon, but I can't see an annotation ribbon
I am sure when I first instaled DS Mechanical I think there was a ribbon on the LHS, but cant see it now
I am a bigginer with this software so I apologise if this is a stupid question I have upgraded from 6.0.3 to 6.1, but when I try to export an .stl, DSM freezes. I have checked all the settings are identical to that in 6.0.3 and they are. I cannot even save a file without DSM freezing. I still have 6.0.3 installed alongside 6.1, but am loathed to uninstall it, because currently I can't use 6.1.
Does anyone else have this issue?
Tom Dear users
we know you've all been waiting for this! You can always agree to our weekly DS newsletter to keep in touch with news and bug fixes.
Review your newsletter setting here https://www.rs-online.com/designspark/my-account/marketing-preferences
But here's the important article on STEP exports :)
https://www.rs-online.com/designspark/how-to-fix-a-failing-step-export-in-dsm-v6-1
When moving an object around the image distorts and measurments appeare not conected to what you are measuring. How do you turn the mode off? I am a new user (Novice) of the Design Spark Mechanical and I cant work out how you can hatch an area. I tried Fill but it doesn't just fill the area I want to fill, But 2 sides of the rectangle are sides of a bigger rectangle.
Any tips on solving this will be welcome Hi guys, this has been bugging me for years.
I want to open multiple files FROM file explorer and open in a single DSM in multiple tabs?
Wether i have DSM open prior or post makes no difference. I get many DSM opening on my taskbar and takes ridiculous amonuts of time.
Is this possible to do while in file explorer?
Thanks Hi everyone,
Since updating to the new version DesignSpark Mechanical V6.1, the file preview images (thumbnails) for my saved .rsdoc files are no longer showing up in Windows Explorer. Only the standard icon is visible.
I am using Windows 11. In the previous version of DSM, the preview worked without any problems.
Is there a known fix for version 6.1 or a specific command to manually reactivate the file preview?
Thank you very much for your support!
I have a formula for a circle with 6 ripples. The circle has a radius of 10 and the ripple radius varies between 9 and 11.
x=(10+1*Sin(6*[t]))*Sin([t])y=(10+1*Sin(6*[t]))*Cos([t])z=0
Interval (t)Start=0End=2PI
The above formula works perfectly. I am trying to enter a new formula as follows where the ripple radius varies propotionally from 10*1.1 to 10/1.1 but am getting unexpected results.
x= (10*1.1^Sin(6*[t]))*Sin([t])y= (10*1.1^Sin(6*[t]))*Cos([t])
I have attached screenshots of the two DS Mechanical curves above as one of a speadsheet graph showing both, which are very similar.
Any ideas what I am doing wrong?
I am new to the forum but have been using DS Mechanical for a year or two for 3D printing. I really appreciate the functionality.
I am current trying out the equation funtionality with some good and some unexpected results which I am hoping to clarify here.
I would like to use degrees instead of radians in the trig functions. (The Design interface standardises on degrees so not sure why formulas should not but I digress.) The documentation states that you I can use the deg/ rad to specify the unit. I have tried but keep getting errors.
I used the following formula as a test which works as expected, a circle with 6 ripples
x=(10+1*Sin(6*[t]))*Sin([t])y=(10+1*Sin(6*[t]))*Cos([t])z=0
Interval (t)Start=0End=2PI
What I have tried:
t-Start=0deg ; No change Start becomes 0t-End=360deg ; End becomes 6283,19 and result is an unexpected straigt linex=(10+1*Sin(6deg*[t]))*Sin([t]) ; Error Illegal name for equation parameterx=(10+1*Sin(0deg+6*[t]))*Sin([t]) ; Same error
Any suggestions appreciated Hi,
I am finding it difficult to make a countersunk slotted hole for a countersunk screw, I have added the 5mm slot for the screw and added a further circle at 10 mm which would be the width of the countersunk head but I cant work out how i would pull say 45 degrees from the top circle if that makes sense, any help appreciated.
Thanks Stuart Is there a way to change an objects scale from one ratio to another?
Lets say I'm drawing something to full size, but I would like to sale it down when finished to a ratio of 1/48 or 1/87 scale then export to STL. Is there a way to do that?
Thanks! aとbの図形合併時、完全に埋めてある内部をくりぬいて空洞にしたいどのようにすればいいのでしょうか?
When merging shapes 'a' and 'b', I want to hollow out the completely filled interior to create a void. How can I do this?
Hello everyone. I’m asking the community to convert a model from *.stl to *.rsdocx for me; the current model doesn't quite match my ANET ET4 printer (the heated bed has a BLTouch sensor), and I’d like to avoid redrawing the whole thing from scratch. Thanks in advance. Ferda2
I need help finishing this part - hidden surface
保存エラー:十分なクォータがありません。
Annotating a drawing
DSM V6.1 failing to export .stl
Fix a failing STEP export in DSM v6.1
distortion of image (depth perspective)
Hatching
Opening multiple files from file explorer into a single DSM.
Nach Update auf V6.1: Keine Vorschau-Bilder (.rsdoc-Thumbnails) im Windows Explorer
Formula problem
Formula using degrees instead of radians
Countersunk Screw Hole
Changing scale ratio from 1:1 to 1:87
くりぬきについて
Request for conversion from *.stl to *.rsdocx
Frequently asked questions
这些 DesignSpark Mechanical 教程面向哪些用户?
这些教程专为所有学习使用 DesignSpark Mechanical 软件的用户设计,无论您是首次安装设置,还是正在处理 3D 设计工作流程中的特定环节。教程从界面入门逐步讲解,直至准备用于 3D 打印或制造的模型,涵盖软件操作的全过程。
我能从 DesignSpark Mechanical 教程中学到什么?
这些教程涵盖完整的机械设计软件工作流程,从下载安装软件和熟悉界面操作,到创建 3D 零件、处理装配体,以及准备并导出用于 3D 打印或制造的模型。
DesignSpark Mechanical 能否用于 3D 打印?
可以。DesignSpark Mechanical 非常适合设计 3D 打印零件。该软件支持使用直观的推拉工具创建和编辑 3D 几何体,并可将完成的模型导出为 STL 格式,直接用于 3D 打印机或打印服务。