- 登录、导航并设置您的首个电路仿真项目
了解 DesignSpark Circuit Simulator
通过我们的电路仿真设计软件教程,学习如何使用 DesignSpark Circuit Simulator,内容涵盖从构建和运行首个仿真,到测试运算放大器电路、滤波器、电源和逻辑电路,分析波形结果以及调试信号行为等方方面面。
无论您是初次接触在线电子电路仿真,还是正在解决特定设计难题,我们的指南都将逐步引导您完成完整的工作流程。
完成这些教程后,您将能够:
- 构建和连接电路设计,包括运算放大器、滤波器和电源
- 运行仿真并分析波形与信号结果
- 使用 SPICE 和 VHDL-AMS 查找、导入并创建元件模型
- 调试电路行为,并在转入硬件前验证设计
教程
通过我们循序渐进式的初级、中级和专家教程,让您轻松、快速地完成您从设计到模拟的旅程。.

入门和用户界面
了解如何登录、浏览和使用工具内的功能

开始一个新的电路设计
我们的如何操作指南是为了帮助您创建您的第一个电路模拟设计

模拟设计和查看模拟结果
了解如何使用工具内的功能来运行和查看模拟结果

使用模型
了解模型以及如何找到或创建一个模型
DesignSpark 电路模拟器社区
寻找灵感、获得支持并与其他 DesignSpark 电路模拟器创建者分享您的作品。
I have a complicated design. Recreating all componanats in simulator will take a long time. Is there any way to transfer schematic to simulator. Thanks If you are a first time user of DesignSpark Circuit Simulator and see a login error like below, then read below for the solution.
Follow these steps:
Erase cookies for your current browsing session. Or open browser Incognito mode.
Go to the software page: https://explore.partquest.com/designspark
Click 'First time user' button, enter your DesignSpark registered email id and follow remaining steps to activate the program.
In the future, you can click the login button straightaway.
When I try to acees DesignSpark Circuit Simulator, I'm requested to login and then get the following error
There was an error when authenticating against the external identity provider: The user account must be pre-created. Please contact your system administrator. The DesignSpark Circuit Simulator software will be undergoing maintenance and it will be unavailable for 4 hours:
Scheduled 09-October-2025
Start: 14:00 EDT / 18:00 UTC
Ends: 18:00 EDT / 22:00 UTC My name is Yuji Miura.
I am new to Design Spark Circuit Simulator.
I have two points I don't understand.
When I try to connect analogue electronic components to digital electronic components, I get the message "Cannot connect different technologies, insert a converter block". I don't know how to insert a converter block.
I want to use a comparator called ADCMP501, but there is no comparator item in the Datasheet Model Builder and I don't know what to do.
Can someone please tell me how to do this? The DesignSpark Circuit Simulator software will be undergoing maintenance and it will be unavailable for approximately 30 minutes:
Scheduled 27-March-2025
Start: 12:00 EDT / 16:00 UTC
The DesignSpark Circuit Simulator software will be undergoing maintenance and it will be unavailable for the following 8-hour period:
Scheduled 28-February-2025
Start: 12:00 noon ET
End: 8:00pm ET DesignSpark Circuit Simulator is a cloud-hosted and browser-based software. Users benefit from an always up-to-date software without the need to download anything. These frequent updates add new features and improve user experience. The following changelog summarises the updates on a monthly basis.
https://www.rs-online.com/designspark/designspark-circuit-simulator-changelog
Hmmm… can't reach this page
It looks like explore.partquest.com closed the connection
Try:
Checking the connection
Checking the proxy and the firewall
ERR_CONNECTION_CLOSED
You can find our Circuit Simulator FAQ section here:
https://www.rs-online.com/designspark/designspark-circuit-simulator-support-faqs
Happy Designing!
I use DesignSpark PCB and I have schematic design, so I want to import the design into DesignSpark Circuit Simulator. I'm using the simulator for the first time to look into the pulse control of a DC motor with a frictional load using a MOSFET H-bridge. Having experienced difficulties with the results, I have simplified the design greatly to that detailed in MAG2 which simply powers up the motor with 24V to its steady state before switching the power off. I would expect the motor speed to decay to zero as its inertia dissipates. Why doesn't this happen? Hi, my name is Riccardo and I'm a new user. I'm working with the browser version of DesingSpark Simulator and I ask you if there's a funcion that creates an automatic Bill Of Materials (I'm working with very basic components, such as resistors, capacitors and leds).
Thank you so much for the answers. Although the automotive industry is moving rapidly toward electrification, there is no reason to stop improving the performance and efficiency of traditional gasoline engines. New power electronics technology from Nexperia can help with that too!
Accurate fuel metering is important for robust engine control, and that translates into tight timing requirements for the fuel injector opening and closing. One method to improve the response of the injector closing is to provide a large back-voltage at the end of the injection event, to rapidly reduce the injector solenoid current. This back voltage can come from the “avalanche” of the main injector driver switch. That switch must be rated to handle repeated avalanche conditions, like the BUK9K13-60RA 240-1816 Power MOSFET from Nexperia. This fuel injector driver example shows the benefit of using that part for better timing control of fuel injector cut-off.
Read the full article at:
https://www.rs-online.com/designspark/quick-off-injector-driver-for-tighter-fuel-metering-using-a-nexperia-power-mosfet
You can find Schematic and PCB reference designs for DesignSpark PCB software and live circuit simulation reference designs for DesignSpark Circuit Simulator in this reference design centre.
For example, check out Siemens' article about
Tighter Fuel Metering with a "Quick-Off" Injector Driver
This and more at https://www.rs-online.com/designspark/reference-designs
Using Current DesignSpark PCB Schematic for simulation
First time user of DS Circuit Simulator and getting a login error? Click for solution.
Unable to access DesignSpark Circuit Simulator
DS Circuit Simulator - scheduled downtime for maintenance (October 2025)
Beginner's Question
DS Circuit Simulator - scheduled downtime for maintenance (March 2025)
DS Circuit Simulator - scheduled downtime for maintenance (Feb 2025)
DS Circuit Simulator Changelog
Unable to launch Circuit Simulator?
Did you know? DS Circuit Simulator FAQs
Can I import my design from DesignSpark PCB?
DC motor simulation
How to create an automatic Bill Of Material?
Tighter fuel metering with a 'quick-off' injector driver
What are reference designs for Circuit Simulator?
Frequently asked questions
DesignSpark Circuit Simulator 是免费使用的吗?
是的。DesignSpark Circuit Simulator 随 Explorer 计划免费提供,包含无限数量的公开设计且无隐藏费用。无需下载;您可以直接在浏览器中访问并运行仿真。针对需要延长仿真时间和私有团队协作的工程师,还提供 Creator 和 Engineer 付费计划。
这些 DesignSpark 电路模拟器教程适合哪些人?
这些教程专为学习使用 DesignSpark 电路模拟器的人设计,无论您是首次运行模拟,还是正在解决特定的电路设计难题。教程循序渐进地指导工具的使用,涵盖从登录、界面导航,到构建设计、运行模拟及分析结果的完整流程。
我通过 DesignSpark 电路模拟器教程能学到什么?
教程覆盖完整的模拟工作流程——从设置首个电路设计、使用元件模型,到运行模拟、分析波形结果,以及调试信号行为。涉及的实用电路类型包括运算放大器电路、滤波器、电源和逻辑电路。
使用 DesignSpark Circuit Simulator 需要下载任何内容吗?
不需要。DesignSpark Circuit Simulator 完全基于浏览器运行。您只需拥有网络连接和一个 DesignSpark 账户即可。这意味着无需安装即可在任何设备上使用,这也是其相较于传统桌面电路仿真工具的主要优势之一。