入门
了解如何下载、安装和登录软件
使用我们为初级、中级和高级工程师提供的分步教程,在从设计到制造的过程中先发制人
了解如何下载、安装和登录软件
学习如何浏览和使用软件内的功能
"我们的如何操作指南可以帮助您构建您的第一个可打印设计 "
了解 3D 模型以及如何使用它们
使用软件内的功能来完成您的项目
准备您的 3D 项目设计,以便打印它
寻找灵感,获得支持,并与其他 DesignSpark Mechanical 创作者分享您的作品。
According to the subscritions page, the DSM versions of Creator & Engineer are the same. Just checking is that the case? Or does engineer have some extras? (I know there are differences with PCB) Hi
I'm trying to install DSM603 but gets the meassage Missing connection to Microsoft Defender Smartscreen, What is that? How to fix it? As our range of products grows, it would be very useful to be able to work out on which assemblies a part is "used on" . This way if I am modyfying a part used on multiple assemblies I can check the change works in each instance. My design register is just a simple spreadsheet and doesn't have this feature , in any case it would be difficult to manage. Within design Spark is there any way to do this ? Any tips how to manage this ? I have been trying to run DSM on the Mac and managed to get it loaded and it appears to respond but!
The home screen window for the design is blank ,no plane showing.
It will not load any of my old STLs
Am I wasting my time trying to get it to work? 你好。自动重新安装电脑windows系统后一直提示这个无法完成注册。试过用代理。用手机流量等。请问应该如何解决。
Hi,
I'm using quite a while a creator plan of DS Mechanical on two different computers (Desktop and Laptop). My Laptop crashed an I installed DS Mechanical on my new laptop. But I'm not able to login. App comes up with a registration error. I guess this is due to the limitation of a maximum of 2 computers for the respective license. But how can I fix this, as I can't log off from my old laptop anymore?
Any help is appreciated,
Kind Regards
Sebastian Hello,
I'm creating a flat round logo 7mm. high, and I'd like to curve it upwards to look like a car logo.
I don't know how to say to make an extrusion but slightly round from the top center.
David I have noticed that since upgrading to 6.0.3 many times the stl files are the wrong size when imported into a slicer program such as Lychee or Anycubic Workbench.
As a test I created a simple part, DSM says the largest block is 9mm on each side, importing into either slicer and the dimension have shrunk to .01 mm.
What's going on?
Buongiorno,
Mechanical con licenza Creator.
Oggi fa così "DesignSpark Mechanical ha riscontrato un errore durante la registrazione"
Mi hanno appena sostituito la scheda madre del PC...ma non vedo alcun nesso...
Succede a qualcun altro?
Grazie Bonjour je rouvre DSM6 depuis plusieurs semaines sans utilisation et la, le fond de ma conception reste noir ?
Quelqu'un à t'il une solution ?
Merci par avance
Albert With a Creator or Engineer subscription, DesignSpark Circuit Simulator allows your simulations to run longer than 1 minute and upto 1 hour of server compute time.
Our Circuit Simulator was introduced last July and can be a good tool for DS PCB users, and we know that some of our DSM users also do PCB designs...
We list some key reasons why you may need an extended simulation time:
Run electro-thermal transient simulations long enough for temperatures to reach steady-state, to verify reliability under real world operating conditions.
Allows compute-intensive simulations, such as switching power electronic circuits, to run as long as necessary for line and load transient response tests.
Monitor the behaviour of critical components to varying inputs over an extended time period, such as for vehicle drive-cycle simulations.
Check it out at https://www.rs-online.com/designspark/designspark-circuit-simulator
表題の件、1度目はできたのですが、2回目からは下記のようなポップアップがでてダウンロード出来なくなりました。解決方法はありますでしょうか?
記
Demonstrating the powerful but unusual edge and face rounding that DesignSpark (Parasolid) has... REJOICE !
Alternatively, pull two edges a small way, then pull in opposite direction to make a full round.
and for circular rounds, select two edges , pull to create a round on each edge a little, then pull in opposite direction.
To remove the full round, select and Fill.
This also works for eccentric round edge pulls as below gif:
Other tapering helical multi-sided with rotational sections are easily made with DSM if needed.
会社のデスクトップでCreatorを、出先のノートパソコンでExplorerを、一つのメールアドレスで使うことができません。どちらかがストップします。併用すること不可能ですか。 「ビュー」など、種類の文字が「作成」欄により半分書けてしまう。
DSM Creator v Engineer
DSM603 - Microsoft Defender
"used on" - Which Assemblies
Will DSM run on a MAC with a Windows emulator
你好。自动重新安装电脑windows系统后一直提示这个无法完成注册。试过用代理。用手机流量等。请问应该如何解决。
Registration Issue when trying to login on a new laptop
how to curve it upwards
DSM 6.0.3 producing inaccurate .stl files
DesignSpark Mechanical ha riscontrato un errore durante la registrazione - error while registering
Espace de travail reste noir ?
What does more than 1 minute of simulation time allow you to do?
3Dモデルのダウンロードができない。
Pull Rounds in DSM v6 - standard radical functionality available to all.
複数のパソコンで使用する
パネルの種類文字をきちんと見たい