- Accueil
- Communauté
- Forums
FORUMS DESIGNSPARK
Communiquez librement avec d'autres membres de DesignSpark via les forums. Créez de nouvelles conversations ou rejoignez les discussions existantes concernant les produits, la technologie, les logiciels et l'innovation future. Aidez à trouver des solutions ou cherchez des réponses à vos propres problèmes techniques en faisant appel à un réseau international d'ingénieurs partageant la même vision.
お世話になります。
投影で円を別の図形に投射すると、円の点が多点になる現象があります。
どの項目の設定を直せば良いでしょうか?
小さい円の場合は多点になりません。 Hi,
I am using Design Spark Mechanical Creator. The dwg & dxf export does not capture all geometry. See screenshots below. The first image is a screenshot of a sectioned drawing in a drawing sheet in Design Spark. The circled red geometries are not all captured when the drawing has been exported to dwg or dxf file when viewed in AutoCad or Sketchup: See 2nd screenshot. In the 2nd screen shot only one of the circled geomteries were captured and rest of the same geometries were not. I have tried all possible export options aswell as both Teigha and Autocad Real dwg translators to no avail. Is this a glitch with translators? Please advise.
If I draw 4 rectangles:
I can pull the 'green areas but not the white. How do I change this? Thanks in advance. DS PCB 11.0 does not show 'auto-rename components' in Tools menu.
My design has four schematic and 472 parts in the projects. Is there some limitation?
Hi
I need help for insert, in a folder, a cartouche. I don't find the mode for create or use one of thats.
Thank.
Fabio I notice that PCB footprints are missing for most of the surface mount diodes, except for SOD80, so the common DO-214, SOD-523 etc are not there. Also some SM transistor footprints are missing. Is this a deliberate omission for the Explorer version?
Infact even the humble 1N4148 diode is not present in the pre-loaded components list.
Because the footprints are not there, the component import does not successfully run.
Did I make an error in installing the software or do I have to create these components?
我的融合功能导轨键在使用中会使整个融合面消失,查了几天的选项栏目找不出哪里的选项出错。 Hello, I need schematic and pcb of GSM800L module
this is what I see direct after start of Programm. When I click somewhere on Screen or hit a Key some Menupoints and Icons go away. What's going wrong here?
I'm trying to create a rectangle and then extend it into a 3D model.
When I enter one of the dimensions, such as ".28125" and then move to
enter the 2nd. dimension, Design Spark Mechanical changes the
".28125" to ".5". Any time I enter a dimension, the system chnages it
to another value. Plz. help. HI Forum,
Just upgraded to v.11.0. My parts library is not here, but my schematics are.
Where do I import my v.10.0 parts library?
Thank you! designSpark Mechanical 使いこなし大全 2023/2/11初判p41で 3.7.3 削除 DELキーですが
ソリッド面を指定して 削除すると隣接する面を・・・・・・と有りますが
どのメニューボタンを 選択し 複数選択するのでしょうか?
ご教授ください。
Hi,
I have subscription.
Ver 6.0.3
Exporting Files (PDF/DXF) produce files however importing these files types to Inscape/LightBurn import nothing (as if the files are empty). Files from other software are imported with no issues.
Suggestions are welcome.
Tnx
hi, i am currently unable to login to desingspark PCB 11.0 as it says it is unable to activate or check my license, could i have some help with this? 无法登陆,有没有明白的教教我Nouveaux messages sur le forum
円の投影による多点現象
dwg & dxf export does not capture all geometry
How do I select faces to pull?
auto-rename components not found
Cartouche
Surface mount Diode footprints
求助:关于融合功能的选择导轨键
Schematic and PCB of GSM800L module
Some Menupoints fade away after first Click with Mouse or Keyboard
I'm a newbie.
Library not transferred
DEL キー
Export PDF and DXF produce empty files
Unable to login to application
无法登陆
Nos forums
Logiciel
Activist Engineering
Communauté
Aspirations en tant qu'ingénieur
- Publications
- 2
Forum sur l'automatisation industrielle
- Publications
- 54
Forum sur la conception électronique
- Publications
- 55
OKdo Rock
ROCK - Mise en route
- Publications
- 69
ROCK- Dépannage
- Publications
- 16