Power
star_borderSuivre
Can you provide skills and technology based learning material
How to Charge a Battery Safely Using Smart Power Selector Technology
How to Get Started with Power-over-Ethernet (PoE)
Ask the Expert - Siemens Power Management
A Look at the ST 3.6kW SiC PFC Totem Pole Reference Design Board
Calculate Quiescent Current to Extend Battery Life in Low-Power Portable Applications
How to Get Started Using the EE-Sim® OASIS Simulation Tool to Accurately Simulate Your Circuit Designs
Ask the Expert - Power design tools with Maxim
WITT Evolution - A new solution for remote power generation
Mains Power Monitor
We, at OKdo, have been working on a new video series and we're thrilled to announce that the first episode of "Projects with Pete" is now live on our YouTube channel.Join Peter Milne, an engineer with a passion for Linux and single-board computers, and myself as we explore the realm of Industrial IoT solutions in our Industrial Automation project series.In the first episode, we delve into building a secure MQTT Edge Gateway using the ROCK 4 Model SE single-board computer.We can't wait to hear your thoughts! Check out the episode and let us know what you think. Unlocking Industrial IoT: Building a Radxa ROCK 4SE MQTT Gateway! | Projects with Pete | OKdo (youtube.com) Good morning I'm looking for an instruction manual for the Windmoller Triumph V made in 1972. I would like if anyone has the pdf
this is the first page, and I have just this.
随着技术的不断发展和应用的普及,设备维保平台正日益成为企业管理和运营中不可或缺的一部分。本文将从技术的角度深入探讨设备维保平台的优势以及未来的应用前景。
数据驱动的维护管理:
设备维保平台以数据为核心,通过大数据分析和机器学习技术,实现对设备状态和维护需求的实时监测和分析。基于历史维护数据和设备运行情况,平台能够预测设备故障,并提供针对性的维护建议,帮助企业更好地制定维护计划,提高维护效率和成本控制能力。
IoT 技术的应用:
设备维保平台与物联网(IoT)技术的结合,为企业提供了全面的设备监测和远程控制功能。通过传感器和智能设备的连接,平台可以实时收集设备运行数据和环境参数,实现对设备状态的远程监控和管理,及时发现和处理潜在问题,提高设备可靠性和安全性。
高效的维护流程和资源优化:
设备维保平台通过优化维护流程和资源分配,提高了企业的维护效率和资源利用率。平台可以自动化维护流程,减少人工干预和错误,提高维护响应速度和准确性。同时,通过智能调度和资源优化算法,平台能够合理分配维护人员和设备,降低维护成本和能源消耗,提高企业的经济效益。
安全性和隐私保护:
在数据安全和隐私保护方面,设备维保平台采用了多层加密和权限控制机制,保障了企业数据的安全性和完整性。平台严格遵循相关法律法规和行业标准,对用户数据进行保密和保护,确保用户信息不被泄露和滥用。
未来展望:
随着技术的不断进步和应用场景的不断拓展,设备维保平台的未来前景十分广阔。我们相信,随着人工智能、大数据和物联网等新技术的融合和应用,设备维保平台将发挥越来越重要的作用,为企业的可持续发展和创新提供强有力的支持。
结语:
设备维保平台是当今企业管理和运营的重要工具,它不仅提高了企业的生产效率和运营质量,还为企业带来了巨大的经济效益和竞争优势。我们期待着与各位论坛会员共同探讨和分享设备维保平台的技术创新和应用实践,共同推动设备维保平台的发展和进步。
谢谢!
177_1781_2656 Mr.张(可免费试用维保平台)
I've got a project that uses JST-SM connectors. It's for an LED pole light which needs to be assembled/reassembled regularly. I'm finding the connectors quite delicate and the pins are getting damage when there's tension or during transport. Is there a more robust alternative I could use? The world has witnessed rapid technological advancements in recent years. One such innovation that has significantly impacted various industries is the all-in-one computer. These compact and versatile devices have revolutionized how businesses operate, particularly within the manufacturing sector. This article explores the ways in which all-in-one computers have influenced modern manufacturing processes and highlights their benefits for both small and large enterprises.
1. Enhanced Productivity through Streamlined Operations
All-in-one computers provide a user-friendly interface that allows manufacturers to streamline various operations, from design and development to production management. By consolidating all necessary applications on one device, employees can work more efficiently, leading to increased productivity across the organization. Additionally, these devices offer touchscreen capabilities, which enable users to interact with software intuitively and effortlessly.
2. Improved Collaboration through Cloud-Based Technology
All-in-one computers are equipped with cloud technology that allows for seamless collaboration among team members, regardless of their physical location. This feature is particularly beneficial in the manufacturing industry where global supply chains and remote workforces are commonplace. With real-time access to project data, employees can efficiently collaborate on design modifications or production adjustments, resulting in improved communication and reduced errors.
3. Increased Mobility for On-the-Go Manufacturing Professionals
The compact nature of all-in-one computers allows manufacturing professionals to work remotely with ease. This mobility is particularly advantageous during factory inspections or when traveling between multiple facilities. By having access to critical information and applications on a single device, employees can make informed decisions quickly and efficiently, ultimately benefiting the overall productivity of the organization.
4. Cost-Effective Solutions for SMEs
All-in-one computers are an affordable solution for small and medium-sized enterprises (SMEs) looking to invest in advanced technology without breaking the bank. These devices offer a cost-effective alternative to traditional desktop PCs, as they require less space, fewer peripherals, and lower maintenance costs. As a result, SMEs can optimize their resources and focus on growing their business while staying competitive with larger organizations.
5. Scalable Technology for Future Growth
As businesses evolve and expand, so too must the technology that supports them. All-in-one computers are designed to be scalable, allowing manufacturers to easily upgrade hardware or software components as needed. This flexibility ensures that companies can adapt to new market demands and industry trends without having to replace their entire IT infrastructure.
Conclusion
The adoption of all-in-one computers in the manufacturing sector has led to significant improvements in productivity, collaboration, mobility, cost-effectiveness, and scalability. As technology continues to advance at an unprecedented pace, it is essential for manufacturers to embrace these innovations to stay competitive in today's global marketplace. By incorporating all-in-one computers into their operations, businesses can streamline processes, improve communication, and ultimately drive success within the manufacturing industry.
for more information In recent years, the rapid advancement of technology has given rise to a new era called "Industry 4.0." This industrial revolution focuses on automating processes through advanced robotics, artificial intelligence (AI), machine learning, and IoT devices. One essential component in this transformation is the Industrial AIoT Computer - an all-in-one device that serves as the brain of smart factories and production lines. In this article, we will explore the purpose and application of industrial AIoT computers from a professional perspective to understand their significance in today's fast-paced world.
1. What is an Industrial AIoT Computer?
An Industrial AIoT computer is a compact, ruggedized device that combines various functionalities such as computing power, connectivity options, and data processing capabilities. It serves as the central hub for IoT devices in industrial settings, allowing seamless communication between machines, sensors, and other equipment. The primary purpose of an Industrial AIoT computer is to facilitate real-time monitoring, analysis, and control over various processes within a smart factory or production line.
Key Features of Industrial AIoT Computers:
a) Ruggedized Design: These computers are built with durability in mind, designed to withstand harsh industrial environments such as high temperatures, vibrations, dust, and moisture. They often come equipped with IP65 or higher ratings for protection against water and dust ingress.
b) High Performance Processing: Industrial AIoT computers utilize powerful processors that can handle complex tasks like real-time data processing, machine learning algorithms, and advanced analytics. This enables them to make intelligent decisions on the fly and optimize production processes.
c) Multiple Connectivity Options: These devices support various communication protocols such as Wi-Fi, Ethernet, Bluetooth, Zigbee, and more, allowing seamless integration with existing industrial systems and IoT devices.
d) Expandability & Customization: Industrial AIoT computers often come with multiple expansion slots or I/O ports for adding peripherals like GPS modules, barcode scanners, RFID readers, etc., to cater to specific industry requirements.
e) Energy Efficiency: To reduce energy consumption and operating costs, these devices are designed with low power consumption in mind while maintaining high performance levels.
Applications of Industrial AIoT Computers:
a) Smart Factory Automation: Industrial AIoT computers serve as the control center for smart factories by monitoring production lines, analyzing data from sensors and machines, and making real-time decisions to optimize processes and increase efficiency.
b) Predictive Maintenance: By collecting data on machine performance and condition, these devices can predict potential issues before they become critical, allowing for timely maintenance and reducing downtime.
c) Quality Control & Assurance: Industrial AIoT computers enable continuous monitoring of product quality by analyzing data from sensors, detecting anomalies or defects in real-time to ensure that only high-quality products reach the end consumer.
d) Logistics Management: In supply chain management and logistics operations, these devices can track assets, monitor inventory levels, optimize routing, and manage deliveries for improved efficiency and cost savings.
e) Environmental Monitoring & Control: Industrial AIoT computers are used in industries such as agriculture, construction, and mining to monitor environmental conditions like temperature, humidity, and air quality, ensuring optimal working environments and safety standards.
Conclusion:
Industrial AIoT Computers have become an indispensable part of the Industry 4.0 revolution by bridging the gap between physical systems and digital technologies. By facilitating real-time monitoring, analysis, and control over industrial processes, these devices are helping industries transition to smarter, more efficient operations that benefit both businesses and consumers alike. As technology continues to advance at an unprecedented pace, it is essential for organizations across various sectors to embrace the potential of Industrial AIoT computers in their journey towards a digital future.
Jahone Chong
for more info
Hi - On our small vessel we have a 12v failry powerful motor to run the autopilot, where the power is supplied by the boat's battery bank. On an 'independant' system we have 240v that is supplied via an inverter, but the power originates from the same battery bank as the 12v system. The problem is that we have a laptop to run a piece of scientific equiptment, and when the laptop is plugged in to the 240v, it picks up interference whenever the 12v autopilot motor is actuated. The laptop only has to be plugged in - the socket can be switched on or off and the interference is picked up by the laptop. There is no interference on the laptop when not plugged in. So some kind of noise is crossing over to the 240v wiring i guess.
We have tried a couple things so far; adding more ferrites in various places, as well as using a voltage cleaner (a bit like a UPS) between the 240 socket and laptop but the interference still gets through.
I've been looking at things like an IEC in-line filter that I can just plug in to the 240 and laptop cord, but these seem to only filter noise generated from mains power. I'm not an electrician so i'm a bit unclear on what the solution might be, as i'm not actually sure what kind of noise it is that's being generated. Any advices welcome. Thanks.
Hello everyone,
I'm researching the contactors and thermal and electronic overload relays. In particular, I'm trying to understand:
The differences in the products provided by the large players (ABB, Schneider Electric, Siemens, Mitsubishi Electric)
The future trends in terms of technological innovation
Brand perception of the large players (e.g., ABB is good/bad because or xyz, and so on)
I wasn't able to find much online other than companies align to each other and tend to produce:
Compact frames to save space in cabinets
Universal coil to support both DC and AC
Wide range voltage support in coils
Modular hardware
Smart wiring connections
While for relays:
Current measurement and output of data
Remote monitoring features
IoT connectivity features
Smart wiring connections
Does any of you know:
1. What is likely to happen technology-wise in the next few years that could be innovative for the market?
2. What are the differentiators of the products provided by the large manufacturers?
3. How are the large manufacturers perceived and how are Japanese players perceived in the western market in terms of contactors and relays?
Thanks in advance for those of you who will read. Hi Everyone,
I am working on a low voltage (12V DC) application that requires the momentary activation of a device for a several minutes. I was trying to discover a suitable timer relay and came across some of the Weidmuller products, in particular the TERM series, however I am not able to figure out if they are momentary activation to start the timer, and whether or not the timer can be restarted mid-cycle by another input signal.Is anyone able to point me in the right direction for understanding these items?Any help much appreciated.Andrew Hi, does anyone know how to download the programming software for the RS Pro Logic Controller ( RS part no 917-6370). The data sheet has a Dopbox link that doesn't work?? Automation of artificial intelligence (AI) helps industries by increasing efficiency, lowering costs, improving decision-making, improving consumer experiences, limiting risks, and speeding up innovation. It automates tasks, reduces errors, swiftly analyses data, provides personalised customer assistance, discovers abnormalities, and encourages creativity. Overall, artificial intelligence automation enables enterprises to optimise processes, promote growth, and remain competitive in the digital era. Hello everyone, I am a lover of machine structures, so I have recorded videos of machine structures on my youtube channel for everyone to refer to and learn from each other, Structural designs of all kinds machines such as filling machines, packing machines, robotic arms, automatic assembly machinesLooking forward to everyone's comments
https://www.youtube.com/watch?v=STC-85-gQmw&list=PLxq4Yft5Rsyf5UKhVWRpfFx3NLxtMUh8Q&index=1 Hi There!
I need to turn on-off a set of 6 digital outputs (relay is iok) from a custom designed PC windows program.
My client already has a S7 1200 PLC wired that has never used. This would be a good solution as he already has a UTP cable from his computer to where all these 6 machines are
Is it easy to interact from a Windows program with a S7 1200 PLC just to turn on-off these DO's in the PLC? Does it need to use OPC or can another simpler protocol be used?
If not, is there an easier solution? (Siemens Logo PLC's?)
Thanks a lot!
As most of this community knows Power control is a vital aspect of the UK industry, with the potential to save companies money, improve efficiency, and reduce environmental impact. That is why I open this discussion with this United Automation article blog on:
https://www.united-automation.com/benefits-of-power-control-solutions-in-the-uk-industry/
After reading this article, I wonder what industries are doing to save energy and be more sustainable with planet Earth.
I want to run some mahines in an industry automatically in different time.Each machine will have a specific time to run.Industrial Automation Forum
Building a Radxa ROCK 4SE MQTT Gateway
WindMoller & Holscher Manual
深度解析:设备维保平台的技术优势与应用前景
Alternative to JST-SM connector?
The Impact of All-In-One Computers on Modern Manufacturing Industry
Application for industrial all in one computer--------Jahone
12v motor causing noise in 240v system
Differentiators in electromagnetic contactors and safety relays
Need help selecting suitable relay(s) for control system
RS Pro Logic programming
Artificial Intelligence and Automation for Transforming Industries
Structural design of machines such as filling machines, packing machines, robotic arms, automatic assembly machines
Control 6 digital outputs (PLC) from a windows computer
Power control in the industry
Can i make an automated systems to run all the machines in a industry in a specific time?
Power
star_borderSuivreFilters & Sorting
No content yet for "Tous"
No content yet for "Articles"
No content yet for "Projets"
No content yet for "Nouvelles"