你觉得这篇文章怎么样? 帮助我们为您提供更好的内容。
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
你觉得这篇文章怎么样?
So we’ve talked about various components in an EPA before (e.g. lab coats, bags, tape and so on). But there is one important part we have not covered yet: ESD protective working surfaces. So let’s change that right now!
Definition of an ESD protective working surface
ESD protective working surfaces aid in the prevention of damage to ESD sensitive items (ESDS) and assemblies from electrostatic discharge. ESD working surfaces, such as mats, are typically an integral part of the ESD workstation, particularly in areas where hand assembly occurs. The purpose of the ESD working surface is two-fold.
- To provide a surface with little to no charge on it.
- To provide a surface that will remove ElectroStatic charges from conductors (including ESDS devices and assemblies) that are placed on the surface.
Types of ESD protective working surface
When deciding to invest in ESD protective working surface, you have the choice of ESD matting (laid-out on a standard non-ESD bench) or ESD benches. Performance-wise there is no difference so what option you go for depends solely on your personal preference.
Examples of ESD protective working surface matting - for more details click here
Generally speaking, ESD matting offers a lower initial investment and is easier to replace. On the other hand, some people prefer the robust and consistent approach of ESD benches.
Grounding your ESD protective working surface
Whatever your choice, your ESD protective working surface needs to be grounded. A ground wire from the surface should connect to the common point ground which is connected to ground, preferably equipment ground. For electronics manufacturing a working surface resistance to ground (Rg) of 1 x 104 to less than 1 x 109 ohms is recommended. Best practice is that ground connections use firm fitting connecting devices such as metallic crimps, snaps and banana plugs to connect to designated ground points. The use of alligator clips is not recommended.
Example of an ESD Protective Working Surface - click here for more grounding products
Using a current limiting resistor in the ground cord is the user’s choice. However, the resistor is not for ESD control purposes. The ESD Association standard for grounding is ANSI/ESD S6.1 which recommends a hard ground (no resistor) but allows the use of a current limiting resistor in the mat’s ground cord. “The grounding conductors (wires) from wrist straps, working surfaces, flooring or floor mats, tools, fixtures, storage units, carts, chairs, garments and other ESD technical elements may or may not contain added resistance. Where added resistance is not present, a direct connection from the ESD technical element to the common point ground or common connection point is acceptable and recommended.
Note: Manufacturers may add resistance to the grounding conductors for purposes other than ESD (e.g. current limiting). Added resistance is acceptable for the purposes of controlling ESD provided electrostatic accumulation does not exceed specific EPA requirements. The typical added resistance in grounding conductors is 1 megohm, although other values may be specified.” [ANSI/ESD S6.1 section 5.3.3 ESD Technical Element Conductors]
Working at an ESD protective working surface
Operators should ensure that the working surface is organized to perform work and that all unnecessary insulators and personal items are removed. Regular plastics, polystyrene foam drink cups and packaging materials etc. are typically high charging and have no place at an ESD protective workstation.
An operator installing an ESD protective working surface mat
Insulators can be a considerable threat to your products. Remember that an insulator cannot be grounded so it will retain its charge for a long time. Removing all non-essential insulators from the ESD protective workstation is an important rule. If not, your company’s investment in the grounded ESD working surface may be wasted. “The biggest threat is Field Induced Discharges, which can occur even at a properly grounded ESD working surface. If an ESDS is grounded in the presence of an ElectroStatic charge, instead of the ESDS having charges removed from it, the ESDS may become charged with a voltage induced on it. Then, when placed on the grounded ESD work surface, a discharge occurs. If the ESDS is removed from the presence of the ElectroStatic charge and grounded again, a second discharge may occur.“ (Ref. ESD Handbook, ESD TR20.20, section 2.7.5).
Maintaining your ESD protective working surface
The ESD working surface must be maintained and should be cleaned with an ESD cleaner. Regular cleaners typically contain silicone and should never be used on an ESD working surface.
Example of an ESD cleaner
The ESD control plan should require testing of the resistance to ground periodically. For more information on testing your ESD working surface, check this post. However, the operator should be on guard every day and check visually that the ground wire is attached.