你觉得这篇文章怎么样? 帮助我们为您提供更好的内容。
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
你觉得这篇文章怎么样?
Hello, everyone. I am George who is a year three student studying in City University of Hong Kong. In this summer, I started to work as an internship trainee in RS Components. During this period, I worked with my partners who are also the internship trainees to finish several projects. One of these projects is to design an Analog Car. In the following, I am going to share what I have done and what kinds of problems faced in this design.
In order to improve the laboratory of EE2109 of City University, we are requested to combine and design a new laboratory of it. In EE2109, students will learn about transistor, operational amplifier, diode, and filter. To combine these technologies and design a interesting laboratory, we decided to design a basic simple Analog Car circuit.
Design:
For a basic Analog Car, it should have two wheels that controlled by two signals. Therefore, we only need two things and they are signal emitter and receiver. In the following, we first focus on the signal emitter – Remote.
For a signal emitter – Remote, we need to generate two signals that controlling two wheels to on or off. For example, we use LED bulb as an emitter, then what we need is an oscillator to generate a frequency and emit though the LED bulb. Besides that, we need an amplifier to ensure the signal emitted is strong enough or not. Therefore, we need to have two sets of this to control two wheels on or off.
Material List:
RS part number |
Manufacturer |
Manufacturing number |
Description |
Quantity |
522-2693 |
Bourns |
3386P-1-103LF |
Variable resistor 10K
|
4 |
479-1390 |
TE Connectivity |
FSM2JH |
Switches
|
2 |
761-3546 |
Fairchild Semiconductor |
LM358N |
IC |
1 |
773-3996 |
Vishay |
TSUS5202 |
IR LED |
2 |
787-4864 |
C & K |
OS102011MS2QN1 |
Power switch |
1 |
744-2202 |
RS |
744-2202 |
9V Battery |
1 |
|
|
BC109 |
Transistor |
2 |
Breadboard:
To check whether it is work or not, we first need to test it on a breadboard. We put all the components, the output is different from what we expected. There are some errors exist. After debugging it, we added some variable resistors to control the voltage gain. Also, we set up a virtual ground to separate the signal ground and common ground.
Schematic:
After a first test on the breadboard, we try to draw the schematic of the circuit on computer. By using the design spark PCB, we can find most of the components from its powerful libraries. However, some components such as variable resistor and battery holder do not exist in the libraries. Then, we can use its model source function. This function enables us to search some components online and directly put them into the design spark PCB. Moreover, we can draw the components by us in design spark PCB.
PCB
Using the Design Spark PCB again, we can convert the schematic to PCB layout. What we need to do is print the layout and buy a copper board. After the PCB fabrication, we can start to drill the hole for components and double-check the copper routes.
After installing all the components on the PCB, we can use the CRO to check whether the frequencies emitted are 5kHz and 1kHz or not. Moreover, we can adjust the strength of LED bulbs and the gain of signals generated.
>Conclusion<
If you are following what we did before, you will get two perfect 5kHz and 1kHz signals emitter. However, if you want to design your own circuit, you can modify it to become yours. Design to enjoy, enjoy your designing. Thank you.
This article is only including the remote part of the Analog Car. For the car body part of the Analog Car, you may refer to another article.