- Accueil
- Communauté
- Forums
FORUMS DESIGNSPARK
Communiquez librement avec d'autres membres de DesignSpark via les forums. Créez de nouvelles conversations ou rejoignez les discussions existantes concernant les produits, la technologie, les logiciels et l'innovation future. Aidez à trouver des solutions ou cherchez des réponses à vos propres problèmes techniques en faisant appel à un réseau international d'ingénieurs partageant la même vision.
Hello guys,
Iam using Designspark PCB 10, when iam trying to open Schematic filr 403 error is coming.
Please provide me solution.
Regards,
Eswar Reddy.K I just upgraded from DesignSpark PCB 10 to 11. Now I am getting Error code 87 at the startup. The error screenshot is pasted below. How to solve this?
Hi to all, maybe this info is outdate for somebidy but i want to share.
In my case: remove DS SPARK V10 i have used REVO UNISTALLER TOOL for total and secure clean;
reinstalled DS PARK v11 (the v10 is out of date and not supported now) remember ADMINISTRATOR RIGHT;
Change your PASSWORD of login in DESIGN SPARK site (is the same for login software) and use a simple password that does not exceed 11 characters;
My experience Sergio.
I know sheet metal is not available, but how does one make a bended plate in such a way that via a stp export Sophia of Tailorsteel is able to process it? Hi,
I'm looking to put a 25° angle on a section of a 3D model. Do I need to split the model and then put in the angle or can I put the angle in another way? Hello
Actually with designsparkV11.0, my library is empty.
Anyone can help me please. How to download, all library necessary for designspark.
Thanks....
Hello,
try to login at DesignSpark Electrical 2018 SP3 (installed on my laptop), then get "Unknown error".
On the wbsite I can login with mine account, please help.
Thanks Rijk
DS has been nothing but a messy, buggy pile of nonsense for years now. Now to top it all off, V10 will no longer run because it can't verify (403 error) so I am forced to install version 11 and 'Richard' around with the libraries, again. Exclamation Mark.
I am porting all my projects to Ki-Cad and this software is getting the boot. I have been using Ki-Cad for a number of years now, and everything just works better.
Also, loving the AI on this forum that flags complaints as spam when you dare to use a single exlamation mark to emphasise how pevved you are.
jpg Import ist gut und schön... nach Update und Einführung der erheblichen Einschränkungen ist diese Funktion auch zwingend nötig.
Leider ist die Größe der Dinge falsch, zu klein. OK, verstehe ich auch, woher sollen auch Maße kommen...
Der Faktor ist etwas 2,85 Siehe auch
Frage wie kann, wenn überhaubt die Größe angepasst, korrigiert werden? Trying to draw something simular to a ladder,But when I try to pull the "rungs" the pull command hilights the space between the rungs and will only allow me to pull them.
Annoying thing is I was able to pull the rungs in the past, so what has changed? I am in the middle of a project using DS 9.
When I attempted to open the project today I found DS 9 now refuses run so I was forced to install DS 11.
Now I find all the libraries I was using with DS 9 are missing from the list in DS 11. The DS 9 project is broken. Because I can't even run DS 9 I am now unable to determine which libraries I was using or the order in which they were searched. The order is important because some items may have had the same names.
I think I had libs included from DS 7, DS 8 and DS8.1 that were held in...
C:\Users\Public\Documents\DesignSpark PCB 7.0\Library
C:\Users\Public\Documents\DesignSpark PCB 8.0\Library
C:\Users\Public\Documents\DesignSpark PCB 8.1\Library
The DS 7 Libraries include additional folders called 'DownloadedLibrary', 'MountingHole' and 'SnapEDA' so I'm pretty sure those were included somewhere in the list.
When DS 9 came along, libraries were moved into
C:\Users\<user name>\Documents\DesignSpark PCB 9.0\Library
This completely screwed things up for me and I had to modify the library list to include the original folders under Public\Documents.
I can't remember if the new DS 9 libs were left included in the list or if I removed them.
All the problems this caused is why I subsequently avoided updating from DS 9 to DS 10 or DS 11.
Now I have no choice.
How can I find out which libs were included and the sort order? It's important that I get everything back to how it was before DS 9 was disabled otherwise it could break things and introduce errors that could go unnoticed.
IMHO completely disabling older versions of DS is a REALLY bad idea. Why can't they continue to run in read only mode so that at least users can examine library and technology files etc. while transitioning to the new version. It's a bit like Microsoft completely disabling Windows 10 and preventing access to existing files before users have moved to Windows 11.
After previous updates (DS 7 through to DS10), earlier versions continued to run. It was left to users to decide whether to update and/or keep earlier versions. That way users were immunue to new bugs or unwanted changes that might disrupt existing projects. Why have you now chosen to completely disable earlier versions? You don't have to support them, just allow them to run as before. It makes no sense.
In my view the fundamental problem here is that the list of libraries and the search order are user selectable options. As such, they should be stored as part of the project file and not overwritten every time DS is updated. I can't imagine anyone wanting to pay a subscription fee for flawed software. Hi all,
I have a problem with opening some of the DSM V.5 files in DSM V6. This is interesting because some of the files opening without any problem and when I try to open other the program is starting and freeze during loading file without any error notification. The file is loading and progress bar freezes in about 30 %.
I’m working on DSM Creator.
I can view all of the files in DSM Viewer however I cannot open them…
Dose any body had the same issue and have any solution for this? Ver11の使用を始めたのですが、grids設定ウインドウの□[mm]の数値を変更してもgridsの間隔が全く変化しません。どのようにすれば、gridの間隔を変更出来るのでしょうか。デフォルトの10.2mmから全く変化がありません。
Discover how one member is using our design software and tools. With PCB design, Circuit Simulation, and 3D mechanical design software in each package (including our free version), we discover why Connector Geek selected the Creator package.
https://www.youtube.com/watch?v=VFFwWYq0gOQ
Leave us a comment below about the video! ミラ線を利用して長方形を作りました。
その後幅のサイズを修正したら、
幅が片側が正しく延長しました。片側が間違いました。
因みに高さが両サイドが正しくつくりました。
不具合と思います。Nouveaux messages sur le forum
Error 403
Error code 87
ERROR 403 or CREDENTIAL ERROR SOLVED
Sheetmetal is not available
Bend or Split 3D model
Library files
error login
DS PCB is awful.
jpg Import Größe
Pull command
Forced to install V11. Unable to determine libs or sort order for DS 9 project.
Problem with opening DSM V.5 files in DSM V6.
gridsの設定について
Interview with ConnectorGeek
bug
Nos forums
Logiciel
Activist Engineering
Communauté
Aspirations en tant qu'ingénieur
- Publications
- 2
Forum sur l'automatisation industrielle
- Publications
- 53
Forum sur la conception électronique
- Publications
- 54
OKdo Rock
ROCK - Mise en route
- Publications
- 69
- Nouveau
- 1
ROCK- Dépannage
- Publications
- 15