Hi all.
Ver 9.x of DSPCB has Goto function. It is useful when to find thing in the schematic drawing.
However, I am afraid of the action of 'Net' (in the pull down menu of 'Goto') .
As you know well, that is in the interaction bar.
1. Under the condition of two or more same name nets separate by bus,
single click net name of 'Net' makes to get only one net.
( I do not know how to get another place of same name net by using 'Goto'.)
I hope to get another place of same name net by using single click together with Alt key.
2. At that time, if you double click instead of single click, it will pick up all net that have same name.
( It is OK if you can see all of them on the screen at one time, but lost or screen out is existing, it will dangerous.)
3. The selected net by 'Goto' is different by select command.
Refer to the attached.
'seg_c' of DISP1 is selected by 'Goto'.
'seg_c' of DISP2 is selected by select command.
There looks are closely same.
The different point is only color of pin number 7.
Under this condition, push delete key. the result as follows.
In this conclusion, The 'Goto' of net picked the net and the connected components.( But components does not change color of selected, only pin number color changing.)
So, the delete action after 'Goto' net will delete net and component that connected selected net.
The 'Goto' function is so so good. So, I hope to request revice the action of 'Net' in 'Goto'.