How do you feel about this article? Help us to provide better content for you.
Thank you! Your feedback has been received.
There was a problem submitting your feedback, please try again later.
What do you think of this article?
近期翻开报纸不难看到许多关于5G的新闻。仿佛全世界为了5G而疯狂,媒体不断报道。国家之间更为了5G之事而发生了争执。人们饭后话题也时不时谈到5G。那么什么是5G呢?究竟是什么原因让人为了他争到头破血流呢?以下是我一些看法。
想要了解5G,我们得先了解一些历史。
翻看历史,从1G时代开始,几乎每隔十年就会增加一个G。1980年代推出了1G,90年代推出了2G,2000年开始使用3G,2010开始了4G时代,而5G预测将在2020年到来。这现象有点类似摩尔定律。摩尔定律由英特尔创始人Gordon Moore大致上说电脑中集成电路的晶体管每两年会翻一倍。这个定律至今仍然引领着IT行业,许多人因为轻视这个定律而失去竞争力,例如太阳公司还有摩托罗拉公司。
从1G到4G
摩尔定律
5G必然跟4G有些不同的地方或者优势。那么他的不同之处在哪里呢?优势又在哪里。
许多人了解5G与4G的差别在与速度方面,认为5G就是比4G快了很多倍。但生活中4G已经足够快了,再快我们也感觉不出明显的区别。但如果是下载影片或大容量的文件时,我们就可以明显感受到区别了。下图是2G至5G之间的速度区别。
明显可见,使用最新的4G中的LTE-A技术所得到的最高网速是5G的最低网速。举个例子,我们下载一部蓝光版(Blu-Ray)影片(假设是15GB/15000MB)的话,LTE-A耗时2分钟多。倘若使用5G的话,假设一直保持最高速度下载的话,只需耗时12秒就能下载完毕(但现实中往往不会达到最高速度)。如果是平时看视频的话,对于一个HD(高清)的影片来说,5Mbps的速度已经非常足够了。显然4G能够满足我们的需求,因此5G在速度方面是有优势的,但对于大众来说,这个优势并不明显。
5G与4G有个明显的差别,在于他们的电信塔。4G电信塔是这样操作的。塔每隔一段时间发射固定信号,那么在这个区域内的用户收到信号的话就可以使用了。但这样有一个坏处,即他的范围内如果没有用户的话,那么塔还是会持续发射信号。这就会导致能源上的浪费。而5G电信塔是他的区域内有多少个用户,那么他就发射多少个直线式的信号到用户终端上,这就是5G的优势,即能源上的节省。
5G信号塔与4G信号塔之间的区别
还有一个优势就是延迟,latency。4G的延迟可达100-200ms级别,但5G理论上可以降低一百倍到1ms。实际上测试的数据显示5G的延迟平均在30ms级别左右(根据美国官方白皮书)。但这对于金融业来说是个好消息。时间对于商人来说可说是金钱。延迟对于投资者来说可能会造成损失。几秒的消息延迟,可能会让他们错过买入/卖出股票的良好时机。因此,许多人会为了更少的延迟而买5G的单。
提供或售卖5G服务的公司有高通(Qualcomm),华为,中兴(ZTE),三星(Samsung),诺基亚(Nokia)等等公司。其中以高通和华为为行业中的领头羊。
吃下这个大饼的好处在于可以成为5G行业中的霸主。5G属于IT行业。根据以往IT行业的例子我们可以看到霸主可以通吃整个领域。总结如下:
微软通吃电脑操作系统领域,市占率高达83%。
Intel(英特尔)通吃电脑芯片领域,市占率高达80%。
Google(谷歌)通吃搜索引擎领域,市占率高达90%
谷歌的Android(安卓系统)在手机操作系统中的市占率达76%。
以上例子阐述了,在IT行业中,接近垄断的情况是很常见的。而称霸的公司则可以得到非常丰厚的利润。现在,我们来看看以前3G和4G的例子。
3G时代可以说是高通称霸天下。当时高通制定了3G的标准制度可说是制定了游戏规则。手机行业刚刚兴起,大家对于新鲜事物很新奇。每个人都奢求一台大哥大。殊不知,一台电话有大部分的成本是要支付高通专利费。举个如今的例子平均一台iPhone需要支付高通7.5美元的专利费。这是多么大的利润啊。况且4G是以3G为基础之上来发展。虽然4G时代由欧洲公司开始反击让的高通的专利比例有所下降,但高通仍然握有4G核心专利,因此4G时代高通还是高高坐在宝座上,没什么人可以撼动。高通通过4G也赚了不少,据统计可达几百亿美元。可见,这块大饼多么的让人眼红,但是被高通占去了一大部分。如今,大家自然希望能够拿下5G这块新的大饼,为此而打架就能够理解了。
自动驾驶,远程医疗,物联网等等新科技都是需要5G为基础发展的行业。以往的3G或者是4G只能连接在手机一些终端上面。可是,以上科技大大地拓展了5G的市场,使得他的客户不再是局限于手机上面,像冰箱,汽车等等都可以接上5G。可见他的市场规模一下子变得庞大了许多。华为等公司都是为了这庞大利益而竞争。
那么暂时是谁在5G方面领先了呢?
在5G标准方面高通仍然占了很大的优势。华为的标准只拿下了eMBB场景中控制信道的编码方案,但在其他的方面仍然被高通拿下了标准。可见如果华为想搞5G的话,免不了给高通专利费。高通我个人觉得是个蛮精明的公司。他不制造设备,也不卖手机,但在专利方面却能让你频频吃官司,苹果就是最好的例子,最后搞得苹果只能采购Intel的东西,销售量因此而下降。虽然许多人总说华为拿下了5G,但我个人觉得高通仍然会笑到最后,因为许多标准都采用高通,而且华为想要制造5G设备的话,免不了向高通交专利费。但在专利数量方面,华为占据了极大的优势。参考下图,可见华为专利数量远远把对手抛在了后面。
各公司专利数量
补充:世界上有一种税叫高通税。高通税是说只要你的手机连接上了2G,3G或4G的网络,那么高通就有权利抽你的税,苹果就是不要给这个税因而闹上法院,但几乎都失败了,平均每架手机会抽3~5%左右的税。
总结,虽然百姓使用普通手机4G或者LTE技术显然能够满足这些需求。但未来的趋势是物联网(IoT, Internet of Things),自动驾驶等等。这些科技需要5G来作为基础。谁拿下了5G专利,那么许多企业包括物联网,自动驾驶等企业只为你是头了,发言权在业界也最大。美国就是不希望把这个机会让给别人因此死死咬着5G技术不放。欧盟虽然也想啃着这块大饼,但近期欧洲感觉没什么势头了。