Loading DesignSpark, please wait...

We apologise for the slowness of this page You are using Internet Explorer 6, upgrading your browser will greatly enhance your experience using DesignSpark

The gateway to online resources and design support for engineers, powered by RS ComponentsAllied

A Raspberry Pi-powered Radio 4 appliance

Posted by Andrew Back on

23611 views

title

Using a Raspberry Pi to build an Internet radio that only receives BBC Radio 4.

Tuning controls and station presets? Why on earth would anyone want such things! As far as I'm concerned the only thing worth listening to on the wireless is Radio 4.

With the above in mind, I decided to build myself an Internet radio that is fixed on Radio 4 and which dispenses with unnecessary clutter, with the only control being for power and volume.

Construction

title

At a flea market earlier this year I picked up a 1950s extension speaker made by Richard Allan. Comprising of simply a cabinet, loudspeaker, step attenuator and input socket, and with plenty of spare room inside, this was ideal for converting into a Raspberry Pi-powered Internet radio.

The cabinet can be seen above with the old step attenuator removed, and alongside this a combination switch/potentiometer ready for fitting in its place. Of course, the audio level output from a Raspberry Pi will not drive a loudspeaker directly and so an amplifier was also required.

title

The amplifier that was used is based around the TDA2030 IC and a PCB supplied by RS Components. For further details including a bill of materials, see the DesignShare project.

In order to provide a power source for the Raspberry Pi, a DC-DC converter with 5v output was connected to the 0 and +ve rails of the amplifier power supply.

Unfortunately, the Raspberry Pi wouldn't quite fit into the base of the cabinet and so the audio and composite video output sockets were removed.

title

Since there was only one loudspeaker and a single mono amplifier, the left and right channels were summed to mono using resistors.

title

A power indicator lamp, the transformer, power supply board, Raspberry Pi and amplifier were then all fitted into the cabinet, and the DC power and audio connections soldered.

title

Finally, the mains lead was connected up to the power switch.

title

The rear cover can be seen below, fitted with a fuse holder, mains lead and strain relief, and an RJ45 socket to allow use with a wired Internet connection (the Pi also has a USB WiFi adapter fitted).

title

Software

The software configuration couldn't be simpler: on booting an init script starts Mplayer and specifies the URL for the BBC Radio 4 stream. That's it! The Mplayer command line being:

mplayer -playlist “http://bbc.co.uk/radio/listen/live/r4.asx“

Result

The above video shows the radio in operation. Note that it takes >40 seconds for the Pi to boot and during which time it makes strange noises that are not unlike those of a 1980s microcomputer loading software from tape!

The strange sounds may be due to the way that I have taken an audio output from the Raspberry Pi — replacing the jack socket with resistors and directly soldering a cable to the PCB. In any case, I quite like the effect and it provides an indication that something is happening while the Pi boots.

Andrew Back

Follow

2 comments

Comments

  • pete wood Avatar pete wood

    Posted by pete wood at

    Brilliant!!! I was considering doing a similar thing with an old TV. Rip out the old screen and stick in a flat screen monitor instead. Then use a Raspberry Pi with XBMC or similar with Iplayer etc; then use my Ipad with the XBMC App to control it... kind of "Retro Tech" meets "Modern Tech" ;0)

    tv set.jpg
    tv set.jpg (45.77 KiB) Not viewed yet

  • boss Avatar boss

    Posted by boss at

    That's a great project, thanks for sharing. I like the connection to the internet on the back of a 'valve' radio, well at least an enclosure from the period!
    The items used span the a period similar to the books on on your bookshelf!

    I must boot my pi up and have some fun!

Leave a comment