DesignSpark フォーラム
このフォーラムでは、世界中のDesignSparkに登録しているメンバーと様々な技術的相談や、議論を行うことができます。また、自身のアイデアに賛同してくれるエンジニアを、世界中から探すこともできるでしょう。
英語の投稿が目立ちますが日本語の質問でも問題ありません。よく海外から片言の日本語で回答を頂いたりします。自動翻訳レベルでも結構ですのでグローバルなユーザとのコミュニケーションをお楽しみください。
你好。自动重新安装电脑windows系统后一直提示这个无法完成注册。试过用代理。用手机流量等。请问应该如何解决。
Hi,
I'm using quite a while a creator plan of DS Mechanical on two different computers (Desktop and Laptop). My Laptop crashed an I installed DS Mechanical on my new laptop. But I'm not able to login. App comes up with a registration error. I guess this is due to the limitation of a maximum of 2 computers for the respective license. But how can I fix this, as I can't log off from my old laptop anymore?
Any help is appreciated,
Kind Regards
Sebastian Hello,
I'm creating a flat round logo 7mm. high, and I'd like to curve it upwards to look like a car logo.
I don't know how to say to make an extrusion but slightly round from the top center.
David I have noticed that since upgrading to 6.0.3 many times the stl files are the wrong size when imported into a slicer program such as Lychee or Anycubic Workbench.
As a test I created a simple part, DSM says the largest block is 9mm on each side, importing into either slicer and the dimension have shrunk to .01 mm.
What's going on?
Buongiorno,
Mechanical con licenza Creator.
Oggi fa così "DesignSpark Mechanical ha riscontrato un errore durante la registrazione"
Mi hanno appena sostituito la scheda madre del PC...ma non vedo alcun nesso...
Succede a qualcun altro?
Grazie Is there a way to "activate" track segments that (almost/often) are unreachable/unclickable ? I tried click+control, click+alt, click +shift, click +alt gr.... Even zoomed in to the max...
e.g to delete a corner ...thanks in advance !. Hi, my name is Riccardo and I'm a new user. I'm working with the browser version of DesingSpark Simulator and I ask you if there's a funcion that creates an automatic Bill Of Materials (I'm working with very basic components, such as resistors, capacitors and leds).
Thank you so much for the answers. Bonjour je rouvre DSM6 depuis plusieurs semaines sans utilisation et la, le fond de ma conception reste noir ?
Quelqu'un à t'il une solution ?
Merci par avance
Albert With a Creator or Engineer subscription, DesignSpark Circuit Simulator allows your simulations to run longer than 1 minute and upto 1 hour of server compute time.
Our Circuit Simulator was introduced last July and can be a good tool for DS PCB users, and we know that some of our DSM users also do PCB designs...
We list some key reasons why you may need an extended simulation time:
Run electro-thermal transient simulations long enough for temperatures to reach steady-state, to verify reliability under real world operating conditions.
Allows compute-intensive simulations, such as switching power electronic circuits, to run as long as necessary for line and load transient response tests.
Monitor the behaviour of critical components to varying inputs over an extended time period, such as for vehicle drive-cycle simulations.
Check it out at https://www.rs-online.com/designspark/designspark-circuit-simulator
表題の件、1度目はできたのですが、2回目からは下記のようなポップアップがでてダウンロード出来なくなりました。解決方法はありますでしょうか?
記
Demonstrating the powerful but unusual edge and face rounding that DesignSpark (Parasolid) has... REJOICE !
Alternatively, pull two edges a small way, then pull in opposite direction to make a full round.
and for circular rounds, select two edges , pull to create a round on each edge a little, then pull in opposite direction.
To remove the full round, select and Fill.
This also works for eccentric round edge pulls as below gif:
Other tapering helical multi-sided with rotational sections are easily made with DSM if needed.
会社のデスクトップでCreatorを、出先のノートパソコンでExplorerを、一つのメールアドレスで使うことができません。どちらかがストップします。併用すること不可能ですか。 Although the automotive industry is moving rapidly toward electrification, there is no reason to stop improving the performance and efficiency of traditional gasoline engines. New power electronics technology from Nexperia can help with that too!
Accurate fuel metering is important for robust engine control, and that translates into tight timing requirements for the fuel injector opening and closing. One method to improve the response of the injector closing is to provide a large back-voltage at the end of the injection event, to rapidly reduce the injector solenoid current. This back voltage can come from the “avalanche” of the main injector driver switch. That switch must be rated to handle repeated avalanche conditions, like the BUK9K13-60RA 240-1816 Power MOSFET from Nexperia. This fuel injector driver example shows the benefit of using that part for better timing control of fuel injector cut-off.
Read the full article at:
https://www.rs-online.com/designspark/quick-off-injector-driver-for-tighter-fuel-metering-using-a-nexperia-power-mosfet
「ビュー」など、種類の文字が「作成」欄により半分書けてしまう。 In 3D Printing and design I was reading the articles on using plastic bottles for filament with 3D printers. I was going to add the feed back at the end of the article where you can give it a thumbs up or down, and answer the 2 questions posed. When I submit it it always says it was unable to send it and to try again later. Problem is that it has happened almost every time I have tried to submit feedback. Just thought I would let you know in case you are unaware.
Thanks最近のフォーラム投稿
你好。自动重新安装电脑windows系统后一直提示这个无法完成注册。试过用代理。用手机流量等。请问应该如何解决。
Registration Issue when trying to login on a new laptop
how to curve it upwards
DSM 6.0.3 producing inaccurate .stl files
DesignSpark Mechanical ha riscontrato un errore durante la registrazione - error while registering
Quasi unreachable track segments
How to create an automatic Bill Of Material?
Espace de travail reste noir ?
What does more than 1 minute of simulation time allow you to do?
3Dモデルのダウンロードができない。
Pull Rounds in DSM v6 - standard radical functionality available to all.
複数のパソコンで使用する
Tighter fuel metering with a 'quick-off' injector driver
パネルの種類文字をきちんと見たい
Feedback never works when you try to give it