DesignSpark フォーラム
このフォーラムでは、世界中のDesignSparkに登録しているメンバーと様々な技術的相談や、議論を行うことができます。また、自身のアイデアに賛同してくれるエンジニアを、世界中から探すこともできるでしょう。
英語の投稿が目立ちますが日本語の質問でも問題ありません。よく海外から片言の日本語で回答を頂いたりします。自動翻訳レベルでも結構ですのでグローバルなユーザとのコミュニケーションをお楽しみください。
Bonjour je rouvre DSM6 depuis plusieurs semaines sans utilisation et la, le fond de ma conception reste noir ?
Quelqu'un à t'il une solution ?
Merci par avance
Albert With a Creator or Engineer subscription, DesignSpark Circuit Simulator allows your simulations to run longer than 1 minute and upto 1 hour of server compute time.
Our Circuit Simulator was introduced last July and can be a good tool for DS PCB users, and we know that some of our DSM users also do PCB designs...
We list some key reasons why you may need an extended simulation time:
Run electro-thermal transient simulations long enough for temperatures to reach steady-state, to verify reliability under real world operating conditions.
Allows compute-intensive simulations, such as switching power electronic circuits, to run as long as necessary for line and load transient response tests.
Monitor the behaviour of critical components to varying inputs over an extended time period, such as for vehicle drive-cycle simulations.
Check it out at https://www.rs-online.com/designspark/designspark-circuit-simulator
表題の件、1度目はできたのですが、2回目からは下記のようなポップアップがでてダウンロード出来なくなりました。解決方法はありますでしょうか?
記
Demonstrating the powerful but unusual edge and face rounding that DesignSpark (Parasolid) has... REJOICE !
Alternatively, pull two edges a small way, then pull in opposite direction to make a full round.
and for circular rounds, select two edges , pull to create a round on each edge a little, then pull in opposite direction.
To remove the full round, select and Fill.
This also works for eccentric round edge pulls as below gif:
Other tapering helical multi-sided with rotational sections are easily made with DSM if needed.
会社のデスクトップでCreatorを、出先のノートパソコンでExplorerを、一つのメールアドレスで使うことができません。どちらかがストップします。併用すること不可能ですか。 Although the automotive industry is moving rapidly toward electrification, there is no reason to stop improving the performance and efficiency of traditional gasoline engines. New power electronics technology from Nexperia can help with that too!
Accurate fuel metering is important for robust engine control, and that translates into tight timing requirements for the fuel injector opening and closing. One method to improve the response of the injector closing is to provide a large back-voltage at the end of the injection event, to rapidly reduce the injector solenoid current. This back voltage can come from the “avalanche” of the main injector driver switch. That switch must be rated to handle repeated avalanche conditions, like the BUK9K13-60RA 240-1816 Power MOSFET from Nexperia. This fuel injector driver example shows the benefit of using that part for better timing control of fuel injector cut-off.
Read the full article at:
https://www.rs-online.com/designspark/quick-off-injector-driver-for-tighter-fuel-metering-using-a-nexperia-power-mosfet
「ビュー」など、種類の文字が「作成」欄により半分書けてしまう。 In 3D Printing and design I was reading the articles on using plastic bottles for filament with 3D printers. I was going to add the feed back at the end of the article where you can give it a thumbs up or down, and answer the 2 questions posed. When I submit it it always says it was unable to send it and to try again later. Problem is that it has happened almost every time I have tried to submit feedback. Just thought I would let you know in case you are unaware.
Thanks I think it's hard to explain what I'm trying to do...Is it not possible to have two pcs. copper pour on the same layer ?First I make a copper pour on the right side of the card and the spokes connect to the pads as expected. This copper pour has positive voltage. Then I make copper pour number two on the left side of the card on the same layer and then the problems start. I want this copper pour to have negative voltage. But when I do this the copper pour I made in the first place becomes negativ and the spokes disappear.Did this make any sense ? インストール後に登録の間にエラーが発生しました。が発生し開かない
再インストールでも同じ改善できない Have bought a new computer and downloaded software for PCP and mechanics.
But when I start these programs, I should start by logging into my account.
But I can't login to DisgnSpark " to any of my accounts.
I receive information that I am unauthorized.
(Even made a new account to see if something went wrong with the account.)
I have downloaded and reinstalled a couple of times without the login working.
I haven't had any problems on the old computer.
However, the software remains on the old computer and works on it.
What do I need to do to access my account from the software? Why do the "Views" alway stay at zero on the topics posted here on DSM? It would be useful to see how many people are viewing certain topics. Just curious if that is turned off on purpose or is a bug or a glitch. Whether I am logged on or off they are always showing "0" views on all topics.
Thanks Molded or Formed parts need a minimum draft to allow parts to extract from shaping tools such as plastic injection molds, pressure / gravity die castings, formed metal pressed sheets. Understanding and being able to design using the necessary draft angle is part of being an Industrial designer or anyone involved in specifying manufacturing information.
Either analyse your own designs or Import supplier models and check the draft before commiting to any manufacture.
DesignSpark Mechanical has a draft dynamic analysis tool in the Measure Tab and I think it's superb.
Example part:
Tube of varing profiles made by blending layout constrained sketches to tangential (red face) and conic 2.5 draft angled face. (blue face).
Using the new Mirror tool or duplicating the curves to make a continuous section, other faces can be made.
Analysis can be made on a singular face or the complete shape.
For example, the draft has been set at 3 degrees; with the direction of draft specified using this arrow:
and choosing the plane shown, a white arrow direction is drawn ( see 2nd above image - arrow in left hand bottom corner).
With 'Both directions' also selected, any face about the specified direction that is not at least 3 degrees will be shown in the user specified or default color - here shown in red.
The part was designed with 2.5 draft.
Changing the check value to 2.51 the result is shown below.
Changing the check value to 2.5 the result is shown below.
Probing can be singular or multiple points:
Transition values will show the gradient of draft. With 1 % transition from a 2.5 degree start, all areas upto 2.58 degrees are shown in red.
Draft angle dynamic dragging:
Whole part analysis.
Shadow Lines can be shown and created:( rename as appropriate ) Shown is a 3 degree shadow line.
Enhanced shaed part with drafting plane.
In the design of a Diecast car wheel shown below, the model creator ( me ) forgot to add draft to the wheel rim - whoops!
Manufacturing errors created by inadaquate design; even even small ones, cost time and money to fix and reputation is lost!
On the wheels rear, all the ribs that create the hollows also need the draft checking. The part will shrink during molding and may shrink tight on any inadquately drafted faces causing part ejection problems.
Again , there are more small area's that are less than 3 degrees. ( 3 degrees isn't the standard for diecast - it will depend upon material and texture ( texture not usually applied to diecast parts) - advice is to always seek experienced manufacturer advice).
Finding small areas like this would be impossible without an analysis tool:
Ask if wanting additional information. It's a simple thing really, although I've used DSM for years it's always bothered me. When I start a new design I get this:
But I want Z pointing up X pointing to the right and Y pointing backwards. This way It's the correct way around for the slicer. I know I can work around this but it's always bothered me. Don't be too hard on me We, at OKdo, have been working on a new video series and we're thrilled to announce that the first episode of "Projects with Pete" is now live on our YouTube channel.Join Peter Milne, an engineer with a passion for Linux and single-board computers, and myself as we explore the realm of Industrial IoT solutions in our Industrial Automation project series.In the first episode, we delve into building a secure MQTT Edge Gateway using the ROCK 4 Model SE single-board computer.We can't wait to hear your thoughts! Check out the episode and let us know what you think. Unlocking Industrial IoT: Building a Radxa ROCK 4SE MQTT Gateway! | Projects with Pete | OKdo (youtube.com)最近のフォーラム投稿
Espace de travail reste noir ?
What does more than 1 minute of simulation time allow you to do?
3Dモデルのダウンロードができない。
Pull Rounds in DSM v6 - standard radical functionality available to all.
複数のパソコンで使用する
Tighter fuel metering with a 'quick-off' injector driver
パネルの種類文字をきちんと見たい
Feedback never works when you try to give it
2 piece of copper pour on same layer
開かない 登録の間にエラーが発生しました。
Unable to activate Mechanics and PCP software by logging into my account
Forum question
Analysing Draft angle - How it works
Default XYZ orientation
Building a Radxa ROCK 4SE MQTT Gateway