Wie finden Sie diesen Artikel? Helfen Sie uns, bessere Inhalte für Sie bereitzustellen.
Vielen Dank! Ihr Feedback ist eingegangen.
There was a problem submitting your feedback, please try again later.
Was denken Sie über diesen Artikel?
Parts list
Qty | Produkt | Part number | |
---|---|---|---|
1 | OKdo Raspberry Pi 4 B Starter Kit 4 GB | 202-0644 | |
Twitter bots - or automated tweets - have got themselves a bad name - however, there are some that are useful and not spam. Twitter actually encourages the useful ones - for example, I use @UKmfg to automatically retweet anything about #UKmfg - or manufacturing in the UK. Although I have to put a few measures in to make sure that swear words or hijacked hashtags are not automatically retweeted.
For the rules on automation from Twitter see here. Many thanks to @AndyPiper for his help on getting this to work!
In this project, I will share how to make a Twitter bot using a Raspberry Pi and Node-RED software.
This used to be very simple - now there are more hoops to jump.
NOTE: This is working as of 17 November 2020 - but be aware of updates to Twitter which may break it.
Preliminaries 1
1) Get a developer account on Twitter and find the keys and tokens.
The instructions and information to do this can be found here: https://developer.twitter.com/en/apply-for-access
Note: You only need one developer account, and, as long as you have the correct permissions, you can then use this to get the keys and tokens so you can tweet from any other account.
2) Go to the developer portal https://developer.twitter.com/en/portal/dashboard
Add an app (bottom of overview tab) and then record the API key, API Secret Key, and Bearer token somewhere safe. Copy and paste it - do not manual transcribe them.
Then click "App Settings" at the bottom of the page.
3) Set the following:
App permisions: Read and write
Enable 3-legged OAuth
Callback URL - any website address here (I use https://twitter.com)
Website URL - any website here (https://twitter.com)
4) Keys and Tokens
At the top of the page, click the "Keys and Tokens" tab.
You should have already saved the API key, API Secret Key, and Bearer token.
Generate the "Access Token and Secret" and copy these to your safe place.
If you want to tweet from your "Twitter Developer Account" then these are the keys and tokens you need. However, if you want to tweet from a different account, you need to jump through these further hoops:
[Note: you can also get these keys using GO - details here https://github.com/smaeda-ks/tw-oob-oauth-cli]
This doesn't have to be done on the Pi, but if you are using it, you first need to intall RubyGems by using the code
sudo apt install ruby-full
More details here: https://www.raspberrypi.org/documentation/linux/software/ruby.md
Then install Twurl - by using the code
sudo gem install twurl
info is here: https://developer.twitter.com/en/docs/tutorials/using-twurl
Then type the code
twurl authorize --consumer-key ABC123 --consumer-secret ZYX789
Where ABC123 is the API key you saved earlier (I don't know why it's called something different)
and ZYX789 is the API secret key
Follow the onscreen instructions, and go to the website https://api.twitter etc that it lists. (Make sure you are either logged out of twitter or logged in to the account you want to tweet from). Enter the supplied Pin in to the terminal.
Congratulations. You have now generated the access keys and tokens! But now to find them ...
5) Finding the keys and tokens!
Now you need to find the .twurlrc file.
. files are hidden, so you need to show hidden files on the Pi, this is in File Manager, View tab and Tick the "Show Hidden"
The .twurlrc file will be in the pi directory.
It should be in your home/USER directory on Mac, and c:\Users\USERNAME\APPData\Local\ directory on a PC.
Open the file and there are the consumer_key and the consumer_secret! Copy and paste those somewhere safe.
Preliminaries 2
1) Install the latest Raspberry Pi operating system on to your Pi
Details here: https://www.raspberrypi.org/software/ (For this project I am using a Raspberry Pi 4 and Raspbian Pi OS (32 bit) 2020-08-20). Follow the onscreen instructions to update and complete the set-up.
2) Install Node-RED
Note: DO NOT USE THE 'RECOMMENDED PROGRAMS' link on the Pi menu, instead go to the "Running on a Pi" section at https://nodered.org/docs/getting-started/raspberrypi and follow the instructions there - use the code:
bash <(curl -sL https://raw.githubusercontent.com/node-red/linux-installers/master/deb/update-nodejs-and-nodered)
And say "Yes" to installing the Pi Nodes.
Wait a long time
Once it is installed run the code:
sudo systemctl enable nodered.service
This will make Node-RED automatically start every time the Pi boots up.
You can then go to a browser and type in localhost:1880 to access Node-RED
3) Install the Twitter Node on Node-RED
Click on the Hamburger Menu (three horizontal lines) in the top right of the sheet
Select Manage Palette and click on the "Install" tab.
Search for "node-red-node-twitter" and click install
The twitter input and output nodes will now be in the left hand column in the "Social" area.
Start writing the flow
Connect an inject node to a twitter out node.
Change the Inject node msg.payload = to "Hello World"
Double click on the Twitter out node.
Click the pen icon next to "add new twitter-credentials ..."
Complete the properties:
Twitter ID: The twitter account you want to tweet from
API Key: consumer_key from the .twurl file
API Secret Key: consumer_secret
Access Token: token from the .twurl file
Access Token secret: secret from the .twurl file
Save and deploy!
Now click the inject node and your tweet should go live.
(Note, you can't duplicate the same tweet, so it may be worth putting the timestamp in for testing purposes!)
Now it is working with an inject node, you have the basis for using the twitter node in any flow. The set up is the same for a twitter input node.
Happy tweeting!