DesignSpark论坛
通过论坛区与其他 DesignSpark 会员自由交流。就产品、技术、软件和未来创新创建新的对话或加入现有的讨论。提供解决方案帮助他人,或者向全球志同道合的工程师网络提问,为自己遇到的技术问题寻找答案。
表題の件、1度目はできたのですが、2回目からは下記のようなポップアップがでてダウンロード出来なくなりました。解決方法はありますでしょうか?
記
Demonstrating the powerful but unusual edge and face rounding that DesignSpark (Parasolid) has... REJOICE !
Alternatively, pull two edges a small way, then pull in opposite direction to make a full round.
and for circular rounds, select two edges , pull to create a round on each edge a little, then pull in opposite direction.
To remove the full round, select and Fill.
This also works for eccentric round edge pulls as below gif:
Other tapering helical multi-sided with rotational sections are easily made with DSM if needed.
会社のデスクトップでCreatorを、出先のノートパソコンでExplorerを、一つのメールアドレスで使うことができません。どちらかがストップします。併用すること不可能ですか。 Although the automotive industry is moving rapidly toward electrification, there is no reason to stop improving the performance and efficiency of traditional gasoline engines. New power electronics technology from Nexperia can help with that too!
Accurate fuel metering is important for robust engine control, and that translates into tight timing requirements for the fuel injector opening and closing. One method to improve the response of the injector closing is to provide a large back-voltage at the end of the injection event, to rapidly reduce the injector solenoid current. This back voltage can come from the “avalanche” of the main injector driver switch. That switch must be rated to handle repeated avalanche conditions, like the BUK9K13-60RA 240-1816 Power MOSFET from Nexperia. This fuel injector driver example shows the benefit of using that part for better timing control of fuel injector cut-off.
Read the full article at:
https://www.rs-online.com/designspark/quick-off-injector-driver-for-tighter-fuel-metering-using-a-nexperia-power-mosfet
「ビュー」など、種類の文字が「作成」欄により半分書けてしまう。 In 3D Printing and design I was reading the articles on using plastic bottles for filament with 3D printers. I was going to add the feed back at the end of the article where you can give it a thumbs up or down, and answer the 2 questions posed. When I submit it it always says it was unable to send it and to try again later. Problem is that it has happened almost every time I have tried to submit feedback. Just thought I would let you know in case you are unaware.
Thanks I think it's hard to explain what I'm trying to do...Is it not possible to have two pcs. copper pour on the same layer ?First I make a copper pour on the right side of the card and the spokes connect to the pads as expected. This copper pour has positive voltage. Then I make copper pour number two on the left side of the card on the same layer and then the problems start. I want this copper pour to have negative voltage. But when I do this the copper pour I made in the first place becomes negativ and the spokes disappear.Did this make any sense ? インストール後に登録の間にエラーが発生しました。が発生し開かない
再インストールでも同じ改善できない Have bought a new computer and downloaded software for PCP and mechanics.
But when I start these programs, I should start by logging into my account.
But I can't login to DisgnSpark " to any of my accounts.
I receive information that I am unauthorized.
(Even made a new account to see if something went wrong with the account.)
I have downloaded and reinstalled a couple of times without the login working.
I haven't had any problems on the old computer.
However, the software remains on the old computer and works on it.
What do I need to do to access my account from the software? Why do the "Views" alway stay at zero on the topics posted here on DSM? It would be useful to see how many people are viewing certain topics. Just curious if that is turned off on purpose or is a bug or a glitch. Whether I am logged on or off they are always showing "0" views on all topics.
Thanks Molded or Formed parts need a minimum draft to allow parts to extract from shaping tools such as plastic injection molds, pressure / gravity die castings, formed metal pressed sheets. Understanding and being able to design using the necessary draft angle is part of being an Industrial designer or anyone involved in specifying manufacturing information.
Either analyse your own designs or Import supplier models and check the draft before commiting to any manufacture.
DesignSpark Mechanical has a draft dynamic analysis tool in the Measure Tab and I think it's superb.
Example part:
Tube of varing profiles made by blending layout constrained sketches to tangential (red face) and conic 2.5 draft angled face. (blue face).
Using the new Mirror tool or duplicating the curves to make a continuous section, other faces can be made.
Analysis can be made on a singular face or the complete shape.
For example, the draft has been set at 3 degrees; with the direction of draft specified using this arrow:
and choosing the plane shown, a white arrow direction is drawn ( see 2nd above image - arrow in left hand bottom corner).
With 'Both directions' also selected, any face about the specified direction that is not at least 3 degrees will be shown in the user specified or default color - here shown in red.
The part was designed with 2.5 draft.
Changing the check value to 2.51 the result is shown below.
Changing the check value to 2.5 the result is shown below.
Probing can be singular or multiple points:
Transition values will show the gradient of draft. With 1 % transition from a 2.5 degree start, all areas upto 2.58 degrees are shown in red.
Draft angle dynamic dragging:
Whole part analysis.
Shadow Lines can be shown and created:( rename as appropriate ) Shown is a 3 degree shadow line.
Enhanced shaed part with drafting plane.
In the design of a Diecast car wheel shown below, the model creator ( me ) forgot to add draft to the wheel rim - whoops!
Manufacturing errors created by inadaquate design; even even small ones, cost time and money to fix and reputation is lost!
On the wheels rear, all the ribs that create the hollows also need the draft checking. The part will shrink during molding and may shrink tight on any inadquately drafted faces causing part ejection problems.
Again , there are more small area's that are less than 3 degrees. ( 3 degrees isn't the standard for diecast - it will depend upon material and texture ( texture not usually applied to diecast parts) - advice is to always seek experienced manufacturer advice).
Finding small areas like this would be impossible without an analysis tool:
Ask if wanting additional information. It's a simple thing really, although I've used DSM for years it's always bothered me. When I start a new design I get this:
But I want Z pointing up X pointing to the right and Y pointing backwards. This way It's the correct way around for the slicer. I know I can work around this but it's always bothered me. Don't be too hard on me We, at OKdo, have been working on a new video series and we're thrilled to announce that the first episode of "Projects with Pete" is now live on our YouTube channel.Join Peter Milne, an engineer with a passion for Linux and single-board computers, and myself as we explore the realm of Industrial IoT solutions in our Industrial Automation project series.In the first episode, we delve into building a secure MQTT Edge Gateway using the ROCK 4 Model SE single-board computer.We can't wait to hear your thoughts! Check out the episode and let us know what you think. Unlocking Industrial IoT: Building a Radxa ROCK 4SE MQTT Gateway! | Projects with Pete | OKdo (youtube.com) Hey out there.
I have this odd problem I can't seem to get around.
I import a spline from a DXF file, created by any app on my pc, the problem occurs.
If I click on the spline and try to fill it. Nothing happens. However if I alter the spline in anyway, move it rotate it...anything. Then try to fill it. It deletes.
This is a repeatable problem. Whats even stranger is I can export a series of splines all exactly the same (copies of each other), but one or two will not work, if it's a series of 10 splines in a row, the 3 and 4th might act up and the rest are fine. If I reExport the same series of splines as a DXF it's always the same objects that delete. The rest are fine.
I suspect an issue with the import engine in some way.
I have no work around at this point. Are there any plans for DS to implement .3MF exports? I use designspark for creating 3D printing models with multicolor printing. .3MF exports are very necessary. Please tell me this in the works and will be released soon....新论坛帖子
3Dモデルのダウンロードができない。
Pull Rounds in DSM v6 - standard radical functionality available to all.
複数のパソコンで使用する
Tighter fuel metering with a 'quick-off' injector driver
パネルの種類文字をきちんと見たい
Feedback never works when you try to give it
2 piece of copper pour on same layer
開かない 登録の間にエラーが発生しました。
Unable to activate Mechanics and PCP software by logging into my account
Forum question
Analysing Draft angle - How it works
Default XYZ orientation
Building a Radxa ROCK 4SE MQTT Gateway
Spline keeps deleting.
.3MF export