DesignSpark论坛
通过论坛区与其他 DesignSpark 会员自由交流。就产品、技术、软件和未来创新创建新的对话或加入现有的讨论。提供解决方案帮助他人,或者向全球志同道合的工程师网络提问,为自己遇到的技术问题寻找答案。
how to switch language?such as Chinese hi , somehow i made something wrong and i cannot make surfaces with the lines, lines are gray instead of black as usual. Can someone advice how to unmake the error?
thanks for help
Having created a design successfully and saved it, I now find that every time I re-open the file, the objects that make up the design appear either above or below the Z-axis baseline (ie either with a positive or negative Z position, instead of at zero). Anyone else had this problem or any thoughts as to the cause or cure? Bonjour,
J'ai réalisé une PCB de 5 couches.
Pourquoi les couches ' Gnd Plane et Vcc Plane ' ne contient pas des pistes ?
Est ce que je peux supprimé les deux couches Gnd Plane et Vcc Plane ?
Merci d'avance
Hello,
I have been trying for 24 hours to get someone to solve a problem for the second time. After pausing my 'Creator' license, I reactivated it a month later, and there is no way to activate it in the application (I am still on the 'Explorer' version). Additionally, there is no way for the support service to assist you 24 hours after making the payment. The last time, the problem was not fixed until support intervened. Something on your end is not activating the license automatically after payment. I am losing design time because of a system that is not well managed.
Best regards, トップアセンブリの重量と重心が分かる方法はありますでしょうか。 I don't know how to do it, please let me know.I would like to see an isometric perspective view of a surface other than the first registered angle. Is there any other way besides moving it manually?
やりかたが分からないので、どうか教えてください。
最初に登録した角度以外の面の等角透視図を見たいです。手動で動かす方法以外に、方法はありませんか? Bonjour,
J'ai réalisé de PCB qui contient 3 couches.
- Est ce qu'il manque des couches.
- C'est quoi Bias--> None ?
Cordialement.
There is a command on the Design tab called Insert Origin, but I am not sure of the situation or where to use this command. Also, after inserting the origin, I believe the design origin remains in the design, can anyone tell me how this is related? As the title states...I cannot change password on my original account, going way back a few years. I had to create another account (different email address) and that login was rejected too. Reset password, can now login to web site. Installed DS PCB V11 and after install it asked for credentials which I entered, it rejected them "invalid credentials". This account stuff has always been a nightmare with DS. What might I be doing wrong??? 表題の件、バージョン情報を推してライセンスIDを確認したいのですが、下のように
Linkが邪魔して読み取れません。どうすればよいでしょうか?
Using the constraint sketcher is more complicated than using the standard traditional sketcher. There are benefits of model to curve persistent constraints and some negative aspects that demand a greater understanding of DSM fundamental principles. Some users have struggled within the Constraint sketcher environment in attempting to have both reference geometry AND dimensions in the same plane and have experienced collapsing / disappearing dimensions. Ultimately, the easiest action is to use the standard sketcher as there are no software contradictions in doing that, but the procedure provided below allows this within the Constraint sketcher environment.
All the information below is particularly for users that are working in the Constraint sketcher and want to add dimensions and reference curves AND ALSO wish for the reference curves to follow the model change using all of DSM change management standard options.or methods.
Now on with the explanation.
To make a body with features that have both annotation dimensions and reference construction geometry lines, the reference construction lines have to be added onto a plane by using sketch on that plane only.
1. Select the face, then select Insert Plane > then activate the plane...
2. Select the activated plane and press K for Sketch > select the sketch option Layout Sketch and add the ddreference curves =
Note that Sketcher Planes that contain Sketch1, 2 ( layout sketches) etc. also have exactly the same behavour and that if required, by a Sketch right click selection, the command 'Use 3D' will create a curve in a curves folder ( not shown).
Note that unless specifically all future model changes are known, it will be wise to not allow the Automatic constraint generation when placing the reference curves as the cuvre ends must follow the hole wherever the hole is moved to. Automatic constraints will attempt to add parallelism, squareness etc. which may conflict when the model holes are potentially moved.
The constraint has not been applied to other sketch entities but to the actual model hole center point by cycling through the geometry on-screen option using the UP <>DOWN keyboard keys or by hoding down Ctrl key and mouse wheel revolving.
It may be helpful when visually identifying the attachment connections to 'Fade Scene', the highlights are then more noticeable - see image below.
3. Add dimensions
Select the model face ( not the Plane with the reference lines)
Add dimensions to the model geometry and not the sketch geometry by display removal of layout Sketch first
> add the dimensions...
Remember , two different planes must be used. The first to add the reference geometry attached to the model which stays attached via the constraints ( delete any possible constricting constraints such as vertical / horizontal because all that is required is point position to the hole center) and a second, an annotation plane with dimensions to the model features only.
Ensure to activate the component as shown:
Note that Planes and Annotation Planes can also belong to the component and this is the preferable structure location for discrete component manipulation and further drawing sheet association of an annotation plane without unnecessary dimension duplication.
With the annotations made, when moving faces ( if necessary) as shown in the gif below, all reference curve geometry follows the model face moved.
Explorer users that want to model as above, they should note that this is print outcome is considerably more simple and substantually faster if using the Drawing Sheet functionality provided in the Creator and Engineer versions. But if actually wanting all the flexible associations shown, considerations / actions must still be taken as described.
The above procedure has taken a long time to establish... and it's regretable that some users have struggled with the technology.
Th standard sketcher is less capable but also less demanding of applied principle. DSM6で作図中にフリーズし全て作図が見えなくなりました。
ストラクチャーツリーや操作履歴は残っているのですが、どこをいじっても元の画面が表示されません
この状態で保存してしまったので閉じて開こうとすると同じ状態になるのが怖くて閉じられません
自動保存も有効にしてあったのに、保存先のフォルダを見ると15分間隔で設定してあるにも関わらず2時間前のファイルしかなくて、それすらも開こうとしたら、エクスプローラー上で雪のように溶けてなくなりました。なんの反応もなく。
windowsがエラーも出さず勝手に目の前でファイルを消すことってあり得ませんよね?これはDSMが「これは不良ファイルだから消してしまえ」という操作をしたという証拠ではないですか?
あのさあDSM、・・・・
とにかく元に戻す方法はないのでしょうか?こういうことって皆さんは良くありますか?
PCは3年前ぐらい前に購入したwindows10を11にアップグレードしたものです。
DSM6を使っております。
アノテーションプレーンに描いたソリッドの寸法が、なにかの拍子に全て消えてなくなってました。
一部ではなく、そのアノテーションプレーンに描いたもの全て。
”戻る”では呼び出せないぐらいの前の工程で起こったらしく、原因がわかりません。
当然ですが、故意的に消した覚えはなく寸法や位置すらも変えておりません。アノテーションプレーンやソリッド自体は残っていますし、コンポーネントやレイヤを全て表示にしても出てきません。
同じデザイン内に別の色々なものがあり、それらを触っているうちになったと思われます。
しかもこういうことは何度かあります。
こうすると消えちゃうよ見たいなのがあれば教えてください。 According to the subscritions page, the DSM versions of Creator & Engineer are the same. Just checking is that the case? Or does engineer have some extras? (I know there are differences with PCB)新论坛帖子
how to switch language?such as Chinese
drawings dont create surfaces
Objects appear above or below Z-axis baseline
Gnd Plane et Vcc Plane
The license activation system from paused is disgraceful
トップアセンブリの重量と重心
Angle other than isometric(アイソメ以外の角度)
Bias
Main uses of the inserted origin and its relationship to the design origin
Credentials rejected even right after changing password
ライセンスIDが読み取れない!
EXPLORER Constraint sketcher users - How to mix Models with Annotation planes and Reference curves without loss of data.
書いたものが全て見えなくなり、自動保存にも不具合が・・・
アノテーションプレーンに描いた全ての寸法が消えました
DSM Creator v Engineer