What Is Thermal Imaging And Why Are FLIR So Good At It
FLIR’s Thermal Tech: It’s an Industrial Superpower You Need
Let’s be honest, thermal imaging sounds like something reserved for spy thrillers or ghost-hunting YouTube channels. But in the real world, FLIR’s thermal cameras are quietly revolutionising industries that feed us, move us, and build the steel backbone of modern life. From sizzling ovens to molten metal, here’s how FLIR tech is keeping things cool (or hot, when needed) across Food & Beverage, Automotive, and Heavy Industry.
However, before we delve into it, let's dispel a few common myths about thermal imaging.
Myth 1: Thermal cameras see through walls
Reality: They detect surface heat, not X-rays. If it’s hot on the surface, you’ll see it. Behind the wall? Not so much. So, all those movies have been giving you the wrong idea about thermal detection, so that mission might be impossible after all.
Myth 2: All heat is bad
Reality: Heat is data. Not every hotspot is a problem; some are signs of normal operation. Also, heat is heat, whether it’s hot or cold; it’s all subjective.
Myth 3: Thermal imaging is only for firefighters
Reality: It’s used across many industries, from food safety to steel production to robotics. However, firefighters do make it look Hollywood.
Myth 4: It’s just a fancy camera
Reality: FLIR systems are smart sensors with analytics, automation, and IIoT integration. It’s the camera that is thrown in for good measure.
Myth 5: You need a degree to use one
Reality: FLIR’s intuitive interfaces mean anyone can get actionable insights; there’s no PhD required. In fact, if you can turn it on, then you're ready to go.
Condition Monitoring
Waiting for Things to Break Is So Last Century:
Food and Beverage
- Oven’s Too Hot? Fridge Too Cold? FLIR’s got eyes on it. Motors, conveyors, and chillers get the thermal once over to catch wear and tear before it turns into downtime.
- Leaks That Sneak: Compressed air, CO₂, vacuum leaks, thermal and acoustic imaging will tag them before they mess with your product safety or energy bill.
- Temperature Drama: Real-time monitoring keeps food processes within safety zones. No spoilage. No contamination. Just compliance and calm.
Automotive Manufacturing
- Robot Overload: FLIR watches robotic arms like a hawk. Overheating? Mechanical stress? Shut it down before it shuts you down.
- Component Whispers: Cooling circuits, AC units, wheel bearings, thermal imaging sees what your diagnostics can’t.
- Electrical Gremlins: Loose terminals and high-resistance connections light up like Christmas trees on FLIR’s radar. Fires? Not today.
Quality Control
When “Close Enough” Doesn’t Come Close:
Food and Beverage
- Hot/Cold Spot Patrol: Cooked or frozen, FLIR ensures uniformity. Because foodborne illness isn’t a vibe.
- Seal the Deal: From microwave meal seals to glue on cartons, thermal imaging checks the integrity, so your packaging doesn’t flop.
- Waste Not: Built-in analytics optimise processes, reduce waste, and keep quality consistent.
Automotive Manufacturing
- Glue That Sticks: Adhesive bonding gets the FLIR treatment, temperature thresholds and placement verified like a boss.
- Weld Watch: Thermal anomalies in welds? FLIR spots them before they become structural regrets.
- Plastic Fantastic: Moulding and IR welding defects don’t stand a chance. Uniformity is the name of the game.
What About Steel and Heavy Industries? How will Thermal Imaging See Us Through?
Hard to imagine needing a thermal imager in steel production, we already know it’s hot in there – right!
Ok here are few examples:
How about monitoring furnace temperatures?
Maintaining the optimal heating conditions.
Detects hot spots or uneven heating in blast furnaces, electric arc furnaces, or ladles.
Inspection of refractory linings, what does that achieve? Thermal imaging can identify wear and tear or damage in furnace linings long before failure occurs. Prevents costly downtime and safety hazards.
How about Process Control?
Checking the temperature of steel can help during casting, rolling, and forging.
Quality and consistency are maintained, this is a must in production.
Preventive Maintenance
As with all industrial processes, motors and bearings are as important as your heart is to keep blood pumping. A motor or bearing failure will kill your process faster than you can say Jack Robinson, and you’ll need an emergency crash team to respond. Or, you could simply monitor with a FLIR Thermal Camera and detect the early signs of overheating, so no one needs 999.
Regular checks will reduce risk of equipment failure, and because these cameras are so flexible, you’ll be able to monitor those hard to get at pieces of equipment, so you’ll be in and out of there in no time.
Safety Monitoring
Consider this as a plus point No. 1: You can identify leaks or spills of molten metal.
Plus point No. 2: Keep your colleagues safe by spotting dangerous heat zones.
Time For Some Thermal Imaging FAQs
Q: Can thermal cameras measure exact temperatures?
A: Yes, they can, and they are extremely accurate, but here’s the important bit to consider: Surface emissivity and environmental conditions can affect precision. So strictly speaking, calibration matters.
Q: Do thermal cameras work in complete darkness?
A: Well since they detect heat or it’s more technical term, infrared radiation they’ll work just fine in the dark, but the operator may need to turn the light on.
Q: Can they detect gas leaks?
A: Yes, but you’ll probably be better using a FLIR acoustic imager; thermal imagers will detect the indirect signs like temperature changes. But, with acoustic imagers, gas leaks can be detected and costs lost quantified, so if that’s important plump for an acoustic imager.
Q: Are thermal cameras safe to use around sensitive equipment or people?
A: It’s the same as using the camera on your smartphone. Thermal cameras are totally passive; they don’t emit radiation, they just detect it.
Q: How often should thermal inspections be done?
A: With thermal cameras, it really depends on what is required. They are your flexible friend when it comes to monitoring assets. For instance, you may want a fixed monitor on critical infrastructure, with an eyes wide open approach. Or a periodic check-in to verify assets weekly, monthly, or quarterly.
Q: What’s the difference between infrared and thermal imaging?
A: Infrared falls within the spectrum of electromagnetic radiation, just beyond the visible light spectrum. Thermal imaging is the art of turning that part of the spectrum into a heat map masterpiece. So, one’s the science and the other is the show. All thermal cameras are infrared, but not all infrared cameras are thermal. “You can lead a horse to water but… well you know the rest”.
Final thought: Could FLIR be the Industrial MVP
Whether it’s predictive maintenance, quality control, or safety assurance, FLIR’s thermal imaging isn’t just watching, it’s working. Real-time diagnostics, automated inspection, and anomaly detection make it the unsung hero of modern industry. And unlike your office thermostat, it actually knows what it’s doing.
Looking for a Thermal Imaging Camera then here you’ll find something to hit the target.
FLIR offers a wide range of thermal cameras, and we’ve grouped by use cases:
| Use Case | Models and Stock Nos |
|---|---|
| Mobile & Compact | FLIR ONE (136-8285) , C3-X (211-0025) , TG165 (202-0645) |
| Industrial Entry-Level | TG267 (193-2941) , TG268 (045-6038) , TG275 (189-6839) , TG297 (193-2944) , TG298 (045-6317) |
| Point & Shoot | E5-XT (189-1586) , E5-PRO (273-2555) , E6-PRO (273-2556) , E8-PRO (272-9212) |
| Electronic Testing | ETS320 (135-6220) |
| Professional | E52 (249-8995) , E54 (206-7257) , E75 (135-3293) , E76 (206-7259) , E86 (206-7334) , E96 (206-7262) |
| High-Performance | T530 (202-0648) , T540 (202-0659) , T560 (206-7351) |
| Fixed Monitoring | AX8 (893-8489) |
| Explosion-Proof | Cx5 (261-9714) |
Comments