Skip to main content

What is Arduino App Lab and What Does It Mean for Engineers?

by ConnorDobson

Earlier this month, Arduino made headlines with two major announcements: the launch of the Arduino® UNO Q (066-5593) and the news that Qualcomm has acquired Arduino, signalling a bold new era for embedded innovation. In our previous article, we explored what makes the UNO Q such a game-changer, a board that merges Linux computing with real-time microcontroller control.

Today, we’re diving deeper into the software that completes this vision: Arduino App Lab. Alongside Arduino’s recent introduction of its AI Assistant, these developments are transforming the way engineers work, making coding easier, enabling rapid prototyping, and shortening time-to-market for new innovations.

Arduino UNO Q board with Arduino App Lab interface on screen.

Arduino App Lab Explained: A Unified Development Environment

Arduino App Lab is a cross-platform tool that runs on your PC or directly on the UNO Q in Single-Board Computer (SBC) mode. It enables engineers to create Apps that combine:

  • Python® programs for Linux-based logic and connectivity.
  • Arduino sketches for precise hardware control.
  • Bricks, modular components that add AI models, web servers, or API clients without complex coding.

This architecture is powered by Bridge, Arduino’s RPC layer, which ensures seamless communication between the Linux processor and the microcontroller.

Arduino UNO Q board with Arduino App Lab interface showing Python

How Arduino App Lab Works: From Idea to Deployment

The workflow is streamlined for rapid prototyping:

  1. Launch App Lab and connect your UNO Q.
  2. Select a ready-made example or start from scratch.
  3. Press Launch, App Lab compiles the microcontroller sketch, builds the Linux component, deploys Bricks, and launches everything on the board.

Logs for both domains are accessible in the editor, making debugging and iteration fast and efficient.

An example of creating and deploying apps in Arduino App Lab

Ready-to-Use Examples for Faster Development

App Lab includes a growing library of examples tailored for engineers:

  • Hello World (Blink LED): Validate connectivity and workflow.
  • AI-powered Apps: Implement object recognition or keyword spotting using Bricks.
  • Web-enabled Projects: Build REST APIs and dashboards with minimal effort.

These examples demonstrate how Linux and microcontroller domains can work together, enabling scalable solutions from simple prototypes to advanced edge AI systems.

Arduino App Lab editor showing example apps in Arduino App Lab.

Bricks: Modular Building Blocks for Complex Features

Bricks are at the heart of Arduino App Lab’s flexibility. They act as plug-and-play modules that bring advanced functionality into your projects without requiring you to build everything from scratch. Each Brick encapsulates a specific service or capability, such as:

  • AI Models for vision or audio recognition.
  • Data Services for external API or database connectivity.
  • UI Components for web-based monitoring and control.

By combining Bricks with your own code, you can deliver sophisticated applications without reinventing the wheel. There are plenty of Bricks available, and they are divided into the following categories:

  • AI - Audio
  • AI - Computer Vision
  • AI - Sensor data
  • API
  • IoT
  • Storage
  • Web User Interface

Why Bricks Matter

For engineers, Bricks mean:

  • Reduced Development Time
  • Rapid Prototyping
  • Scalability

Bricks transform App Lab into more than an editor, they make it a platform for innovation, enabling complex applications without the complexity.

Visual representation of Arduino App Lab Bricks for AI, web, and data services.

Why Engineers Should Care: Rapid Prototyping Made Simple

The synergy between UNO Q hardware and App Lab software offers:

  • Unified Development: One editor for Linux and microcontroller code.
  • Cross-Domain Integration: Bridge ensures smooth data exchange.
  • Scalability: Start small and expand to AI and IoT without changing platforms.

Combined with Arduino’s AI Assistant, which we explored in our recent article, these tools are making engineers’ lives easier: reducing complexity, accelerating development, and paving the way for faster innovation.

Ready to start building?

Explore Arduino App Lab today, the Arduino UNO Q (066-5593) is available to order from RS.

Stay tuned to our Arduino Hub for upcoming projects and articles showcasing the full potential of UNO Q and App Lab.

 

Arduino UNO Q coming out of a box
The Arduino UNO Q (066-5593) .

 

Find Out More About the Arduino UNO Q

Our Expert Team is ready to help you explore why Arduino UNO Q is the smart choice for your next project. Get in touch today to start the conversation.

I work for RS, please feel free to reach out with any queries about our solutions and services.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments