How can I control the brightness of the sensor? Can anyone recommend an affordable, entry-level hardware solution that would accomplish this? (Other programming languages, Raspberry Pis, or microcontrollers are not considered.)
A friend sent me this code:
#include <stdio.h>
#include "CH341.h"
static int open_device(HANDLE *out)
{
*out = CH341OpenDeviceEx(0);
if (*out == NULL || *out == INVALID_HANDLE_VALUE) {
return -1;
}
return 0;
}
static void close_device(HANDLE h)
{
CH341CloseDevice(h);
}
static int configure_io(HANDLE h)
{
if (CH341ResetDevice(0) != 0) return -1;
if (CH341SetOutput(0, 0xffffffff, 0x00000000, 0x00000000) != 0) return -1;
if (CH341SetOutput(0, 0b11111, 0xffffffff, 0xffffffff) != 0) return -1;
return 0;
}
int main(void)
{
HANDLE hdlCh341;
if (open_device(&hdlCh341) != 0) {
fprintf(stderr, "Failed to open CH341 device\n");
return 1;
}
printf("%lu\n", (unsigned long)hdlCh341);
printf("%lu\n", CH341GetVersion());
if (configure_io(hdlCh341) != 0) {
fprintf(stderr, "Failed to configure CH341 I/O\n");
close_device(hdlCh341);
return 1;
}
close_device(hdlCh341);
return 0;
}
Comments