DesignSpark Circuit Simulator Maintenance on 23rd May at 15:00 UTC for 2 hours

Skip to main content

Upgrading the Air Quality Application to the December 2022 Release

by Andrew Back

WEB interface for ESDK

Latest release includes support for new sensors and new features such as a LAN dashboard.

A new Air Quality application device image for ESDK hardware is now available for download and includes a number of updates, including new features for the local device display and a brand new LAN web interface. In addition to which a bug was fixed which could cause the integrated display to not function if there was no Ethernet connection.

Upgrade steps

Since this upgrade involves writing out a new image, it’s important to first backup the configuration file, /boot/aq/aq.toml, along with any CSV logs in /aq/data/.

The latest image can be downloaded via:

https://downloads.designspark.io/projects/aq-device/images/aq-pi-011222.zip

Following which this can be written out to the Micro SD card using either the command line dd utility (Linux and Mac) or a graphical tool, such as balenaEtcher. Finally, the configuration file aq.toml can be copied back to the aq directory in the boot partition.

New sensors

New sensors shown on ESDK screen

Support has been added to the DesignSpark.ESDK library and in turn the aq-device application which uses this, for the following new ESDK sensor modules:

  • NO2 (nitrogen dioxide)
  • FDH (formaldehyde)
  • NRD (nuclear radiation)

Thereby enabling sensing for a key atmospheric pollutant, a known carcinogen, and nuclear radiation. For further details, please see the above-linked articles. A small number of each of these boards is being assembled for the Air Quality beta community, but as with the rest of the ESDK platform, these are open hardware designs and anyone is free to assemble their own boards.

Since there was not sufficient space on the default screen to add panels for the new sensors, there is now a second sensor data screen — which can be seen above — and switching between the two is done using the ESDK inner two physical buttons. It’s possible that the application may be further extended in future to support additional sensors — either official modules, else third-party modules integrated via the plug-in mechanism — and more screens may be added in the same manner.

GPS status

GPS Status indicator - cross hairs

Those who make use of the GPS receiver will be pleased to learn that the local display now indicates when this has a position fix, via a small cross hairs icon which appears top-right.

CSV logging

CSV Logging - Recording

Similarly, the local display also indicates when CSV logging is enabled. Logging can be enabled to start at boot time via aq.toml, and also toggled via the top physical button. However, please be aware that there can be a delay of a few seconds before the button press is registered and so repeatedly pressing this should be avoided.

Local debug

Debug Screen

A debug screen may be accessed via a long press on the touch screen. The information provided here includes, if it is enabled, details of the GPS receiver mode and how many satellites it can see. Along with the location also, which if the GPS receiver is not enabled, is taken from aq.toml.

Debug Screen - Save Successful

A second debug screen may be accessed via a short press and this provides details of the last successful and unsuccessful attempts at publishing data to the DesignSpark Metrics cloud.

Another long press on the touch screen will return to the sensor dashboard.

LAN dashboard

AQ Dashboard

A major new feature in this release is a network dashboard, which provides the same information as the local dashboard, albeit over a LAN connection and with all sensor data plotted. Where a plot has multiple metrics these may be toggled on/off by clicking on the corresponding legend, which can prove particularly useful with sensors such as PM2, which provides four measurements.

The dashboard may be accessed via the URL:

http://airquality.local

LAN Dashboard

Debug information is also available via this interface and may be selected using the menu item.

See the above video for a demonstration.

Wrapping up

In this article, we’ve taken a look at the new features in the December 2022 release of the Air Quality device application and how to upgrade to this. As ever the official documentation should be consulted for all the configuration details.

  — Andrew Back

Open source (hardware and software!) advocate, Treasurer and Director of the Free and Open Source Silicon Foundation, organiser of Wuthering Bytes technology festival and founder of the Open Source Hardware User Group.
DesignSpark Logo

Enjoying DesignSpark?

Create an account to unlock powerful PCB and 3D Mechanical design software, collaborate in our forums, and download over a million free 3D models, schematics, and footprints.
Create an account

Already a DesignSpark member? Log In

Comments