UCLR Formula Student Progress so far…
Overview
We are a student-led team that competes in Formula Student UK with the University College London (UCL). Last academic year, our team consisted of 50 people working to design and manufacture our new car, Lola. We improved our performance in the static events, which was a highlight during our concept class competition in 2025.
Our main design philosophy is to maximise mechanical grip and to be as lightweight as possible. We did this by reducing the weight of our chassis and front suspension and taking a radical approach to our rear suspension design, all in line with the regulations. Unfortunately, we could not manufacture the car in time for the 2026 competition, but we are working hard as a team to be ready for next year’s competition.
This year, we're aiming to improve on our scrutineering performance and complete the endurance event, which held us back in previous years. We're also targeting a total vehicle weight of less than 200kg as part of our overall lightweighting philosophy.
Car Development
When designing a new car, the most important things to design first are the chassis and suspension in parallel. We started with a few initial sketches around the front suspension pick-up points and load paths. We aimed to minimise the number of tubes using strong triangulation to retain stiffness and reduce weight to 30kg, in conjunction with FEA static studies in ANSYS to find the minimum wall thickness of the tubes that could withstand acceleration and cornering loads. Further considerations were to have a minimum clearance of 10 mm from the regulations to account for any manufacturing differences and to reduce the number of tubes going to a single node to make the chassis easier to weld.
For the front suspension, we opted for a double-wishbone mono-shock pullrod assembly to lower the centre of mass and reduce weight. With this design, we achieved a 33% reduction in mass compared with our previous pushrod front suspension. Because we considered the front suspension pickup points during chassis design, no additional mass was required to accommodate chassis integration.
One of the biggest challenges we ran into was sourcing components on the timeline we needed, especially with a small team managing procurement alongside design work. We also had to balance performance optimisation against our cost constraints, which is a big part of why we went with the solid axle and trailing arm setup instead of a differential. It meant more design work upfront to make sure we weren't sacrificing too much performance, but it kept us within budget.
Our approach to the rear suspension was constrained by cost because a differential can be quite complex, expensive and heavy. As our main goal for our car design is to reduce mass and cost, we went with a solid axle attached to two trailing arms, which is connected to a torsion bar. The torsion bar acts as an anti-roll bar by providing roll stiffness and heave decoupling. During cornering, the inside wheel is intentionally unloaded to help reduce tyre scrub and understeer within the corners.
Figure 1 - Some manufactured parts of the trailing arms for the rear suspension.
Our engine is a single-cylinder Honda CRF450R as it satisfied the power-to-weight ratio we wanted to achieve by having a 15- 20 kg mass advantage compared to a four-cylinder engine while achieving similar lap times in OptimumLap. The only downside is that the single-cylinder engine produces a significant amount of noise and high vibrations. Meaning the exhaust design research needed to be conducted around acoustics to find a muffler and silencer that can reduce the engine noise in line with the regulation while reducing back pressure.
Figure 2 - The single-cylinder Honda CRF450R engine used for our car.
Sensor selection was the starting point of the loom design. This year we decided to manufacture our loom in-house with the electronics team to reduce cost and to allow for more freedom in sensor selection.
The electronics team worked closely with the vehicle designers to identify what needed to be measured, define the operating requirements, and narrow down suitable sensors and electrical components. The component list was then restructured so that each component was represented by a single connector and its corresponding mating part. Connectors were grouped by system, particularly those in the shutdown circuit and those already fitted to the engine harness. Separate dash and gear-shifter blocks were also added to the architecture. An Excel connection sheet was developed to define the pin-to-pin wiring between components and provide a clearer basis for the final loom. Wiring diagrams and magnetic component blocks on whiteboards were used to explore the relative positions of major systems. Finally, individual components and complete subsystems were bench-tested before integration.
Testing
While Lola hasn't competed yet, our previous car's performance in the 2025 concept class static events gave us a strong base to build from, and a lot of the lessons from that scored performance directly shaped decisions like the cooling and intake redesign this year.
As Lola has not been produced yet, full car testing is not an option now. However, over the past year, multiple CFD simulations have been conducted on our new cooling system, which includes a sidepod redesign to find the optimal geometry to minimise overheating of our engine. From this, an 80% inlet area side duct produced an average 11.7 degrees Celsius drop across the radiator in trackside testing with our old car, which aligned with the predictions made in CFD.
Figure 3 - Final intake geometry fully assembled.
CFD studies were conducted to determine our intake design as we tested different geometries such as a straight runner and a curved runner with and without a diffuser to find a design with the least pressure loss. The curved runner without a diffuser produced a reduction of 47% in pressure loss compared to the straight runner. Having a diffuser with the curved runner made the performance of the intake worse as it caused flow separation.
A test was done with the Honda CRF450R to find how much noise the engine produces at an unknown RPM. The noise was measured in decibels, and the engine’s RPM was back-calculated based on the pulse from the audio files. Then a Fourier transform of the audio file was used to find the loudest harmonics produced, which were 6th, 9th, and 12th. Post-testing, a J-pipe and silencer were added to the exhaust system to reduce noise at those specific harmonics.
Team dynamics
Our team structure consists of six sub-teams, including design, build, performance, electronics, costing and operations. These sub-teams have leaders who are overseen by the team manager and the technical director. The team manager is responsible for sponsorship, procurement and operations. Whereas the technical director is responsible for ensuring that the technical drawings produced by the team are up to standard and that manufacturing is being completed on time in line with the Gantt chart.
Our team is made up of students from a real mix of backgrounds, not just mechanical engineering. We've got members from electronic and electrical engineering, computer science, and even some from outside engineering entirely, which has been genuinely useful when it comes to problems like the loom design and sensor integration, where you need people who think differently about the same problem. Having that spread of expertise across the sub-teams means each area gets people who actually specialise in it, rather than everyone generalising across the board.
As a team, we host weekly meetings for each sub-team, as well as a general team meeting, to make sure all team members are up to date with what is happening. We also like to host social the most notable one is our annual Secret Santa to help boost team morale, making our team members feel welcomed and comfortable being themselves in the team.
Lessons learned from the current year
Outsourcing our manufacturing to other trusted suppliers to help speed up our process.
Creating a manufacturing list with the other racing teams in our university to track how long parts might take to be delivered.
Keeping the group we send to on-track testing small to allow for a more efficient process, as we can run multiple test programs.
Improve our team dynamics by reducing our team size from 50 to 30 dedicated members that we can rely on when deadlines get tight.
RS BOM
Below is a Bill of Materials outlining the key RS components Student Fund used across our loom and testing setup this year.
| Item | Link | Amount (£) (exc.VAT) |
| 8 x Small orange cones | (050-3681) | 60.96 |
|
2x Brake Pressure Sensor |
(031-5083) | 265.32 |
|
100m Spec 55 - 20 AWG wire |
(329-9433) | 112.95 |
|
DR25 Heat Shrink |
(219-6507) | 77.38 |
|
Electrical Tape |
(504-2396) | 16.16 |
Comments